This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [21 Jul 2021 10:50] – [Power on sequence] Andrei Cozma | resources:eval:user-guides:ad-fxtof1-ebz:ug_xavier_nx [21 Jan 2022 13:29] (current) – [Power on sequence] Andrei Cozma | ||
---|---|---|---|
Line 12: | Line 12: | ||
==== Prepare SD card ==== | ==== Prepare SD card ==== | ||
- | * Follow steps presented | + | * Download and flash on a SD card the latest image provided from the following link: [[repo> |
* Download L4T BSP [[https:// | * Download L4T BSP [[https:// | ||
* Extract kernel_src from BSP package | * Extract kernel_src from BSP package | ||
Line 25: | Line 25: | ||
* Connect the HDMI cable from the monitor to the Jetson HDMI connector | * Connect the HDMI cable from the monitor to the Jetson HDMI connector | ||
* Connect the 25 pins flex cable between the camera and the interposer | * Connect the 25 pins flex cable between the camera and the interposer | ||
- | * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides. | + | * Connect the 15 pons camera cable between the J1 connector of Jetson Xavier NX and the P1 connector of the interposer. |
+ | <WRAP center round important 100%> | ||
+ | Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | ||
+ | </ | ||
* Connect a USB mouse and keyboard to the Xavier NX | * Connect a USB mouse and keyboard to the Xavier NX | ||
* Connect the power supply to the interposer | * Connect the power supply to the interposer | ||
Line 48: | Line 51: | ||
{{: | {{: | ||
+ | |||
+ | ==== Enabling the point cloud display in aditof-demo ==== | ||
+ | |||
+ | * The demo application has the capability to display a point cloud image if it detects an OpenCV module called viz. | ||
+ | Unfortunately OpenCV does not provide binaries for this module so a manual build is needed. The steps required to | ||
+ | install OpenCV and include it in the project are presented here: | ||
+ | [[https:// | ||
+ | |||
+ | * If aditof-demo finds all the OpenCV required modules a button in the interface will allow you to display the point cloud. By toggling the button a separate window will appear. | ||
+ | {{ : | ||
{{navigation AD-FXTOF1-EBZ# | {{navigation AD-FXTOF1-EBZ# | ||