This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_rpi [09 Apr 2021 13:02] – Add ad-fxtof1-ebz user guide for Rpi Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_rpi [21 Jan 2022 13:27] (current) – [Power on sequence] Andrei Cozma | ||
---|---|---|---|
Line 17: | Line 17: | ||
* Plug the SD card into the Raspberry Pi SD card slot. To benefit from the most recent software updates it is highly recommended to update the SD card with the [[https:// | * Plug the SD card into the Raspberry Pi SD card slot. To benefit from the most recent software updates it is highly recommended to update the SD card with the [[https:// | ||
* Connect the HDMI cable from the monitor to the Raspberry Pi HDMI connector | * Connect the HDMI cable from the monitor to the Raspberry Pi HDMI connector | ||
- | * Connect the molex cable between the camera and the interposer | + | * Connect the 25 pins flex cable between the camera and the interposer |
- | * Connect the RPi camera cable between the RPi and the P1 connector of the interposer | + | * Connect the 15 pins camera cable between the RPi and the P1 connector of the interposer. **Make sure to use the cable with contacts on opposite sides.** |
+ | <WRAP center round important 100%> | ||
+ | Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | ||
+ | </ | ||
* Connect the interposer to the power supply | * Connect the interposer to the power supply | ||
* Connect the RPi to the power supply | * Connect the RPi to the power supply | ||
Line 43: | Line 46: | ||
{{: | {{: | ||
+ | |||
+ | ==== Enabling the point cloud display in aditof-demo ==== | ||
+ | |||
+ | * The demo application has the capability to display a point cloud image if it detects an OpenCV module called viz. | ||
+ | Unfortunately OpenCV does not provide binaries for this module so a manual build is needed. The steps required to | ||
+ | install OpenCV and include it in the project are presented here: | ||
+ | [[https:// | ||
+ | |||
+ | * If aditof-demo finds all the OpenCV required modules a button in the interface will allow you to display the point cloud. By toggling the button a separate window will appear. | ||
+ | {{ : | ||
{{navigation AD-FXTOF1-EBZ# | {{navigation AD-FXTOF1-EBZ# | ||