This is an old revision of the document!
Raspberry Pi User Guide
Setting up the system
Required hardware
Power on sequence
Plug the
SD card into the Raspberry Pi
SD card slot. To benefit from the most recent software updates it is highly recommended to update the
SD card with the
latest SD card image
Connect the HDMI cable from the monitor to the Raspberry Pi HDMI connector
Connect the molex cable between the camera and the interposer
Connect the RPi camera cable between the RPi and the P1 connector of the interposer
Connect the interposer to the power supply
Connect the RPi to the power supply
Connect a
USB mouse and keyboard to the Raspberry Pi. It's possible to use either a mouse & keyboard combo or a separate mouse and keyboard
Power off sequence
Troubleshooting
Linux does not boot
The
SD card is corrupted and this prevents the system from booting. Reflash the
SD card with the
SD card image.
Running the evaluation application
Once Linux boots you'll see on the HDMI monitor the Linux desktop and on the top left corner a shortcut to the evaluation application. Double clicking on the icon will start the evaluation application. A console window will open to show the application's status and, after a few seconds, the evaluation application GUI will be displayed.