This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [17 Dec 2021 12:55] – Add point cloud description Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [02 May 2022 07:41] (current) – Nvidia source file link updated Robert Budai | ||
---|---|---|---|
Line 13: | Line 13: | ||
==== Prepare SD card ==== | ==== Prepare SD card ==== | ||
* Download and flash on a SD card the latest image provided from the following link: [[repo> | * Download and flash on a SD card the latest image provided from the following link: [[repo> | ||
- | * Download L4T BSP [[https:// | + | * Download L4T BSP [[https:// |
* Extract kernel_src from BSP package | * Extract kernel_src from BSP package | ||
* ADI ToF camera driver and devicetree should be taken from [[https:// | * ADI ToF camera driver and devicetree should be taken from [[https:// | ||
Line 25: | Line 25: | ||
* Connect the HDMI cable from the monitor to the Jetson HDMI connector | * Connect the HDMI cable from the monitor to the Jetson HDMI connector | ||
* Connect the 25 pins flex cable between the camera and the interposer | * Connect the 25 pins flex cable between the camera and the interposer | ||
- | * Connect the 15 pins camera cable between the Jetson Nano and the P1 connector of the interposer. Make sure to use the cable with contacts on opposite sides. | + | * Connect the 15 pins camera cable between the Jetson Nano and the P1 connector of the interposer. |
+ | <WRAP center round important 100%> | ||
+ | Some of the AD-FXTOF1-EBZ kits are missing the correct 15 pins cable to connect to Raspberry Pi or the Nvidia platforms. If in your box there is only one 15 pins cable having the contacts on the same side, please get a new cable with contacts on opposite sides (e.g. [[https:// | ||
+ | </ | ||
* Connect a USB mouse and keyboard to the Jetson | * Connect a USB mouse and keyboard to the Jetson | ||
* Connect the interposer to the power supply | * Connect the interposer to the power supply |