This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [22 Sep 2021 14:25] – [Power on sequence] Septimiu Vana | resources:eval:user-guides:ad-fxtof1-ebz:ug_jetson [17 Dec 2021 12:55] – Add point cloud description Septimiu Vana | ||
---|---|---|---|
Line 41: | Line 41: | ||
* remove the 5V supply from the interposer | * remove the 5V supply from the interposer | ||
+ | ===== Running the evaluation application ===== | ||
+ | |||
+ | [[https:// | ||
+ | |||
+ | Once Linux boots you'll see on the HDMI monitor the Linux desktop and on the top left corner a shortcut to the evaluation application. Double clicking on the icon will start the evaluation application. A console window will open to show the application' | ||
+ | |||
+ | {{: | ||
+ | |||
+ | When starting the application, | ||
+ | |||
+ | The evaluation application allows to do live streaming of depth and IR data as well as recording the depth and IR data and playing back from a file. The depth data is displayed as a color map ranging from warm to cold colors as the distance from the camera increases. A point in the middle of the depth image shows the distance in mm to the target. | ||
+ | |||
+ | There are 3 operating modes that determine the range of the system: | ||
+ | |||
+ | * Near - 25cm to 80cm | ||
+ | * Medium - 30cm to 3m | ||
+ | |||
+ | When in a certain operating mode the system will measure distances outside of the mode's range but those will not be accurate. The evaluation application also displays the temperature in deg C of the camera (AFE). | ||
+ | |||
+ | The framerate at which data is acquired from the system is constantly updated on the GUI. The camera board outputs data at 30 frames per second (fps), but due to USB connection limitations, | ||
+ | |||
+ | ==== Enabling the point cloud display in aditof-demo ==== | ||
+ | |||
+ | * The demo application has the capability to display a point cloud image if it detects an OpenCV module called viz. | ||
+ | Unfortunately OpenCV does not provide binaries for this module so a manual build is needed. The steps required to | ||
+ | install OpenCV and include it in the project are presented here: | ||
+ | [[https:// | ||
+ | |||
+ | * If aditof-demo finds all the OpenCV required modules a button in the interface will allow you to display the point cloud. By toggling the button a separate window will appear. | ||
+ | {{ : | ||
==== Troubleshooting ==== | ==== Troubleshooting ==== | ||
Line 46: | Line 76: | ||
* The SD card is corrupted and this prevents the system from booting. Reflash the SD card or check generated devicetree or kernel image | * The SD card is corrupted and this prevents the system from booting. Reflash the SD card or check generated devicetree or kernel image | ||
- | ---- | + | * The demo application hangs after closing the main window |
- | ===== Running | + | * Due to some limitations the application always hangs if it is closed using the regular X button from the window top bar (title bar). To avoid this unpleasant hang, we've made available a second X button in the top right corner right above the title bar that can be used to safely close the demo application. We hope this to be a temporary workaround. |
- | [[https:// | ||
{{navigation AD-FXTOF1-EBZ# | {{navigation AD-FXTOF1-EBZ# | ||