This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-freqcvt1-ebz:software [29 Mar 2016 13:18] – [Theory of operation] Michael Hennerich | resources:eval:user-guides:ad-freqcvt1-ebz:software [19 Jan 2018 10:25] (current) – rename xcomm_zynq -> master Alexandru Ardelean | ||
---|---|---|---|
Line 12: | Line 12: | ||
An additional checkbox in the plugin is displayed, allowing the user to enable or disable the tuning logic. Once enabled the RX/TX LO Spin-Button switches it’s range from 70MHz-6GHz to 1MHz-100MHz. | An additional checkbox in the plugin is displayed, allowing the user to enable or disable the tuning logic. Once enabled the RX/TX LO Spin-Button switches it’s range from 70MHz-6GHz to 1MHz-100MHz. | ||
+ | {{: | ||
Two environmental variables allow the user to control the sign in the mixing equation as well as the window size (span) where the signal is centred around the SAW band pass filter center frequency. | Two environmental variables allow the user to control the sign in the mixing equation as well as the window size (span) where the signal is centred around the SAW band pass filter center frequency. | ||
Line 28: | Line 29: | ||
^ Function ^ File ^ | ^ Function ^ File ^ | ||
- | | FMCOMMS2/3 Device Tree | [[linux.github> | + | | FMCOMMS2/3 Device Tree | [[linux.github> |