The production testing of AD-FMCXMWBR1-EBZ (DUT) is automated. The test procedure runs on ADRV9009-ZU11EG RF-SOM.
For the test is needed an SD card with the Kuiper image that has the test procedure installed. If there is no such SD card available, it can be created.
Creating a carrier SD test card
Release february 2022
Figure 1. AD-FMCXMWBR1-EBZ on carrier
Figure 2. AD-FMCXMWBR1-EBZ test setup
After the connections are done as explained in the “Required setup for production test” power up by switching S12 of ADRV2CRR-FMC to on position. When booting, it is mandatory to have the full setup, with the AD-FMCXMWBR1-EBZ board connected. This way, the devices on the test board will be probed correctly at startup. The test instructions will prompt on the screen and the testing should be done using the following steps: