Wiki

This version is outdated by a newer approved version.DiffThis version (07 Nov 2013 18:48) was approved by Robin Getz.The Previously approved version (05 Nov 2013 23:16) is available.Diff

This is an old revision of the document!


AD-FMCOMMS3-EBZ Hardware

Downloads

This is the latest and greatest Rev “A” of this board, and is ready for production. Note that the Transfomers on the Rev D board are Mini Circuits TCM1-63AX+. They are rated for a operating frequency between 10 MHz and 6 GHz.

Picture and Main components

Outline

For those that don't want to load up the Allegro viewer, here is a basic outline/component placements of the board. While this board does meet parts of the VITA-57.1 (FMC) specifications, there are many things it violates, and is not designed to be a form/fit/function board.

  • The FMC cutout for the bezel is missing (so we could space the SMA connectors out as far as possible, and achieve maximum isolation between the channels.
  • The mounting holes near the end of the board with the connectors is also in the wrong place (so it didn't effect the RF path between the connectors and the AD9361.
  • The FMC height specification on the top side of the board is violated to put some 90 degree SMA connectors.

Size

The size of the board (not including the SMA connectors, which project beyond the edge of the board) is 73.3mm x 69mm. This is under the FMC specifications of 84mm x 69mm). The mounting holes are not compliant with the FMC standard, and are shown below.

Layers

The AD-FMCOMMS3-EBZ is a 10 layer board.

Design Cross Section

Subclass Name Type Material Thickness (MIL) Conductivity (mho/cm) Dielectric Constant Loss Tangent Shield Width (MIL)
SURFACE AIR 0 1 0
TOP CONDUCTOR COPPER 2.025 595900 1 0 8.00
DIELECTRIC FR-4 8 0 3.38 0.035
L2_GND PLANE COPPER 1.35 595900 1 0.035 Y
DIELECTRIC BT_EPOXY 3 0 4.10 0.02
L3_PWR PLANE COPPER 1.35 595900 1 0.035 Y
DIELECTRIC FR-4 3 0 4.10 0.035
L4_GND PLANE COPPER 1.35 595900 1 0.035 Y
DIELECTRIC BT_EPOXY 4.60 0 4.10 0.02
L5_SIG CONDUCTOR COPPER 1.35 595900 1 0.035 3.80
DIELECTRIC FR-4 8 0 4.10 0.035
L6_SIG CONDUCTOR COPPER 1.35 595900 1 0.035 3.80
DIELECTRIC BT_EPOXY 4.60 0 4.10 0.02
L7_GND PLANE COPPER 1.35 595900 1 0.035 Y
DIELECTRIC FR-4 3 0 4.10 0.035
L8_PWR PLANE COPPER 1.35 595900 1 0.035 Y
DIELECTRIC BT_EPOXY 3 0 4.10 0.02
L9_GND PLANE COPPER 1.35 595900 1 0.035 Y
DIELECTRIC FR-4 8 0 3.38 0.035
BOTTOM CONDUCTOR COPPER 2.025 595900 1 0 8.00
SURFACE AIR 0 1 0

Navigation - AD-FMCOMMS3-EBZ

resources/eval/user-guides/ad-fmcomms3-ebz/hardware.1383846475.txt.gz · Last modified: 07 Nov 2013 18:47 by Robin Getz