This is an old revision of the document!
The AD9361 is a high performance, highly integrated RF Agile Transceiver™. Its programmability and wideband capability make it ideal for a broad range of transceiver applications. The device combines an RF front end with a flexible mixed-signal baseband section and integrated frequency synthesizers, simplifying design-in by providing a configurable digital interface to a processor.
This document describes the No-OS software used to control the AD9361 part.
An API is available to be used on systems without OS to interact with the AD9361 and provides all the necessary functions to control it.
Below is presented a short description of all the functions provided in the API:
Device Global Settings | |
---|---|
struct ad9361_rf_phy *ad9361_init (AD9361_InitParam *init_param) | Initializes the FMCOMMS2 board. Receives as parameter a structure that contains the AD9361 initial parameters. Returns a structure that contains the AD9361 current state in case of success, negative error code otherwise. |
int32_t ad9361_set_en_state_machine_mode (struct ad9361_rf_phy *phy, uint32_t mode) | Sets the Enable State Machine (ENSM) mode. Receives as parameters a structure that contains the AD9361 current state and the ENSM mode (SLEEP, ALERT, FDD, PINCTRL). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_en_state_machine_mode (struct ad9361_rf_phy *phy, uint32_t *mode) | Gets the Enable State Machine (ENSM) mode. Receives as parameters a structure that contains the AD9361 current state and a variable to store the selected ENSM mode. Returns 0 in case of success, negative error code otherwise. |
Receive Chain Settings | |
int32_t ad9361_set_rx_rf_gain (struct ad9361_rf_phy *phy, uint8_t ch, int32_t gain_db) | Sets the receive RF gain for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel number (0, 1) and the RF gain. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_rf_gain (struct ad9361_rf_phy *phy, uint8_t ch, int32_t *gain_db) | Gets current receive RF gain for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RF gain. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_rf_bandwidth (struct ad9361_rf_phy *phy, uint32_t bandwidth_hz) | Sets the RF bandwidth. Receives as parameters a structure that contains the AD9361 current state and the desired bandwidth in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_rf_bandwidth (struct ad9361_rf_phy *phy, uint32_t *bandwidth_hz) | Gets current RF bandwidth. Receives as parameters a structure that contains the AD9361 current state and a variable to store the bandwidth value in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_sampling_freq (struct ad9361_rf_phy *phy, uint32_t sampling_freq_hz) | Sets the sampling frequency. Receives as parameters a structure that contains the AD9361 current state and the desired sampling frequency in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_sampling_freq (struct ad9361_rf_phy *phy, uint32_t *sampling_freq_hz) | Gets current sampling frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the sampling frequency value in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_lo_freq (struct ad9361_rf_phy *phy, uint64_t lo_freq_hz) | Sets the LO frequency. Receives as parameters a structure that contains the AD9361 current state and the desired LO frequency in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_lo_freq (struct ad9361_rf_phy *phy, uint64_t *lo_freq_hz) | Gets current LO frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the LO frequency value in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_lo_int_ext(struct ad9361_rf_phy *phy, uint8_t int_ext) | Switches between internal and external LO. Receives as parameters a structure that contains the AD9361 current state and the desired option (INT_LO, EXT_LO). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_rssi (struct ad9361_rf_phy *phy, uint8_t ch, struct rf_rssi *rssi) | Gets the RSSI for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RSSI. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_gain_control_mode (struct ad9361_rf_phy *phy, uint8_t ch, uint8_t gc_mode) | Sets the gain control mode for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and the gain control mode (GAIN_MGC, GAIN_FASTATTACK_AGC, GAIN_SLOWATTACK_AGC, GAIN_HYBRID_AGC). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_gain_control_mode (struct ad9361_rf_phy *phy, uint8_t ch, uint8_t *gc_mode) | Gets the gain control mode for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the gain control mode. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_fir_config (struct ad9361_rf_phy *phy, AD9361_RXFIRConfig fir_cfg) | Sets the FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the FIR filter configuration. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_fir_config(struct ad9361_rf_phy *phy, uint8_t rx_ch, AD9361_RXFIRConfig *fir_cfg) | Gets the RX FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state, the desired channel (RX1, RX2) and the location for storing the FIR filter configuration. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_fir_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_fir_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis) | Gets the status of the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_rfdc_track_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the RX RFDC Tracking. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE).Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_rfdc_track_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis) | Gets the status of the RX RFDC Tracking. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer.Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_bbdc_track_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the RX BasebandDC Tracking. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE).Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_bbdc_track_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis) | Gets the status of the RX BasebandDC Tracking. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer.Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_quad_track_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the RX Quadrature Tracking. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE).Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_quad_track_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis) | Gets the status of the RX Quadrature Tracking. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer.Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_rx_rf_port_input (struct ad9361_rf_phy *phy,uint32_t mode) | Sets the RX RF input port. Receives as parameters a structure that contains the AD9361 current state and the desired port (A_BALANCED, B_BALANCED, C_BALANCED, A_N, A_P, B_N, B_P, C_N, C_P, TX_MON1, TX_MON2, TX_MON1_2). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_rf_port_input (struct ad9361_rf_phy *phy,uint32_t *mode) | Gets the selected RX RF input port. Receives as parameters a structure that contains the AD9361 current state and the location to store the selected port value. Returns 0 in case of success, negative error code otherwise. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_rx_fastlock_store(struct ad9361_rf_phy *phy, uint32_t profile) | Stores RX fastlock profile. To create a profile tune the synthesizer (ad9361_set_rx_lo_freq()) and then call this function specifying the target profile number. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_rx_fastlock_recall(struct ad9361_rf_phy *phy, uint32_t profile) | Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param→rx_fastlock_pincontrol_enable), the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_rx_fastlock_load(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values) | Recalls specified RX fastlock profile. When in fastlock pin select mode (init_param→rx_fastlock_pincontrol_enable), the function needs to be called before then the pin-control can be used. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the Fastlock profile program data (val0,val1,val2,…,val15). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_rx_fastlock_save(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values) | Saves RX fastlock profile. In order to use more than 8 Profiles, an existing profile can be read back and stored by the user application. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the location for storing the profile data. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_rx_lo_powerdown(struct ad9361_rf_phy *phy, uint8_t option) | Powers down the RX Local Oscillator. Receives as parameters a structure that contains the AD9361 current state and the option (ON, OFF). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_rx_lo_power(struct ad9361_rf_phy *phy, uint8_t *option) | Gets the RX Local Oscillator power status. Receives as parameters a structure that contains the AD9361 current state and the location to store the selected option. Returns 0 in case of success, negative error code otherwise. |
Transmit Chain Settings | |
int32_t ad9361_set_tx_attenuation (struct ad9361_rf_phy *phy, uint8_t ch, uint32_t attenuation_mdb) | Sets the transmit attenuation for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel number (0, 1) and the attenuation in dB. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_attenuation (struct ad9361_rf_phy *phy, uint8_t ch, uint32_t *attenuation_mdb) | Gets current transmit attenuation for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the attenuation value in dB. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_rf_bandwidth (struct ad9361_rf_phy *phy, uint32_t bandwidth_hz) | Sets the RF bandwidth. Receives as parameters a structure that contains the AD9361 current state and the desired bandwidth in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_rf_bandwidth (struct ad9361_rf_phy *phy, uint32_t *bandwidth_hz) | Gets current RF bandwidth. Receives as parameters a structure that contains the AD9361 current state and a variable to store the bandwidth value in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_sampling_freq (struct ad9361_rf_phy *phy, uint32_t sampling_freq_hz) | Sets the sampling frequency. Receives as parameters a structure that contains the AD9361 current state and the desired sampling frequency in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_sampling_freq (struct ad9361_rf_phy *phy, uint32_t *sampling_freq_hz) | Gets current sampling frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the sampling frequency value in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_lo_freq (struct ad9361_rf_phy *phy, uint64_t lo_freq_hz) | Sets the LO frequency. Receives as parameters a structure that contains the AD9361 current state and the desired LO frequency in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_lo_freq (struct ad9361_rf_phy *phy, uint64_t *lo_freq_hz) | Gets current LO frequency. Receives as parameters a structure that contains the AD9361 current state and a variable to store the LO frequency value in Hz. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_lo_int_ext(struct ad9361_rf_phy *phy, uint8_t int_ext) | Switches between internal and external LO. Receives as parameters a structure that contains the AD9361 current state and the desired option (INT_LO, EXT_LO). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_fir_config (struct ad9361_rf_phy *phy, AD9361_TXFIRConfig fir_cfg) | Sets the FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the FIR filter configuration. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_fir_config(struct ad9361_rf_phy *phy, uint8_t tx_ch, AD9361_TXFIRConfig *fir_cfg) | Gets the TX FIR filter configuration. Receives as parameters a structure that contains the AD9361 current state and the location to store the FIR filter configuration. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_fir_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_fir_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis) | Gets the status of the FIR filter. Receives as parameters a structure that contains the AD9361 current state and the enable/disable status buffer. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_rssi (struct ad9361_rf_phy *phy, uint8_t ch, uint32_t *rssi_db_x_1000) | Gets the TX RSSI for the selected channel. Receives as parameters a structure that contains the AD9361 current state, the desired channel (0, 1) and a variable to store the RSSI. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_rf_port_output (struct ad9361_rf_phy *phy, uint32_t mode) | Sets the TX RF output port. Receives as parameters a structure that contains the AD9361 current state and the desired port (TXA, TXB). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_rf_port_output (struct ad9361_rf_phy *phy, uint32_t *mode) | Gets the selected TX RF output port. Receives as parameters a structure that contains the AD9361 current state and the location for storing the selected port. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_tx_auto_cal_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the auto calibration. Receives as parameters a structure that contains the AD9361 current state and the desired mode (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_auto_cal_en_dis (struct ad9361_rf_phy *phy, uint8_t *en_dis) | Gets the status of the auto calibration flag. Receives as parameters a structure that contains the AD9361 current state and the location for storing the selected mode. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_tx_fastlock_store(struct ad9361_rf_phy *phy, uint32_t profile) | Stores TX fastlock profile. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_tx_fastlock_recall(struct ad9361_rf_phy *phy, uint32_t profile) | Recalls specified TX fastlock profile. Receives as parameters a structure that contains the AD9361 current state and the profile number (0 - 7). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_tx_fastlock_load(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values) | Loads TX fastlock profile. A previously saved profile can be loaded in any of the 8 available slots. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the Fastlock profile program data (val0,val1,val2,…,val15). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_tx_fastlock_save(struct ad9361_rf_phy *phy, uint32_t profile, uint8_t *values) | Saves TX fastlock profile. In order to use more than 8 Profiles, an existing profile can be read back and stored by the user application. Receives as parameters a structure that contains the AD9361 current state, the profile number (0 - 7) and the location for storing the profile data. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_tx_lo_powerdown(struct ad9361_rf_phy *phy, uint8_t option) | Powers down the TX Local Oscillator. Receives as parameters a structure that contains the AD9361 current state and the desired option (ON, OFF). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_tx_lo_power(struct ad9361_rf_phy *phy, uint8_t *option) | Gets the TX Local Oscillator power status. Receives as parameters a structure that contains the AD9361 current state and the location to store the selected option. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_trx_path_clks (struct ad9361_rf_phy *phy, uint32_t *rx_path_clks, uint32_t *tx_path_clks) | Sets the RX and TX path rates. Receives as parameters a structure that contains the AD9361 current state, the RX and the TX clocks. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_trx_path_clks (struct ad9361_rf_phy *phy, uint32_t *rx_path_clks, uint32_t *tx_path_clks) | Gets the RX and TX path rates. Receives as parameters a structure that contains the AD9361 current state, the RX and the TX buffers to store the clock frequencies. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_no_ch_mode (struct ad9361_rf_phy *phy, uint8_t no_ch_mode) | Set the number of channels mode. Receives as parameters a structure that contains the AD9361 current state and the number of channels mode (1 - 1×1; 2 - 2×2). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_do_mcs(struct ad9361_rf_phy *phy_master, struct ad9361_rf_phy *phy_slave) | Do multi chip synchronization. Receives as parameters a structure that contains the AD9361 master current state and a structure that contains the AD9361 slave current state. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_trx_fir_en_dis (struct ad9361_rf_phy *phy, uint8_t en_dis) | Enables/disables the TRX FIR filters. Receives as parameters a structure that contains the AD9361 current state and the desired option (ENABLE, DISABLE). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_set_trx_rate_gov (struct ad9361_rf_phy *phy, uint32_t rate_gov) | Set the OSR rate governor. Receives as parameters a structure that contains the AD9361 current state and the desired OSR rate governor (HIGHEST_OSR, NOMINAL_OSR). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_trx_rate_gov (struct ad9361_rf_phy *phy, uint32_t *rate_gov) | Gets the OSR rate governor. Receives as parameters a structure that contains the AD9361 master current state and the location for storing the OSR rate governor. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_do_calib(struct ad9361_rf_phy *phy, uint32_t cal, int32_t arg) | Performs the selected calibration. Receives as parameters a structure that contains the AD9361 current state, the desired calibration (TX_QUAD_CAL, RFDC_CAL) and for TX_QUAD_CAL, the optional RX phase value overwrite (set to zero). Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_trx_load_enable_fir(struct ad9361_rf_phy *phy, AD9361_RXFIRConfig rx_fir_cfg, AD9361_TXFIRConfig tx_fir_cfg) | Loads and enables TRX FIR filters configurations. Receives as parameters a structure that contains the AD9361 current state, the RX FIR filter configuration and the TX FIR filter configuration. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_do_dcxo_tune_coarse(struct ad9361_rf_phy *phy, uint32_t coarse) | Does DCXO coarse tuning. Receives as parameters a structure that contains the AD9361 current state and the DCXO coarse tuning value. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_do_dcxo_tune_fine(struct ad9361_rf_phy *phy, uint32_t fine) | Does DCXO fine tuning. Receives as parameters a structure that contains the AD9361 current state and the DCXO fine tuning value. Returns 0 in case of success, negative error code otherwise. |
int32_t ad9361_get_temperature(struct ad9361_rf_phy *phy, int32_t *temp) | Gets the temperature. Receives as parameters a structure that contains the AD9361 current state and the location for storing the current temperature (degrees C * 1000). Returns 0 in case of success, negative error code otherwise. |
Notes: 1. Below is defined the AD9361_ParamInit structure used by the ad9361_init() function:
For more details on each of the struct members please see here: AD9361 Device Driver Customization
typedef struct { /* Device selection */ enum dev_id dev_sel; /* Identification number */ uint8_t id_no; /* Reference Clock */ uint32_t reference_clk_rate; /* Base Configuration */ uint8_t two_rx_two_tx_mode_enable; /* adi,2rx-2tx-mode-enable */ uint8_t one_rx_one_tx_mode_use_rx_num; /* adi,1rx-1tx-mode-use-rx-num */ uint8_t one_rx_one_tx_mode_use_tx_num; /* adi,1rx-1tx-mode-use-tx-num */ uint8_t frequency_division_duplex_mode_enable; /* adi,frequency-division-duplex-mode-enable */ uint8_t frequency_division_duplex_independent_mode_enable; /* adi,frequency-division-duplex-independent-mode-enable */ uint8_t tdd_use_dual_synth_mode_enable; /* adi,tdd-use-dual-synth-mode-enable */ uint8_t tdd_skip_vco_cal_enable; /* adi,tdd-skip-vco-cal-enable */ uint32_t tx_fastlock_delay_ns; /* adi,tx-fastlock-delay-ns */ uint32_t rx_fastlock_delay_ns; /* adi,rx-fastlock-delay-ns */ uint8_t rx_fastlock_pincontrol_enable; /* adi,rx-fastlock-pincontrol-enable */ uint8_t tx_fastlock_pincontrol_enable; /* adi,tx-fastlock-pincontrol-enable */ uint8_t external_rx_lo_enable; /* adi,external-rx-lo-enable */ uint8_t external_tx_lo_enable; /* adi,external-tx-lo-enable */ uint8_t dc_offset_tracking_update_event_mask; /* adi,dc-offset-tracking-update-event-mask */ uint8_t dc_offset_attenuation_high_range; /* adi,dc-offset-attenuation-high-range */ uint8_t dc_offset_attenuation_low_range; /* adi,dc-offset-attenuation-low-range */ uint8_t dc_offset_count_high_range; /* adi,dc-offset-count-high-range */ uint8_t dc_offset_count_low_range; /* adi,dc-offset-count-low-range */ uint8_t split_gain_table_mode_enable; /* adi,split-gain-table-mode-enable */ uint32_t trx_synthesizer_target_fref_overwrite_hz; /* adi,trx-synthesizer-target-fref-overwrite-hz */ uint8_t qec_tracking_slow_mode_enable; /* adi,qec-tracking-slow-mode-enable */ /* ENSM Control */ uint8_t ensm_enable_pin_pulse_mode_enable; /* adi,ensm-enable-pin-pulse-mode-enable */ uint8_t ensm_enable_txnrx_control_enable; /* adi,ensm-enable-txnrx-control-enable */ /* LO Control */ uint64_t rx_synthesizer_frequency_hz; /* adi,rx-synthesizer-frequency-hz */ uint64_t tx_synthesizer_frequency_hz; /* adi,tx-synthesizer-frequency-hz */ uint8_t tx_lo_powerdown_managed_enable; /* adi,tx-lo-powerdown-managed-enable */ /* Rate & BW Control */ uint32_t rx_path_clock_frequencies[6]; /* adi,rx-path-clock-frequencies */ uint32_t tx_path_clock_frequencies[6]; /* adi,tx-path-clock-frequencies */ uint32_t rf_rx_bandwidth_hz; /* adi,rf-rx-bandwidth-hz */ uint32_t rf_tx_bandwidth_hz; /* adi,rf-tx-bandwidth-hz */ /* RF Port Control */ uint32_t rx_rf_port_input_select; /* adi,rx-rf-port-input-select */ uint32_t tx_rf_port_input_select; /* adi,tx-rf-port-input-select */ /* TX Attenuation Control */ int32_t tx_attenuation_mdB; /* adi,tx-attenuation-mdB */ uint8_t update_tx_gain_in_alert_enable; /* adi,update-tx-gain-in-alert-enable */ /* Reference Clock Control */ uint8_t xo_disable_use_ext_refclk_enable; /* adi,xo-disable-use-ext-refclk-enable */ uint32_t dcxo_coarse_and_fine_tune[2]; /* adi,dcxo-coarse-and-fine-tune */ uint32_t clk_output_mode_select; /* adi,clk-output-mode-select */ /* Gain Control */ uint8_t gc_rx1_mode; /* adi,gc-rx1-mode */ uint8_t gc_rx2_mode; /* adi,gc-rx2-mode */ uint8_t gc_adc_large_overload_thresh; /* adi,gc-adc-large-overload-thresh */ uint8_t gc_adc_ovr_sample_size; /* adi,gc-adc-ovr-sample-size */ uint8_t gc_adc_small_overload_thresh; /* adi,gc-adc-small-overload-thresh */ uint16_t gc_dec_pow_measurement_duration; /* adi,gc-dec-pow-measurement-duration */ uint8_t gc_dig_gain_enable; /* adi,gc-dig-gain-enable */ uint16_t gc_lmt_overload_high_thresh; /* adi,gc-lmt-overload-high-thresh */ uint16_t gc_lmt_overload_low_thresh; /* adi,gc-lmt-overload-low-thresh */ uint8_t gc_low_power_thresh; /* adi,gc-low-power-thresh */ uint8_t gc_max_dig_gain; /* adi,gc-max-dig-gain */ /* Gain MGC Control */ uint8_t mgc_dec_gain_step; /* adi,mgc-dec-gain-step */ uint8_t mgc_inc_gain_step; /* adi,mgc-inc-gain-step */ uint8_t mgc_rx1_ctrl_inp_enable; /* adi,mgc-rx1-ctrl-inp-enable */ uint8_t mgc_rx2_ctrl_inp_enable; /* adi,mgc-rx2-ctrl-inp-enable */ uint8_t mgc_split_table_ctrl_inp_gain_mode; /* adi,mgc-split-table-ctrl-inp-gain-mode */ /* Gain AGC Control */ uint8_t agc_adc_large_overload_exceed_counter; /* adi,agc-adc-large-overload-exceed-counter */ uint8_t agc_adc_large_overload_inc_steps; /* adi,agc-adc-large-overload-inc-steps */ uint8_t agc_adc_lmt_small_overload_prevent_gain_inc_enable; /* adi,agc-adc-lmt-small-overload-prevent-gain-inc-enable */ uint8_t agc_adc_small_overload_exceed_counter; /* adi,agc-adc-small-overload-exceed-counter */ uint8_t agc_dig_gain_step_size; /* adi,agc-dig-gain-step-size */ uint8_t agc_dig_saturation_exceed_counter; /* adi,agc-dig-saturation-exceed-counter */ uint32_t agc_gain_update_interval_us; /* adi,agc-gain-update-interval-us */ uint8_t agc_immed_gain_change_if_large_adc_overload_enable; /* adi,agc-immed-gain-change-if-large-adc-overload-enable */ uint8_t agc_immed_gain_change_if_large_lmt_overload_enable; /* adi,agc-immed-gain-change-if-large-lmt-overload-enable */ uint8_t agc_inner_thresh_high; /* adi,agc-inner-thresh-high */ uint8_t agc_inner_thresh_high_dec_steps; /* adi,agc-inner-thresh-high-dec-steps */ uint8_t agc_inner_thresh_low; /* adi,agc-inner-thresh-low */ uint8_t agc_inner_thresh_low_inc_steps; /* adi,agc-inner-thresh-low-inc-steps */ uint8_t agc_lmt_overload_large_exceed_counter; /* adi,agc-lmt-overload-large-exceed-counter */ uint8_t agc_lmt_overload_large_inc_steps; /* adi,agc-lmt-overload-large-inc-steps */ uint8_t agc_lmt_overload_small_exceed_counter; /* adi,agc-lmt-overload-small-exceed-counter */ uint8_t agc_outer_thresh_high; /* adi,agc-outer-thresh-high */ uint8_t agc_outer_thresh_high_dec_steps; /* adi,agc-outer-thresh-high-dec-steps */ uint8_t agc_outer_thresh_low; /* adi,agc-outer-thresh-low */ uint8_t agc_outer_thresh_low_inc_steps; /* adi,agc-outer-thresh-low-inc-steps */ uint32_t agc_attack_delay_extra_margin_us; /* adi,agc-attack-delay-extra-margin-us */ uint8_t agc_sync_for_gain_counter_enable; /* adi,agc-sync-for-gain-counter-enable */ /* Fast AGC */ uint32_t fagc_dec_pow_measuremnt_duration; /* adi,fagc-dec-pow-measurement-duration */ uint32_t fagc_state_wait_time_ns; /* adi,fagc-state-wait-time-ns */ /* Fast AGC - Low Power */ uint8_t fagc_allow_agc_gain_increase; /* adi,fagc-allow-agc-gain-increase-enable */ uint32_t fagc_lp_thresh_increment_time; /* adi,fagc-lp-thresh-increment-time */ uint32_t fagc_lp_thresh_increment_steps; /* adi,fagc-lp-thresh-increment-steps */ /* Fast AGC - Lock Level (Lock Level is set via slow AGC inner high threshold) */ uint8_t fagc_lock_level_lmt_gain_increase_en; /* adi,fagc-lock-level-lmt-gain-increase-enable */ uint32_t fagc_lock_level_gain_increase_upper_limit; /* adi,fagc-lock-level-gain-increase-upper-limit */ /* Fast AGC - Peak Detectors and Final Settling */ uint32_t fagc_lpf_final_settling_steps; /* adi,fagc-lpf-final-settling-steps */ uint32_t fagc_lmt_final_settling_steps; /* adi,fagc-lmt-final-settling-steps */ uint32_t fagc_final_overrange_count; /* adi,fagc-final-overrange-count */ /* Fast AGC - Final Power Test */ uint8_t fagc_gain_increase_after_gain_lock_en; /* adi,fagc-gain-increase-after-gain-lock-enable */ /* Fast AGC - Unlocking the Gain */ uint32_t fagc_gain_index_type_after_exit_rx_mode; /* adi,fagc-gain-index-type-after-exit-rx-mode */ uint8_t fagc_use_last_lock_level_for_set_gain_en; /* adi,fagc-use-last-lock-level-for-set-gain-enable */ uint8_t fagc_rst_gla_stronger_sig_thresh_exceeded_en; /* adi,fagc-rst-gla-stronger-sig-thresh-exceeded-enable */ uint32_t fagc_optimized_gain_offset; /* adi,fagc-optimized-gain-offset */ uint32_t fagc_rst_gla_stronger_sig_thresh_above_ll; /* adi,fagc-rst-gla-stronger-sig-thresh-above-ll */ uint8_t fagc_rst_gla_engergy_lost_sig_thresh_exceeded_en; /* adi,fagc-rst-gla-engergy-lost-sig-thresh-exceeded-enable */ uint8_t fagc_rst_gla_engergy_lost_goto_optim_gain_en; /* adi,fagc-rst-gla-engergy-lost-goto-optim-gain-enable */ uint32_t fagc_rst_gla_engergy_lost_sig_thresh_below_ll; /* adi,fagc-rst-gla-engergy-lost-sig-thresh-below-ll */ uint32_t fagc_energy_lost_stronger_sig_gain_lock_exit_cnt; /* adi,fagc-energy-lost-stronger-sig-gain-lock-exit-cnt */ uint8_t fagc_rst_gla_large_adc_overload_en; /* adi,fagc-rst-gla-large-adc-overload-enable */ uint8_t fagc_rst_gla_large_lmt_overload_en; /* adi,fagc-rst-gla-large-lmt-overload-enable */ uint8_t fagc_rst_gla_en_agc_pulled_high_en; /* adi,fagc-rst-gla-en-agc-pulled-high-enable */ uint32_t fagc_rst_gla_if_en_agc_pulled_high_mode; /* adi,fagc-rst-gla-if-en-agc-pulled-high-mode */ uint32_t fagc_power_measurement_duration_in_state5; /* adi,fagc-power-measurement-duration-in-state5 */ /* RSSI Control */ uint32_t rssi_delay; /* adi,rssi-delay */ uint32_t rssi_duration; /* adi,rssi-duration */ uint8_t rssi_restart_mode; /* adi,rssi-restart-mode */ uint8_t rssi_unit_is_rx_samples_enable; /* adi,rssi-unit-is-rx-samples-enable */ uint32_t rssi_wait; /* adi,rssi-wait */ /* Aux ADC Control */ uint32_t aux_adc_decimation; /* adi,aux-adc-decimation */ uint32_t aux_adc_rate; /* adi,aux-adc-rate */ /* AuxDAC Control */ uint8_t aux_dac_manual_mode_enable; /* adi,aux-dac-manual-mode-enable */ uint32_t aux_dac1_default_value_mV; /* adi,aux-dac1-default-value-mV */ uint8_t aux_dac1_active_in_rx_enable; /* adi,aux-dac1-active-in-rx-enable */ uint8_t aux_dac1_active_in_tx_enable; /* adi,aux-dac1-active-in-tx-enable */ uint8_t aux_dac1_active_in_alert_enable; /* adi,aux-dac1-active-in-alert-enable */ uint32_t aux_dac1_rx_delay_us; /* adi,aux-dac1-rx-delay-us */ uint32_t aux_dac1_tx_delay_us; /* adi,aux-dac1-tx-delay-us */ uint32_t aux_dac2_default_value_mV; /* adi,aux-dac2-default-value-mV */ uint8_t aux_dac2_active_in_rx_enable; /* adi,aux-dac2-active-in-rx-enable */ uint8_t aux_dac2_active_in_tx_enable; /* adi,aux-dac2-active-in-tx-enable */ uint8_t aux_dac2_active_in_alert_enable; /* adi,aux-dac2-active-in-alert-enable */ uint32_t aux_dac2_rx_delay_us; /* adi,aux-dac2-rx-delay-us */ uint32_t aux_dac2_tx_delay_us; /* adi,aux-dac2-tx-delay-us */ /* Temperature Sensor Control */ uint32_t temp_sense_decimation; /* adi,temp-sense-decimation */ uint16_t temp_sense_measurement_interval_ms; /* adi,temp-sense-measurement-interval-ms */ int8_t temp_sense_offset_signed; /* adi,temp-sense-offset-signed */ uint8_t temp_sense_periodic_measurement_enable; /* adi,temp-sense-periodic-measurement-enable */ /* Control Out Setup */ uint8_t ctrl_outs_enable_mask; /* adi,ctrl-outs-enable-mask */ uint8_t ctrl_outs_index; /* adi,ctrl-outs-index */ /* External LNA Control */ uint32_t elna_settling_delay_ns; /* adi,elna-settling-delay-ns */ uint32_t elna_gain_mdB; /* adi,elna-gain-mdB */ uint32_t elna_bypass_loss_mdB; /* adi,elna-bypass-loss-mdB */ uint8_t elna_rx1_gpo0_control_enable; /* adi,elna-rx1-gpo0-control-enable */ uint8_t elna_rx2_gpo1_control_enable; /* adi,elna-rx2-gpo1-control-enable */ uint8_t elna_gaintable_all_index_enable; /* adi,elna-gaintable-all-index-enable */ /* Digital Interface Control */ uint8_t digital_interface_tune_skip_mode; /* adi,digital-interface-tune-skip-mode */ uint8_t digital_interface_tune_fir_disable; /* adi,digital-interface-tune-fir-disable */ uint8_t pp_tx_swap_enable; /* adi,pp-tx-swap-enable */ uint8_t pp_rx_swap_enable; /* adi,pp-rx-swap-enable */ uint8_t tx_channel_swap_enable; /* adi,tx-channel-swap-enable */ uint8_t rx_channel_swap_enable; /* adi,rx-channel-swap-enable */ uint8_t rx_frame_pulse_mode_enable; /* adi,rx-frame-pulse-mode-enable */ uint8_t two_t_two_r_timing_enable; /* adi,2t2r-timing-enable */ uint8_t invert_data_bus_enable; /* adi,invert-data-bus-enable */ uint8_t invert_data_clk_enable; /* adi,invert-data-clk-enable */ uint8_t fdd_alt_word_order_enable; /* adi,fdd-alt-word-order-enable */ uint8_t invert_rx_frame_enable; /* adi,invert-rx-frame-enable */ uint8_t fdd_rx_rate_2tx_enable; /* adi,fdd-rx-rate-2tx-enable */ uint8_t swap_ports_enable; /* adi,swap-ports-enable */ uint8_t single_data_rate_enable; /* adi,single-data-rate-enable */ uint8_t lvds_mode_enable; /* adi,lvds-mode-enable */ uint8_t half_duplex_mode_enable; /* adi,half-duplex-mode-enable */ uint8_t single_port_mode_enable; /* adi,single-port-mode-enable */ uint8_t full_port_enable; /* adi,full-port-enable */ uint8_t full_duplex_swap_bits_enable; /* adi,full-duplex-swap-bits-enable */ uint32_t delay_rx_data; /* adi,delay-rx-data */ uint32_t rx_data_clock_delay; /* adi,rx-data-clock-delay */ uint32_t rx_data_delay; /* adi,rx-data-delay */ uint32_t tx_fb_clock_delay; /* adi,tx-fb-clock-delay */ uint32_t tx_data_delay; /* adi,tx-data-delay */ uint32_t lvds_bias_mV; /* adi,lvds-bias-mV */ uint8_t lvds_rx_onchip_termination_enable; /* adi,lvds-rx-onchip-termination-enable */ uint8_t rx1rx2_phase_inversion_en; /* adi,rx1-rx2-phase-inversion-enable */ uint8_t lvds_invert1_control; /* adi,lvds-invert1-control */ uint8_t lvds_invert2_control; /* adi,lvds-invert2-control */ /* GPO Control */ uint8_t gpo0_inactive_state_high_enable; /* adi,gpo0-inactive-state-high-enable */ uint8_t gpo1_inactive_state_high_enable; /* adi,gpo1-inactive-state-high-enable */ uint8_t gpo2_inactive_state_high_enable; /* adi,gpo2-inactive-state-high-enable */ uint8_t gpo3_inactive_state_high_enable; /* adi,gpo3-inactive-state-high-enable */ uint8_t gpo0_slave_rx_enable; /* adi,gpo0-slave-rx-enable */ uint8_t gpo0_slave_tx_enable; /* adi,gpo0-slave-tx-enable */ uint8_t gpo1_slave_rx_enable; /* adi,gpo1-slave-rx-enable */ uint8_t gpo1_slave_tx_enable; /* adi,gpo1-slave-tx-enable */ uint8_t gpo2_slave_rx_enable; /* adi,gpo2-slave-rx-enable */ uint8_t gpo2_slave_tx_enable; /* adi,gpo2-slave-tx-enable */ uint8_t gpo3_slave_rx_enable; /* adi,gpo3-slave-rx-enable */ uint8_t gpo3_slave_tx_enable; /* adi,gpo3-slave-tx-enable */ uint8_t gpo0_rx_delay_us; /* adi,gpo0-rx-delay-us */ uint8_t gpo0_tx_delay_us; /* adi,gpo0-tx-delay-us */ uint8_t gpo1_rx_delay_us; /* adi,gpo1-rx-delay-us */ uint8_t gpo1_tx_delay_us; /* adi,gpo1-tx-delay-us */ uint8_t gpo2_rx_delay_us; /* adi,gpo2-rx-delay-us */ uint8_t gpo2_tx_delay_us; /* adi,gpo2-tx-delay-us */ uint8_t gpo3_rx_delay_us; /* adi,gpo3-rx-delay-us */ uint8_t gpo3_tx_delay_us; /* adi,gpo3-tx-delay-us */ /* Tx Monitor Control */ uint32_t low_high_gain_threshold_mdB; /* adi,txmon-low-high-thresh */ uint32_t low_gain_dB; /* adi,txmon-low-gain */ uint32_t high_gain_dB; /* adi,txmon-high-gain */ uint8_t tx_mon_track_en; /* adi,txmon-dc-tracking-enable */ uint8_t one_shot_mode_en; /* adi,txmon-one-shot-mode-enable */ uint32_t tx_mon_delay; /* adi,txmon-delay */ uint32_t tx_mon_duration; /* adi,txmon-duration */ uint32_t tx1_mon_front_end_gain; /* adi,txmon-1-front-end-gain */ uint32_t tx2_mon_front_end_gain; /* adi,txmon-2-front-end-gain */ uint32_t tx1_mon_lo_cm; /* adi,txmon-1-lo-cm */ uint32_t tx2_mon_lo_cm; /* adi,txmon-2-lo-cm */ /* GPIO definitions */ int32_t gpio_resetb; /* reset-gpios */ /* MCS Sync */ int32_t gpio_sync; /* sync-gpios */ int32_t gpio_cal_sw1; /* cal-sw1-gpios */ int32_t gpio_cal_sw2; /* cal-sw2-gpios */ /* External LO clocks */ uint32_t (*ad9361_rfpll_ext_recalc_rate)(struct refclk_scale *clk_priv); int32_t (*ad9361_rfpll_ext_round_rate)(struct refclk_scale *clk_priv, uint32_t rate); int32_t (*ad9361_rfpll_ext_set_rate)(struct refclk_scale *clk_priv, uint32_t rate); }AD9361_InitParam;
2. Below is defined the rf_rssi structure used by the ad9361_get_rx_rssi() function:
struct rf_rssi { u32 ant; // Antenna number for which RSSI is reported u32 symbol; // Runtime RSSI u32 preamble; // Initial RSSI s32 multiplier; // Multiplier to convert reported RSSI u8 duration; // Duration to be considered for measuring };
3. Below is defined the AD9361_RXFIRConfig structure used by the ad9361_set_rx_fir_config() function:
typedef struct { uint32_t rx; // 1, 2, 3(both) int32_t rx_gain; // -12, -6, 0, 6 uint32_t rx_dec; // 1, 2, 4 int16_t rx_coef[64]; }AD9361_RXFIRConfig;
4. Below is defined the AD9361_TXFIRConfig structure used by the ad9361_set_tx_fir_config() function:
typedef struct { uint32_t tx; // 1, 2, 3(both) int32_t tx_gain; // -6, 0 uint32_t tx_int; // 1, 2, 4 int16_t tx_coef[64]; }AD9361_TXFIRConfig;
The AD9361 No-OS Software together with the Generic Platform Driver can be used as a base for any microprocessor platform.
The Platform Driver implements the communication with the device and hides the actual details of the communication protocol to the AD9361 driver. When the desired type of processor is chosen, the specific communication functions have to be implemented.
The following information was obtained compiling the AD9361 project (with the Generic Platform Driver integrated) using the gcc v4.7.2 and the Optimize for size (-Os) option enabled.
text data bss dec hex filename 45159 1624 24 46807 b6d7 ad9361_generic
Note: The source code from the GitHub SHA 13c1ba56164f4b63844f63e5dd596286b6faf8b3 was used for calculating the code size information (https://github.com/analogdevicesinc/no-OS/tree/13c1ba56164f4b63844f63e5dd596286b6faf8b3/ad9361/sw).
This guide provides some quick instructions on how to setup the AD-FMCOMMS2-EBZ on either:
The ML605 XPS project remain on this website only for legacy purposes. The support for XPS projects has been discontinued.
//#define XILINX #define ALTERA
The Console Commands Driver is optional for the project. It was created in addition to the AD9361 driver to control the part using some console commands.
The following commands were implemented for controlling the AD9361:
Command | Description |
---|---|
help? | Displays all available commands. |
register? | Gets the specified register value. |
tx_lo_freq? | Gets current TX LO frequency [MHz]. |
tx_lo_freq= | Sets the TX LO frequency [MHz]. |
tx_samp_freq? | Gets current TX sampling frequency [Hz]. |
tx_samp_freq= | Sets the TX sampling frequency [Hz]. |
tx_rf_bandwidth? | Gets current TX RF bandwidth [Hz]. |
tx_rf_bandwidth= | Sets the TX RF bandwidth [Hz]. |
tx1_attenuation? | Gets current TX1 attenuation [mdB]. |
tx1_attenuation= | Sets the TX1 attenuation [mdB]. |
tx2_attenuation? | Gets current TX2 attenuation [mdB]. |
tx2_attenuation= | Sets the TX2 attenuation [mdB]. |
tx_fir_en? | Gets current TX FIR state. |
tx_fir_en= | Sets the TX FIR state. |
rx_lo_freq? | Gets current RX LO frequency [MHz]. |
rx_lo_freq= | Sets the RX LO frequency [MHz]. |
rx_samp_freq? | Gets current RX sampling frequency [Hz]. |
rx_samp_freq= | Sets the RX sampling frequency [Hz]. |
rx_rf_bandwidth? | Gets current RX RF bandwidth [Hz]. |
rx_rf_bandwidth= | Sets the RX RF bandwidth [Hz]. |
rx1_gc_mode? | Gets current RX1 GC mode. |
rx1_gc_mode= | Sets the RX1 GC mode. |
rx2_gc_mode? | Gets current RX2 GC mode. |
rx2_gc_mode= | Sets the RX2 GC mode. |
rx1_rf_gain? | Gets current RX1 RF gain. |
rx1_rf_gain= | Sets the RX1 RF gain. |
rx2_rf_gain? | Gets current RX2 RF gain. |
rx2_rf_gain= | Sets the RX2 RF gain. |
rx_fir_en? | Gets current RX FIR state. |
rx_fir_en= | Sets the RX FIR state. |
dds_tx1_f1_freq? | Gets current DDS TX1 F1 frequency [MHz]. |
dds_tx1_f1_freq= | Sets the DDS TX1 F1 frequency [MHz]. |
dds_tx1_f2_freq? | Gets current DDS TX1 F2 frequency [MHz]. |
dds_tx1_f2_freq= | Sets the DDS TX1 F2 frequency [MHz]. |
dds_tx1_f1_phase? | Gets current DDS TX1 F1 phase [degrees]. |
dds_tx1_f1_phase= | Sets the DDS TX1 F1 phase [degrees]. |
dds_tx1_f2_phase? | Gets current DDS TX1 F2 phase [degrees]. |
dds_tx1_f2_phase= | Sets the DDS TX1 F2 phase [degrees]. |
dds_tx1_f1_scale? | Gets current DDS TX1 F1 scale. |
dds_tx1_f1_scale= | Sets the DDS TX1 F1 scale. |
dds_tx1_f2_scale? | Gets current DDS TX1 F2 scale. |
dds_tx1_f2_scale= | Sets the DDS TX1 F2 scale. |
dds_tx2_f1_freq? | Gets current DDS TX2 F1 frequency [MHz]. |
dds_tx2_f1_freq= | Sets the DDS TX2 F1 frequency [MHz]. |
dds_tx2_f2_freq? | Gets current DDS TX2 F2 frequency [MHz]. |
dds_tx2_f2_freq= | Sets the DDS TX2 F2 frequency [MHz]. |
dds_tx2_f1_phase? | Gets current DDS TX2 F1 phase [degrees]. |
dds_tx2_f1_phase= | Sets the DDS TX2 F1 phase [degrees]. |
dds_tx2_f2_phase? | Gets current DDS TX2 F2 phase [degrees]. |
dds_tx2_f2_phase= | Sets the DDS TX2 F2 phase [degrees]. |
dds_tx2_f1_scale? | Gets current DDS TX2 F1 scale. |
dds_tx2_f1_scale= | Sets the DDS TX2 F1 scale. |
dds_tx2_f2_scale? | Gets current DDS TX2 F2 scale. |
dds_tx2_f2_scale= | Sets the DDS TX2 F2 scale. |
Commands can be executed using a serial terminal connected to the UART peripheral of the development board.
The following image shows an example of how the TX LO frequency can be set to 2.4 GHz using the corresponding command.
The source code of the no-OS software and the scripts can be downloaded from the Analog Devices github.
no-OS Software
HDL Reference Designs for FMCOMMS2
HDL Reference Designs for FMCOMMS5