This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:reference_hdl [15 Mar 2016 15:15] – make things a little more generic Robin Getz | resources:eval:user-guides:ad-fmcomms2-ebz:reference_hdl [01 Feb 2023 02:07] (current) – Replaced the obsolete Kuiper Linux page link; repaired broken links Joyce Velasco | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | |||
====== AD9361 HDL Reference Designs ====== | ====== AD9361 HDL Reference Designs ====== | ||
Line 37: | Line 36: | ||
* [[adi> | * [[adi> | ||
* [[../ | * [[../ | ||
+ | * [[../ | ||
===== Supported Carriers ===== | ===== Supported Carriers ===== | ||
Line 55: | Line 55: | ||
* [[https:// | * [[https:// | ||
- | ===== Download ====== | + | ===== Download |
- | FPGA Reference Designs on GitHub : | + | <WRAP round info 100%> |
- | + | ||
- | <WRAP round info 80%> | + | |
Please note that the projects **FMCOMMS2**, | Please note that the projects **FMCOMMS2**, | ||
- | + | The **ARRADIO** Quartus project uses [[https:// | |
- | The **ARRADIO** Quartus project uses [[https:// | + | |
- | </ | + | |
- | <WRAP round download 80%> | + | |
- | **Vivado / Quartus Downloads** | + | |
- | * Main repository with latest changes (always synced with the latest release) | + | |
- | * https:// | + | |
- | * Releases (the used tool version can be found in README.md) | + | |
- | * https:// | + | |
- | * https:// | + | |
- | * https:// | + | |
</ | </ | ||
+ | |||
+ | {{page>/ | ||
+ | {{page>/ | ||
+ | {{page>/ | ||
<WRAP round help 80%> | <WRAP round help 80%> | ||
- | * Questions? [[https:// | + | * Questions? [[/ |
</ | </ | ||
===== Generating Xilinx netlist files ====== | ===== Generating Xilinx netlist files ====== | ||
- | The repository will not contain Xilinx netlist files, only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[http:// | + | The repository will not contain Xilinx netlist files, only Xilinx coregen xco files are provided with the reference design. You must regenerate the IP core files using this file. See [[/ |
- | {{navigation AD-FMCOMMS2-EBZ# |