This is an old revision of the document!
This guide provides some quick instructions (still takes awhile to download, and set things up) on how to setup the AD-FMCOMMS2-EBZ on:
Instructions on how to build the ZynqMP / MPSoC Linux kernel and devicetrees from source can be found here:
This specifies any shell prompt running on the target
Xilinx Zynq MP First Stage Boot Loader Release 2017.2 Oct 19 2017 - 09:35:44 NOTICE: ATF running on XCZU9EG/silicon v4/RTL5.1 at 0xfffea000, with PMU firmware NOTICE: BL31: Secure code at 0x0 NOTICE: BL31: Non secure code at 0x8000000 NOTICE: BL31: v1.3(release):f9b244b NOTICE: BL31: Built : 09:35:17, Oct 19 2017 U-Boot 2016.07 (Dec 16 2016 - 15:04:11 -0700) Xilinx ZynqMP ZCU102 revB I2C: ready DRAM: 4 GiB EL Level: EL2 Chip ID: xczu9eg MMC: sdhci@ff170000: 0 Using default environment In: serial@ff000000 Out: serial@ff000000 Err: serial@ff000000 Bootmode: LVL_SHFT_SD_MODE1 SCSI: SATA link 0 timeout. SATA link 1 timeout. AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl SATA mode flags: 64bit ncq pm clo only pmp fbss pio slum part ccc apst scanning bus for devices... Found 0 device(s). Net: ZYNQ GEM: ff0e0000, phyaddr 12, interface rgmii-id Warning: ethernet@ff0e0000 using MAC address from ROM eth0: ethernet@ff0e0000 Hit any key to stop autoboot: 0 switch to partitions #0, OK mmc0 is current device Device: sdhci@ff170000 Manufacturer ID: 3 OEM: 5344 Name: SL08G Tran Speed: 50000000 Rd Block Len: 512 SD version 3.0 High Capacity: Yes Capacity: 7.4 GiB Bus Width: 4-bit Erase Group Size: 512 Bytes reading uEnv.txt 301 bytes read in 9 ms (32.2 KiB/s) Loaded environment from uEnv.txt Importing environment from SD ... Running uenvcmd ... reading Image 14209536 bytes read in 991 ms (13.7 MiB/s) reading system.dtb 43396 bytes read in 48 ms (882.8 KiB/s) Wrong Image Format for bootm command ERROR: can't get kernel image! reading system.dtb 43396 bytes read in 49 ms (864.3 KiB/s) reading Image 14209536 bytes read in 987 ms (13.7 MiB/s) ## Flattened Device Tree blob at 04000000 Booting using the fdt blob at 0x4000000 Loading Device Tree to 000000000fff2000, end 000000000ffff983 ... OK Starting kernel ... [ 0.000000] Booting Linux on physical CPU 0x0 [ 0.000000] Linux version 4.9.0-12434-g7f38ed6 (michael@mhenneri-D04) (gcc version 4.9.2 20140904 (prerelease) (crosstool-NG linaro-1.13.1-4.9-2014.09 - Linaro GCC 4.9-2014.09) ) #387 SMP Thu Oct 19 10 :59:25 CEST 2017 [ 0.000000] Boot CPU: AArch64 Processor [410fd034] [ 0.000000] earlycon: cdns0 at MMIO 0x00000000ff000000 (options '115200n8') [ 0.000000] bootconsole [cdns0] enabled [ 0.000000] efi: Getting EFI parameters from FDT: [ 0.000000] efi: UEFI not found. [ 0.000000] cma: Reserved 128 MiB at 0x0000000078000000 [ 0.000000] psci: probing for conduit method from DT. [ 0.000000] psci: PSCIv1.0 detected in firmware. [ 0.000000] psci: Using standard PSCI v0.2 function IDs [ 0.000000] psci: MIGRATE_INFO_TYPE not supported. [ 0.000000] percpu: Embedded 21 pages/cpu @ffffffc87ff62000 s47488 r8192 d30336 u86016 [ 0.000000] Detected VIPT I-cache on CPU0 [ 0.000000] CPU features: enabling workaround for ARM erratum 845719 [ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 1034240 [ 0.000000] Kernel command line: earlycon=cdns,mmio,0xFF000000,115200n8 console=ttyPS0,115200n8 root=/dev/mmcblk0p2 rw rootwait cma=128M root=/dev/mmcblk0p2 rw rootwait [ 0.000000] PID hash table entries: 4096 (order: 3, 32768 bytes) [ 0.000000] Dentry cache hash table entries: 524288 (order: 10, 4194304 bytes) [ 0.000000] Inode-cache hash table entries: 262144 (order: 9, 2097152 bytes) [ 0.000000] software IO TLB [mem 0x73fff000-0x77fff000] (64MB) mapped at [ffffffc073fff000-ffffffc077ffefff] [ 0.000000] Memory: 3918800K/4194304K available (9148K kernel code, 628K rwdata, 3524K rodata, 512K init, 389K bss, 144432K reserved, 131072K cma-reserved) [ 0.000000] Virtual kernel memory layout: [ 0.000000] modules : 0xffffff8000000000 - 0xffffff8008000000 ( 128 MB) [ 0.000000] vmalloc : 0xffffff8008000000 - 0xffffffbebfff0000 ( 250 GB) [ 0.000000] .text : 0xffffff8008080000 - 0xffffff8008970000 ( 9152 KB) [ 0.000000] .rodata : 0xffffff8008970000 - 0xffffff8008cf0000 ( 3584 KB) [ 0.000000] .init : 0xffffff8008cf0000 - 0xffffff8008d70000 ( 512 KB) [ 0.000000] .data : 0xffffff8008d70000 - 0xffffff8008e0d200 ( 629 KB) [ 0.000000] .bss : 0xffffff8008e0d200 - 0xffffff8008e6e7e0 ( 390 KB) [ 0.000000] fixed : 0xffffffbefe7fd000 - 0xffffffbefec00000 ( 4108 KB) [ 0.000000] PCI I/O : 0xffffffbefee00000 - 0xffffffbeffe00000 ( 16 MB) [ 0.000000] vmemmap : 0xffffffbf00000000 - 0xffffffc000000000 ( 4 GB maximum) [ 0.000000] 0xffffffbf00000000 - 0xffffffbf1dc00000 ( 476 MB actual) [ 0.000000] memory : 0xffffffc000000000 - 0xffffffc880000000 ( 34816 MB) [ 0.000000] Hierarchical RCU implementation. [ 0.000000] Build-time adjustment of leaf fanout to 64. [ 0.000000] RCU restricting CPUs from NR_CPUS=8 to nr_cpu_ids=4. [ 0.000000] RCU: Adjusting geometry for rcu_fanout_leaf=64, nr_cpu_ids=4 [ 0.000000] NR_IRQS:64 nr_irqs:64 0 [ 0.000000] GIC: Adjusting CPU interface base to 0x00000000f902f000 [ 0.000000] GIC: Using split EOI/Deactivate mode [ 0.000000] arm_arch_timer: Architected cp15 timer(s) running at 99.99MHz (phys). [ 0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x171015c90f, max_idle_ns: 440795203080 ns [ 0.000003] sched_clock: 56 bits at 99MHz, resolution 10ns, wraps every 4398046511101ns [ 0.008295] Console: colour dummy device 80x25 [ 0.012559] Calibrating delay loop (skipped), value calculated using timer frequency.. 199.99 BogoMIPS (lpj=399996) [ 0.022922] pid_max: default: 32768 minimum: 301 [ 0.027604] Mount-cache hash table entries: 8192 (order: 4, 65536 bytes) [ 0.034174] Mountpoint-cache hash table entries: 8192 (order: 4, 65536 bytes) [ 0.041780] ASID allocator initialised with 65536 entries [ 0.047510] zynqmp_plat_init Power management API v0.3 [ 0.052529] EFI services will not be available. [ 0.057272] Detected VIPT I-cache on CPU1 [ 0.057298] CPU1: Booted secondary processor [410fd034] [ 0.057558] Detected VIPT I-cache on CPU2 [ 0.057576] CPU2: Booted secondary processor [410fd034] [ 0.057833] Detected VIPT I-cache on CPU3 [ 0.057851] CPU3: Booted secondary processor [410fd034] [ 0.057886] Brought up 4 CPUs [ 0.088169] SMP: Total of 4 processors activated. [ 0.092846] CPU features: detected feature: 32-bit EL0 Support [ 0.098643] CPU: All CPU(s) started at EL2 [ 0.102714] alternatives: patching kernel code [ 0.107781] devtmpfs: initialized [ 0.116903] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns [ 0.129064] xor: measuring software checksum speed [ 0.173723] 8regs : 2376.000 MB/sec [ 0.213751] 8regs_prefetch: 2170.000 MB/sec [ 0.258121] 32regs : 2632.000 MB/sec [ 0.298150] 32regs_prefetch: 2459.000 MB/sec [ 0.302575] xor: using function: 32regs (2632.000 MB/sec) [ 0.308002] pinctrl core: initialized pinctrl subsystem [ 0.313634] NET: Registered protocol family 16 [ 0.333916] cpuidle: using governor menu [ 0.338003] Failed to initialise IOMMU /amba/smmu@fd800000 [ 0.343528] vdso: 2 pages (1 code @ ffffff8008977000, 1 data @ ffffff8008d74000) [ 0.350728] hw-breakpoint: found 6 breakpoint and 4 watchpoint registers. [ 0.357908] DMA: preallocated 256 KiB pool for atomic allocations [ 0.378184] reset_zynqmp reset-controller: Xilinx zynqmp reset driver probed [ 0.385780] ARM CCI_400_r1 PMU driver probed[ 0.392280] zynqmp-pinctrl ff180000.pinctrl: zynqmp pinctrl initialized [ 0.418915] HugeTLB registered 2 MB page size, pre-allocated 0 pages [ 0.493298] raid6: int64x1 gen() 458 MB/s [ 0.565380] raid6: int64x1 xor() 478 MB/s [ 0.637451] raid6: int64x2 gen() 676 MB/s [ 0.709444] raid6: int64x2 xor() 597 MB/s [ 0.781506] raid6: int64x4 gen() 981 MB/s [ 0.853541] raid6: int64x4 xor() 733 MB/s [ 0.925631] raid6: int64x8 gen() 1021 MB/s [ 0.997656] raid6: int64x8 xor() 722 MB/s [ 1.069712] raid6: neonx1 gen() 732 MB/s [ 1.141750] raid6: neonx1 xor() 755 MB/s [ 1.213798] raid6: neonx2 gen() 1135 MB/s [ 1.285853] raid6: neonx2 xor() 1005 MB/s [ 1.357898] raid6: neonx4 gen() 1507 MB/s [ 1.429929] raid6: neonx4 xor() 1176 MB/s [ 1.501973] raid6: neonx8 gen() 1541 MB/s [ 1.574022] raid6: neonx8 xor() 1190 MB/s [ 1.578099] raid6: using algorithm neonx8 gen() 1541 MB/s [ 1.583461] raid6: .... xor() 1190 MB/s, rmw enabled [ 1.588392] raid6: using intx1 recovery algorithm [ 1.594670] SCSI subsystem initialized [ 1.598408] usbcore: registered new interface driver usbfs [ 1.603737] usbcore: registered new interface driver hub [ 1.609016] usbcore: registered new device driver usb [ 1.614058] media: Linux media interface: v0.10 [ 1.618517] Linux video capture interface: v2.00 [ 1.623102] pps_core: LinuxPPS API ver. 1 registered [ 1.628010] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it> [ 1.637103] PTP clock support registered [ 1.641000] EDAC MC: Ver: 3.0.0 [ 1.644344] FPGA manager framework [ 1.647673] fpga-region fpga-full: FPGA Region probed [ 1.652667] Advanced Linux Sound Architecture Driver Initialized. [ 1.658903] Bluetooth: Core ver 2.22 [ 1.662303] NET: Registered protocol family 31 [ 1.666703] Bluetooth: HCI device and connection manager initialized [ 1.673021] Bluetooth: HCI socket layer initialized [ 1.677863] Bluetooth: L2CAP socket layer initialized [ 1.682893] Bluetooth: SCO socket layer initialized [ 1.688281] clocksource: Switched to clocksource arch_sys_counter [ 1.694241] VFS: Disk quotas dquot_6.6.0 [ 1.698105] VFS: Dquot-cache hash table entries: 512 (order 0, 4096 bytes) [ 1.709332] NET: Registered protocol family 2 [ 1.713813] TCP established hash table entries: 32768 (order: 6, 262144 bytes) [ 1.721090] TCP bind hash table entries: 32768 (order: 7, 524288 bytes) [ 1.727982] TCP: Hash tables configured (established 32768 bind 32768) [ 1.734348] UDP hash table entries: 2048 (order: 4, 65536 bytes) [ 1.740351] UDP-Lite hash table entries: 2048 (order: 4, 65536 bytes) [ 1.746835] NET: Registered protocol family 1 [ 1.751191] RPC: Registered named UNIX socket transport module. [ 1.756924] RPC: Registered udp transport module. [ 1.761586] RPC: Registered tcp transport module. [ 1.766257] RPC: Registered tcp NFSv4.1 backchannel transport module. [ 1.773094] hw perfevents: enabled with armv8_pmuv3 PMU driver, 7 counters available [ 1.781328] futex hash table entries: 1024 (order: 5, 131072 bytes) [ 1.787442] audit: initializing netlink subsys (disabled) [ 1.792782] audit: type=2000 audit(1.736:1): initialized [ 1.798555] workingset: timestamp_bits=62 max_order=20 bucket_order=0 [ 1.805477] NFS: Registering the id_resolver key type [ 1.810353] Key type id_resolver registered [ 1.814492] Key type id_legacy registered [ 1.818475] nfs4filelayout_init: NFSv4 File Layout Driver Registering... [ 1.825144] jffs2: version 2.2. (NAND) (SUMMARY) �© 2001-2006 Red Hat, Inc. [ 1.836396] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247) [ 1.843592] io scheduler noop registered [ 1.847483] io scheduler deadline registered [ 1.851726] io scheduler cfq registered (default) [ 1.856952] nwl-pcie fd0e0000.pcie: Link is DOWN [ 1.861415] OF: PCI: host bridge /amba/pcie@fd0e0000 ranges: [ 1.867017] OF: PCI: MEM 0xe0000000..0xefffffff -> 0xe0000000 [ 1.872890] OF: PCI: MEM 0x600000000..0x7ffffffff -> 0x600000000 [ 1.879124] nwl-pcie fd0e0000.pcie: PCI host bridge to bus 0000:00 [ 1.885175] pci_bus 0000:00: root bus resource [bus 00-ff] [ 1.890621] pci_bus 0000:00: root bus resource [mem 0xe0000000-0xefffffff] [ 1.897455] pci_bus 0000:00: root bus resource [mem 0x600000000-0x7ffffffff pref] [ 1.905185] pci 0000:00:00.0: PCI bridge to [bus 01-0c] [ 1.911528] xilinx-dpdma fd4c0000.dma: Xilinx DPDMA engine is probed [ 1.918053] Write failed gate address:1000f02 [ 1.922301] xilinx-zynqmp-dma fd500000.dma: ZynqMP DMA driver Probe success [ 1.929279] xilinx-zynqmp-dma fd510000.dma: ZynqMP DMA driver Probe success [ 1.936192] xilinx-zynqmp-dma fd520000.dma: ZynqMP DMA driver Probe success [ 1.943111] xilinx-zynqmp-dma fd530000.dma: ZynqMP DMA driver Probe success [ 1.950030] xilinx-zynqmp-dma fd540000.dma: ZynqMP DMA driver Probe success [ 1.956953] xilinx-zynqmp-dma fd550000.dma: ZynqMP DMA driver Probe success [ 1.963872] xilinx-zynqmp-dma fd560000.dma: ZynqMP DMA driver Probe success [ 1.970790] xilinx-zynqmp-dma fd570000.dma: ZynqMP DMA driver Probe success [ 1.977742] zynqmp_pm firmware: Power management API v0.3 [ 2.015848] Serial: 8250/16550 driver, 4 ports, IRQ sharing disabled 2.032580] console [ttyPS0] enabled0 at MMIO 0xff000000 (irq = 39, base_baud = 6249999) is a xuartps [ 2.032580] console [ttyPS0] enabled [ 2.039540] bootconsole [cdns0] disabled [ 2.039540] bootconsole [cdns0] disabled [ 2.047964] ff010000.serial: ttyPS1 at MMIO 0xff010000 (irq = 40, base_baud = 6249999) is a xuartps [ 2.057130] [drm] Initialized [ 2.060434] [drm] load() is defered & will be called again [ 2.066516] xilinx-drm-dp-sub fd4aa000.dp_sub: Xilinx DisplayPort Subsystem is probed [ 2.074419] Unable to detect cache hierarchy from DT for CPU 0 [ 2.084703] brd: module loaded [ 2.090388] loop: module loaded [ 2.094184] ahci-ceva fd0c0000.ahci: couldn't get PHY in node ahci: -517 [ 2.100937] mtdoops: mtd device (mtddev=name/number) must be supplied [ 2.108622] m25p80 spi0.0: SPI-NOR-UniqueID 10000023536359160025001817101588af [ 2.115762] m25p80 spi0.0: found n25q512a, expected m25p80 [ 2.121340] m25p80 spi0.0: n25q512a (131072 Kbytes) [ 2.126148] 4 ofpart partitions found on MTD device spi0.0 [ 2.131599] Creating 4 MTD partitions on "spi0.0": [ 2.136376] 0x000000000000-0x000000100000 : "qspi-fsbl-uboot" [ 2.142594] 0x000000100000-0x000000600000 : "qspi-linux" [ 2.148287] 0x000000600000-0x000000620000 : "qspi-device-tree" [ 2.154478] 0x000000620000-0x000000c00000 : "qspi-rootfs" [ 2.161044] libphy: Fixed MDIO Bus: probed [ 2.166010] tun: Universal TUN/TAP device driver, 1.6 [ 2.170974] tun: (C) 1999-2004 Max Krasnyansky <maxk@qualcomm.com> [ 2.177241] CAN device driver interface [ 2.184002] macb ff0e0000.ethernet: Not enabling partial store and forward [ 2.191184] libphy: MACB_mii_bus: probed [ 2.196867] macb ff0e0000.ethernet eth0: Cadence GEM rev 0x50070106 at 0xff0e0000 irq 23 (00:0a:35:03:6f:71) [ 2.206608] TI DP83867 ff0e0000.etherne:0c: attached PHY driver [TI DP83867] (mii_bus:phy_addr=ff0e0000.etherne:0c, irq=-1) [ 2.218237] usbcore: registered new interface driver asix [ 2.223588] usbcore: registered new interface driver ax88179_178a [ 2.229647] usbcore: registered new interface driver cdc_ether [ 2.235462] usbcore: registered new interface driver net1080 [ 2.241104] usbcore: registered new interface driver cdc_subset [ 2.247007] usbcore: registered new interface driver zaurus [ 2.252574] usbcore: registered new interface driver cdc_ncm [ 2.260581] usbcore: registered new interface driver uas [ 2.265836] usbcore: registered new interface driver usb-storage [ 2.272059] mousedev: PS/2 mouse device common for all mice [ 2.277915] rtc_zynqmp ffa60000.rtc: rtc core: registered ffa60000.rtc as rtc0 [ 2.285081] i2c /dev entries driver [ 2.290599] usbcore: registered new interface driver uvcvideo [ 2.296262] USB Video Class driver (1.1.1) [ 2.300823] cdns-wdt fd4d0000.watchdog: Xilinx Watchdog Timer at ffffff800a010000 with timeout 10s [ 2.309866] Bluetooth: HCI UART driver ver 2.3 [ 2.314223] Bluetooth: HCI UART protocol H4 registered [ 2.319341] Bluetooth: HCI UART protocol BCSP registered [ 2.324639] Bluetooth: HCI UART protocol LL registered [ 2.329757] Bluetooth: HCI UART protocol ATH3K registered [ 2.335138] Bluetooth: HCI UART protocol Three-wire (H5) registered [ 2.341424] Bluetooth: HCI UART protocol Intel registered [ 2.346803] Bluetooth: HCI UART protocol Broadcom registered [ 2.352412] Bluetooth: HCI UART protocol QCA registered [ 2.357653] usbcore: registered new interface driver bcm203x [ 2.363292] usbcore: registered new interface driver bpa10x [ 2.368849] usbcore: registered new interface driver bfusb [ 2.374315] usbcore: registered new interface driver btusb [ 2.379755] Bluetooth: Generic Bluetooth SDIO driver ver 0.1 [ 2.385442] usbcore: registered new interface driver ath3k [ 2.390975] EDAC MC: ECC not enabled [ 2.394619] EDAC DEVICE0: Giving out device to module zynqmp-ocm-edac controller zynqmp_ocm: DEV ff960000.memory-controller (INTERRUPT) [ 2.407548] sdhci: Secure Digital Host Controller Interface driver [ 2.413643] sdhci: Copyright(c) Pierre Ossman [ 2.417981] sdhci-pltfm: SDHCI platform and OF driver helper [ 2.425963] ledtrig-cpu: registered to indicate activity on CPUs [ 2.431988] usbcore: registered new interface driver usbhid [ 2.437479] usbhid: USB HID core driver [ 2.441982] ad9361 spi32766.0: ad9361_probe : enter (ad9361) [ 2.451251] fpga_manager fpga0: Xilinx ZynqMP FPGA Manager registered [ 2.458173] xilinx-dp-snd-pcm dp_snd_pcm0: Xilinx DisplayPort Sound PCM probed [ 2.465416] xilinx-dp-snd-pcm dp_snd_pcm1: Xilinx DisplayPort Sound PCM probed [ 2.475104] Write failed to divider address:fd1a007c [ 2.480308] xilinx-dp-snd-codec dp_snd_codec0: Xilinx DisplayPort Sound Codec probed [ 2.488349] xilinx-dp-snd-card dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok [ 2.498020] xilinx-dp-snd-card dp_snd_card: xilinx-dp-snd-codec-dai <-> xilinx-dp-snd-codec-dai mapping ok [ 2.507912] xilinx-dp-snd-card dp_snd_card: Xilinx DisplayPort Sound Card probed [ 2.515314] pktgen: Packet Generator for packet performance testing. Version: 2.75 [ 2.523003] Netfilter messages via NETLINK v0.30. [ 2.527729] ip_tables: (C) 2000-2006 Netfilter Core Team [ 2.532999] Initializing XFRM netlink socket [ 2.537441] NET: Registered protocol family 10 [ 2.542258] ip6_tables: (C) 2000-2006 Netfilter Core Team [ 2.547607] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver [ 2.553797] NET: Registered protocol family 17 [ 2.558167] NET: Registered protocol family 15 [ 2.562593] bridge: filtering via arp/ip/ip6tables is no longer available by default. Update your scripts to load br_netfilter if you need this. [ 2.575517] Ebtables v2.0 registered [ 2.579108] can: controller area network core (rev 20120528 abi 9) [ 2.585265] NET: Registered protocol family 29 [ 2.589672] can: raw protocol (rev 20120528) [ 2.593918] can: broadcast manager protocol (rev 20161123 t) [ 2.599563] can: netlink gateway (rev 20130117) max_hops=1 [ 2.605084] Bluetooth: RFCOMM TTY layer initialized [ 2.609895] Bluetooth: RFCOMM socket layer initialized [ 2.615018] Bluetooth: RFCOMM ver 1.11 [ 2.618745] Bluetooth: BNEP (Ethernet Emulation) ver 1.3 [ 2.624038] Bluetooth: BNEP filters: protocol multicast [ 2.629252] Bluetooth: BNEP socket layer initialized [ 2.634194] Bluetooth: HIDP (Human Interface Emulation) ver 1.2 [ 2.640099] Bluetooth: HIDP socket layer initialized [ 2.645194] 9pnet: Installing 9P2000 support [ 2.649388] Key type dns_resolver registered [ 2.654078] registered taskstats version 1 [ 2.658470] Btrfs loaded, crc32c=crc32c-generic [ 2.672950] PLL: shutdown [ 2.675574] [drm] load() is defered & will be called again [ 2.681633] xilinx-psgtr fd400000.zynqmp_phy: Lane:1 type:8 protocol:4 pll_locked:yes [ 2.689628] xilinx-drm-dp fd4a0000.dp: device found, version 4.010 [ 2.695724] xilinx-drm-dp fd4a0000.dp: Display Port, version 1.0200 (tx) [ 2.702755] xilinx-psgtr fd400000.zynqmp_phy: Lane:3 type:3 protocol:2 pll_locked:yes [ 2.710553] ahci-ceva fd0c0000.ahci: AHCI 0001.0301 32 slots 2 ports 6 Gbps 0x3 impl platform mode [ 2.719447] ahci-ceva fd0c0000.ahci: flags: 64bit ncq sntf pm clo only pmp fbs pio slum part ccc sds apst [ 2.729782] scsi host0: ahci-ceva [ 2.733211] scsi host1: ahci-ceva [ 2.736573] ata1: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x100 irq 36 [ 2.744407] ata2: SATA max UDMA/133 mmio [mem 0xfd0c0000-0xfd0c1fff] port 0x180 irq 36 [ 2.754766] xilinx-psgtr fd400000.zynqmp_phy: Lane:2 type:0 protocol:3 pll_locked:yes [ 2.784444] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.789857] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 1 [ 2.797694] xhci-hcd xhci-hcd.0.auto: hcc params 0x0238f625 hci version 0x100 quirks 0x02010810 [ 2.806327] xhci-hcd xhci-hcd.0.auto: irq 221, io mem 0xfe200000 [ 2.812401] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002 [ 2.819111] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.826311] usb usb1: Product: xHCI Host Controller [ 2.831171] usb usb1: Manufacturer: Linux 4.9.0-12434-g7f38ed6 xhci-hcd [ 2.837771] usb usb1: SerialNumber: xhci-hcd.0.auto [ 2.842928] hub 1-0:1.0: USB hub found [ 2.846609] hub 1-0:1.0: 1 port detected [ 2.850655] xhci-hcd xhci-hcd.0.auto: xHCI Host Controller [ 2.856065] xhci-hcd xhci-hcd.0.auto: new USB bus registered, assigned bus number 2 [ 2.863810] usb usb2: New USB device found, idVendor=1d6b, idProduct=0003 [ 2.870516] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1 [ 2.877716] usb usb2: Product: xHCI Host Controller [ 2.882576] usb usb2: Manufacturer: Linux 4.9.0-12434-g7f38ed6 xhci-hcd [ 2.889172] usb usb2: SerialNumber: xhci-hcd.0.auto [ 2.894296] hub 2-0:1.0: USB hub found [ 2.897977] hub 2-0:1.0: 1 port detected [ 2.902774] cdns-i2c ff020000.i2c: 400 kHz mmio ff020000 irq 25 [ 2.908837] 0-0020 supply vcc not found, using dummy regulator [ 2.915542] GPIO line 322 (sel0) hogged as output/low [ 2.920714] GPIO line 323 (sel1) hogged as output/high [ 2.925971] GPIO line 324 (sel2) hogged as output/high [ 2.931224] GPIO line 325 (sel3) hogged as output/high [ 2.936397] pca953x 0-0020: interrupt support not compiled in [ 2.942137] 0-0021 supply vcc not found, using dummy regulator [ 2.948496] pca953x 0-0021: interrupt support not compiled in [ 2.954961] ina2xx 3-0040: power monitor ina226 (Rshunt = 5000 uOhm) [ 2.961638] ina2xx 3-0041: power monitor ina226 (Rshunt = 5000 uOhm) [ 2.968324] ina2xx 3-0042: power monitor ina226 (Rshunt = 5000 uOhm) [ 2.974997] ina2xx 3-0043: power monitor ina226 (Rshunt = 5000 uOhm) [ 2.981674] ina2xx 3-0044: power monitor ina226 (Rshunt = 5000 uOhm) [ 2.988353] ina2xx 3-0045: power monitor ina226 (Rshunt = 5000 uOhm) [ 2.995026] ina2xx 3-0046: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.001695] ina2xx 3-0047: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.008377] ina2xx 3-004a: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.015052] ina2xx 3-004b: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.021337] i2c i2c-0: Added multiplexed i2c bus 3 [ 3.026696] ina2xx 4-0040: power monitor ina226 (Rshunt = 2000 uOhm) [ 3.033378] ina2xx 4-0041: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.040062] ina2xx 4-0042: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.046736] ina2xx 4-0043: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.053408] ina2xx 4-0044: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.060088] ina2xx 4-0045: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.066486] ata2: SATA link down (SStatus 0 SControl 330) [ 3.066768] ina2xx 4-0046: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.067173] ina2xx 4-0047: power monitor ina226 (Rshunt = 5000 uOhm) [ 3.067191] i2c i2c-0: Added multiplexed i2c bus 4 [ 3.088296] random: fast init done [ 3.092659] ata1: SATA link down (SStatus 0 SControl 330) [ 3.097635] i2c i2c-0: Added multiplexed i2c bus 5 [ 3.097773] i2c i2c-0: Added multiplexed i2c bus 6 [ 3.097777] pca954x 0-0075: registered 4 multiplexed busses for I2C mux pca9544 [ 3.098668] cdns-i2c ff030000.i2c: 400 kHz mmio ff030000 irq 26 [ 3.099569] at24 7-0054: 1024 byte 24c08 EEPROM, writable, 1 bytes/write [ 3.099585] i2c i2c-1: Added multiplexed i2c bus 7 [ 3.099785] i2c i2c-1: Added multiplexed i2c bus 8 [ 3.101809] si570 9-005d: registered, current frequency 300000000 Hz [ 3.101826] i2c i2c-1: Added multiplexed i2c bus 9 [ 3.115761] si570 10-005d: registered, current frequency 148500000 Hz [ 3.115778] i2c i2c-1: Added multiplexed i2c bus 10 [ 3.115985] i2c i2c-1: Added multiplexed i2c bus 11 [ 3.116117] i2c i2c-1: Added multiplexed i2c bus 12 [ 3.116245] i2c i2c-1: Added multiplexed i2c bus 13 [ 3.116388] i2c i2c-1: Added multiplexed i2c bus 14 [ 3.116392] pca954x 1-0074: registered 8 multiplexed busses for I2C switch pca9548 [ 3.117790] at24 15-0050: 256 byte 24c02 EEPROM, writable, 1 bytes/write [ 3.117806] i2c i2c-1: Added multiplexed i2c bus 15 [ 3.117945] i2c i2c-1: Added multiplexed i2c bus 16 [ 3.118081] i2c i2c-1: Added multiplexed i2c bus 17 [ 3.118547] i2c i2c-1: Added multiplexed i2c bus 18 [ 3.118691] i2c i2c-1: Added multiplexed i2c bus 19 [ 3.118830] i2c i2c-1: Added multiplexed i2c bus 20 [ 3.118974] i2c i2c-1: Added multiplexed i2c bus 21 [ 3.119112] i2c i2c-1: Added multiplexed i2c bus 22 [ 3.119117] pca954x 1-0075: registered 8 multiplexed busses for I2C switch pca9548 [ 3.172287] mmc0: SDHCI controller on ff170000.sdhci [ff170000.sdhci] using ADMA 64-bit [ 3.172708] ad9361 spi32766.0: ad9361_probe : enter (ad9361) [ 3.304741] mmc0: new ultra high speed DDR50 SDHC card at address e624 [ 3.311462] mmcblk0: mmc0:e624 SL08G 7.40 GiB [ 3.316713] mmcblk0: p1 p2 p3 [ 3.416956] ad9361 spi32766.0: ad9361_probe : AD936x Rev 2 successfully initialized [ 3.435516] cf_axi_dds 99024000.cf-ad9361-dds-core-lpc: Analog Devices CF_AXI_DDS_DDS MASTER (9.00.b) at 0x99024000 mapped to 0xffffff800a178000, probed DDS AD9361 [ 3.450477] PLL: enable [ 3.453191] PLL: shutdown [ 3.455891] OF: graph: no port node found in /xilinx_drm [ 3.461122] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013). [ 3.467715] [drm] No driver support for vblank timestamp query. [ 3.473635] xilinx-drm xilinx_drm: No connectors reported connected with modes [ 3.480828] [drm] Cannot find any crtc or sizes - going 1024x768 [ 3.492477] Console: switching to colour frame buffer device 128x48 [ 3.503298] xilinx-drm xilinx_drm: fb0: frame buffer device [ 3.532289] [drm] Initialized xilinx_drm 1.0.0 20130509 on minor 0 [ 4.557574] cf_axi_adc 99020000.cf-ad9361-lpc: ADI AIM (10.00.b) at 0x99020000 mapped to 0xffffff800a4c0000, probed ADC AD9361 as MASTER [ 4.570069] input: gpio-keys as /devices/platform/gpio-keys/input/input0 [ 4.576898] rtc_zynqmp ffa60000.rtc: setting system clock to 2017-04-27 11:03:14 UTC (1493290994) [ 4.587830] ALSA device list: [ 4.590713] #0: DisplayPort monitor [ 4.595264] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities [ 5.026539] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null) [ 5.034560] VFS: Mounted root (ext4 filesystem) on device 179:2. [ 5.045332] devtmpfs: mounted [ 5.048329] Freeing unused kernel memory: 512K (ffffffc000cf0000 - ffffffc000d70000) Mount failed for selinuxfs on /sys/fs/selinux: No such file or directory [ 6.041604] systemd-udevd[2931]: could not open moddep file '/lib/modules/4.9.0-12434-g7f38ed6/modules.dep.bin' [ OK ]ting up X socket directories... * STARTDISTCC is set to false in /etc/default/distcc * /usr/bin/distccd not starting [ OK ]rting IIO Daemon iiod Last login: Thu Apr 27 11:03:18 UTC 2017 on tty1 Welcome to Linaro 14.04 (GNU/Linux 4.9.0-12434-g7f38ed6 aarch64) * Documentation: https://wiki.analog.com/ https://ez.analog.com/ New release '16.04.3 LTS' available. Run 'do-release-upgrade' to upgrade to it. root@analog:~#
This specifies any shell prompt running on the target
root@analog:~# iio_info | grep iio:device iio:device0: ad7291 iio:device1: ad9361-phy iio:device2: cf-ad9361-dds-core-lpc iio:device3: cf-ad9361-lpc
This specifies any shell prompt running on the target
root@analog:~# fru-dump -b /sys/bus/i2c/devices/14-0050/eeprom read 256 bytes from /sys/bus/i2c/devices/14-0050/eeprom Date of Man : Wed Aug 27 16:42:00 2014 Manufacture : Analog Devices Product Name : AD9361 Software Development Kit Serial Number : Non-ASCII Part Number : AD-FMCOMMS3-EBZ FRU File ID : Empty Field PCB Rev : A PCB ID : FMCOMMSFMC03A BOM Rev : 1 Uses LVDS : Y
Please see also here:Oscilloscope
The IIO Oscilloscope application can be used to connect to another platform that has a connected device in order to configure the device and read data from it.
Build and start osc on a network enabled Linux host.
Once the application is launched goto Settings → Connect and enter the IP address of the target in the popup window.