This shows you the differences between two versions of the page.
Both sides previous revision Previous revision | |||
resources:eval:user-guides:ad-fmcomms2-ebz:prerequisites [26 Oct 2016 16:22] Lucian Sin added AD9364 to title |
resources:eval:user-guides:ad-fmcomms2-ebz:prerequisites [26 Oct 2016 17:13] Lucian Sin added AD9364 to text |
||
---|---|---|---|
Line 2: | Line 2: | ||
What you need, depends on what you are trying to do. As a minimum, you need to start out with: | What you need, depends on what you are trying to do. As a minimum, you need to start out with: | ||
- | - The AD9361 based card. To determine which card is best for you, check out the [[introduction]] section. | + | - The AD9361/AD9364 based card. To determine which card is best for you, check out the [[introduction]] section. |
- | - A carrier platform. ADI does not offer these boards for sale or loan, getting one yourself is normal part of development or evaluation of the AD9361. Our recommended carriers (the ones we use all the time) are either: | + | - A carrier platform. ADI does not offer these boards for sale or loan, getting one yourself is normal part of development or evaluation of the AD9361/AD9364. Our recommended carriers (the ones we use all the time) are either: |
- | * The [[http://zedboard.org/product/zedboard|ZedBoard]]. This is a low cost board, which can be used for basic HDL designs, or just for looking at the AD9361. Most of our software and RF developers have this board. | + | * The [[http://zedboard.org/product/zedboard|ZedBoard]]. This is a low cost board, which can be used for basic HDL designs, or just for looking at the AD9361/AD9364. Most of our software and RF developers have this board. |
* The [[xilinx>zc706|Xilinx ZC706]]. The fabric on this device is much larger, and if you are looking at targeting - this is the recommended option. | * The [[xilinx>zc706|Xilinx ZC706]]. The fabric on this device is much larger, and if you are looking at targeting - this is the recommended option. | ||
* The [[https://www.arrow.com/en/products/sockit/arrow-development-tools|Arrow SoCKit]]. This is a low cost board, which can be used for basic HDL designs, or just for looking at the AD9361. | * The [[https://www.arrow.com/en/products/sockit/arrow-development-tools|Arrow SoCKit]]. This is a low cost board, which can be used for basic HDL designs, or just for looking at the AD9361. | ||
- | * There are a few more boards, which do work, and are supported, but they are just not tested as often (most of the full time developers who work with the AD9361 based boards use the Zed or the ZC706). The experience of the fabric only solutions is very close to the ARM/FPGA SoC based solutions, but the GUI runs on a host PC (Windows or Linux). | + | * There are a few more boards, which do work, and are supported, but they are just not tested as often (most of the full time developers who work with the AD9361/AD9364 based boards use the Zed or the ZC706). The experience of the fabric only solutions is very close to the ARM/FPGA SoC based solutions, but the GUI runs on a host PC (Windows or Linux). |
* {{page>quickstart#supported_carriers&firstseconly}} | * {{page>quickstart#supported_carriers&firstseconly}} | ||
- some way to interact with the platform, | - some way to interact with the platform, |