Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcomms2-ebz:hardware [08 Oct 2013 15:28] – Move Downloads to the top, since that is what most people want Robin Getz | resources:eval:user-guides:ad-fmcomms2-ebz:hardware [09 Mar 2023 01:25] (current) – updated the design files download link Joyce Velasco |
---|
====== AD-FMCOMMS2-EBZ Hardware ====== | ====== AD-FMCOMMS2-EBZ Hardware ====== |
| \\ |
| |
===== Downloads ===== | ===== Schematics, PCB Layout, Bill of Materials ===== |
| |
<WRAP round download 65%> | <WRAP round download 65%> |
<WRAP info>This is the latest and greatest Rev "C" of this board, and is ready for production. Note that the Baluns on the Rev C board (T101-T104) are Johanson Technology's [[http://www.johansontechnology.com/images/stories/ip/baluns/Balun_2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an alternative balun should be installed. This is described inside the //"AD9361 RF Port Interface"// document, which is a part of the full AD9361 documentation package. The test results were taken with Rev C, using the Johanson Technology's 2450BL15B050E balun. | <WRAP info>This is the latest and greatest Rev "E" of this board. Note that the Baluns on the Rev C board (T101-T104) are Johanson Technology's [[https://www.johansontechnology.com/datasheets/2450BL15B050/2450BL15B050.pdf|2450BL15B050E]] 2.45 GHz Balun. This balun is rated for a operating frequency of 2400~2500 MHz. If you want to evaluate the part outside of this frequency range, an [[./hardware/configuration_options|alternative balun]] should be installed. The test results were taken using the Johanson Technology's 2450BL15B050E balun. |
| |
</WRAP> | </WRAP> |
* {{:resources:eval:user-guides:ad-fmcomms2-ebz:ad9361_fmc_revc_schematic.pdf|Rev C Schematics}} | [[adi>media/en/reference-design-documentation/design-integration-files/ad-fmcomms2-ebz-designsupport.zip|AD-FMCOMMS2-EBZ Design & Integration Files]] |
* {{:resources:eval:user-guides:ad-fmcomms2-ebz:ad9361_fmc_revc_gerbers.zip|Rev C Gerbers}} | |
* {{:resources:eval:user-guides:ad-fmcomms2-ebz:ad9361_fmc_revc_bom.xls|Rev C Bill of materials}} | * Schematic |
* {{:resources:eval:user-guides:ad-fmcomms2-ebz:ad9361_fmc_revc_pcb.brd.7z|Rev C Allegro Board File}} (This file is [[http://www.7-zip.org/7z.html|compressed]]). Get the [[http://www.cadence.com/products/pcb/Pages/downloads.aspx|Allegro FREE Physical Viewer]] (You need 16.5 or higher). | * PCB Layout |
| * Bill of Materials |
| * The Epson crystal used on this board, has the generic part number "TSX-3225 40.0000MHZ" - however, the generic part number does not have the specifications needed to meet the AD9361 datasheet specs. ADI has worked with Epson to provide a tighter tolerance part, which can be ordered as the "OUTD-2B-0166" or "X1E000021036701" (either part number will work, depending on which system your Epson contact/distributor has) which meets the requirements that the AD9361 demands. |
| * Allegro Project (Get the [[https://www.cadence.com/en_US/home/tools/pcb-design-and-analysis/allegro-downloads-start.html|Allegro FREE Physical Viewer]]; you need 16.5 or higher). |
</WRAP> | </WRAP> |
| |
| ===== I/O Voltage ===== |
| |
| The AD-FMComms2 (AD9361) assumes a VDD_INTERFACE voltage between 1.71V and 2.625V (1.8 to 2.5 +/- 5%), so on your FPGA carrier board, you should ensure that V<sub>ADJ</sub> is between these levels. Setting things to 3.3V will damage the part. |
| |
| |
| |
===== Picture and Main components ===== | ===== Picture and Main components ===== |
{{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} | {{:resources:eval:user-guides:ad-fmcomms2-ebz:fmcomms2c_layers.png?direct&600|}} |
| |
{{navigation AD-FMCOMMS2-EBZ#quickstart|Quick Start Guides#.:|Overview#reference_hdl|Reference HDL Design}} | |