This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-fmcomms2-ebz:hardware:functional_overview [17 Oct 2016 14:28] – [Power] remove ADP7104 and ADP190, added ADP2164 Lucian Sin | resources:eval:user-guides:ad-fmcomms2-ebz:hardware:functional_overview [27 Jan 2023 14:45] (current) – Update documentation link for AD9361 Reference Manual Paul Pop | ||
---|---|---|---|
Line 43: | Line 43: | ||
The device also allows real-time monitoring of internal signals via another set of dedicated pins. Again, these signals are passed to the FMC connector. The internal signals are multiplexed into these pins- and details of which are best described in the data sheet. | The device also allows real-time monitoring of internal signals via another set of dedicated pins. Again, these signals are passed to the FMC connector. The internal signals are multiplexed into these pins- and details of which are best described in the data sheet. | ||
+ | |||
+ | More information can be found in the AD9361 Reference Manual [[https:// | ||
===== Power ===== | ===== Power ===== |