Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcomms2-ebz:downloads [01 Apr 2016 14:05] – make pointer to page /resources/tools-software/linux-software/embedded_arm_images#Download Linux Image Lucian Sin | resources:eval:user-guides:ad-fmcomms2-ebz:downloads [31 Jan 2023 09:10] (current) – Replaced the obsolete Kuiper Linux page link Joyce Velasco |
---|
| |
The source code of the no-OS software and the scripts can be downloaded from the Analog Devices github. | The source code of the no-OS software and the scripts can be downloaded from the Analog Devices github. |
| |
**no-OS Software** | |
| |
<WRAP round download 100%> | <WRAP round download 100%> |
* **AD9361 No-OS Software** https://github.com/analogdevicesinc/no-OS/tree/master/ad9361/sw | * **AD9361 Example project** [[repo>no-OS/tree/master/projects/ad9361]] |
* **Generic Platform Driver** https://github.com/analogdevicesinc/no-OS/tree/master/ad9361/sw/platform_generic | * **AD9361 Generic Driver** [[repo>no-OS/tree/master/drivers/rf-transceiver/ad9361]] |
* **Linux Userspace Platform Driver** https://github.com/analogdevicesinc/no-OS/tree/master/ad9361/sw/platform_linux | * **Linux Makefile** [[repo>no-OS/tree/master/projects/ad9361/src/Makefile.linux]] |
* **Xilinx Platform Driver** https://github.com/analogdevicesinc/no-OS/tree/master/ad9361/sw/platform_xilinx | |
* **Xilinx Scripts** https://github.com/analogdevicesinc/no-OS/tree/master/ad9361/scripts | |
* **Console Commands Driver** https://github.com/analogdevicesinc/no-OS/tree/master/ad9361/sw/console_commands | |
</WRAP> | </WRAP> |
| |
===== Download HDL ====== | ===== Download HDL ====== |
| |
**HDL Reference Designs** | |
| |
<WRAP round info 100%> | <WRAP round info 100%> |
{{page>/resources/fpga/docs/hdl/downloads_insert#arradio&nofooter&noeditbtn}} | {{page>/resources/fpga/docs/hdl/downloads_insert#arradio&nofooter&noeditbtn}} |
| |
| ===== Download Linux Image ===== |
| |
{{page>/resources/tools-software/linux-software/embedded_arm_images#Download Linux Image}} | The **BOLD** is what you should type. It's not too much more than [[wp>Special Agent Oso]]'s three special steps, and it also allows you to go for that specialty coffee you have been craving. |
| |
| For different platforms you'll need different images. Currently we provide a single pre-build images, that can work on all the platforms we support. |
| |
| <note important>Make sure you unzip the image using either [[https://www.7-zip.org/|7-zip]] or on Linux it can be done via command-line **xz -d <image_name>.img.xz**. The actual file that needs to be dumped to the SD card has to have the ***.img** extension.</note> |
| |
| <note important>Your SD-card needs to be at least 16 GB for releases 2019-R2 and newer. Or 8 GB for older releases.</note> |
| |
| <note warning>If your computer has security restrictions imposed by your company's IT department, which prevent your from writing data to SD-cards (or the data is encrypted when written on the SD-card), then consider using a computer that doesn't have such restrictions, or communicating with your IT department to find a solution.</note> |
| |
| <WRAP hi round download 80%> |
| * [[:resources:tools-software:linux-software:adi-kuiper_images:release_notes|Download Release Images]] |
| </WRAP> |
| |
| Now, depending if you are using Linux or Windows, follow these instructions to write the file to your SD card. |
| * [[resources:tools-software:linux-software:zynq_images:linux_hosts|Linux Hosts]] |
| * [[resources:tools-software:linux-software:zynq_images:windows_hosts|Windows Hosts]] |
| |
===== Download Filters ===== | ===== Download Filters ===== |
| |
In order to run the wizard, your [[mw>products/matlab/|MATLAB]] license needs to include the following components: | In order to run the wizard, your [[mw>products/matlab/|MATLAB]] license needs to include the following components: |
* MATLAB (R2014a or higher version is required) | * MATLAB (R2015b or higher version is required) |
* Signal Processing Toolbox | * Signal Processing Toolbox |
* DSP System Toolbox | * DSP System Toolbox |
* Within the application directory run the command "AD9361_Filter_Wizard" from the MATLAB command line. | * Within the application directory run the command "AD9361_Filter_Wizard" from the MATLAB command line. |
| |
The Filter Design Wizard has been applied in the SimRF models of AD9361, provided by MathWorks as a hardware support package. **Download this version if to be used with the AD9361 SimRF model:** | The Filter Design Wizard has been applied in the RF Blockset (formerly SimRF) models of AD9361, provided by MathWorks as a hardware support package. **Download this version if to be used with the AD9361 RF Blockset (formerly SimRF) model:** |
| |
<WRAP round download> | <WRAP round download> |
* {{:resources:eval:user-guides:ad-fmcomms2-ebz:software:ad9361_filter_design_wizard_v2.mlappinstall|AD9361 Filter Design Wizard for SimRF Model}} | * {{:resources:eval:user-guides:ad-fmcomms2-ebz:software:ad9361_filter_design_wizard_v2.mlappinstall|AD9361 Filter Design Wizard for RF Blockset (formerly SimRF) Model}} |
</WRAP> | </WRAP> |
| |
===== Download IIO-Oscilloscope ===== | ===== Download IIO-Oscilloscope ===== |
<WRAP round download> | <WRAP round download> |
Latest releases: | Latest releases (goto this page to download the file): |
* [[https://github.com/analogdevicesinc/iio-oscilloscope/releases]] | * [[https://github.com/analogdevicesinc/iio-oscilloscope/releases]] |
| |
* **IIO Oscilloscope for Windows - v0.2-2015_R1 ** | |
* Download: [[https://github.com/analogdevicesinc/iio-oscilloscope/releases/download/v0.2-2015_R1/adi-osc-2015_R1-setup.exe|adi-osc-2015_R1-setup.exe]] | |
| |
Historic releases: | |
| |
* **IIO Oscilloscope (OSC) for Win32 & Win64 (2014_R2 Alpha Pre-Release) ** | |
* Download: [[http://swdownloads.analog.com/cse/osc/adi-osc-setup.exe|adi-osc-setup.exe]] | |
</WRAP> | </WRAP> |
| |
<WRAP round download> | <WRAP round download> |
* [[https://github.com/analogdevicesinc/libiio/releases|Installer for latest stable build (Windows 32-bit / 64-bit)]] | * [[https://github.com/analogdevicesinc/libiio/releases|Installer for latest stable build (Windows 32-bit / 64-bit)]] |
* [[https://ci.appveyor.com/project/analogdevicesinc/libiio/build/artifacts|Installer for latest nighty build (Windows 32-bit / 64-bit)]] (may be unstable / buggy) | * [[https://ci.appveyor.com/project/analogdevicesinc/libiio/build/artifacts?branch=master|Installer for latest nighty build (Windows 32-bit / 64-bit)]] (may be unstable / buggy) |
</WRAP> | </WRAP> |