This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcomms2-ebz:downloads [18 Mar 2016 16:51] – Libiio Lucian Sin | resources:eval:user-guides:ad-fmcomms2-ebz:downloads [31 Jan 2023 09:10] (current) – Replaced the obsolete Kuiper Linux page link Joyce Velasco | ||
---|---|---|---|
Line 3: | Line 3: | ||
The source code of the no-OS software and the scripts can be downloaded from the Analog Devices github. | The source code of the no-OS software and the scripts can be downloaded from the Analog Devices github. | ||
- | **no-OS Software** | + | <WRAP round download |
- | + | * **AD9361 | |
- | <WRAP round download | + | * **AD9361 |
- | * **AD9361 | + | * **Linux Makefile** [[repo>no-OS/ |
- | * **Generic | + | |
- | * **Linux Userspace Platform Driver** https:// | + | |
- | * **Xilinx Platform Driver** https:// | + | |
- | * **Xilinx Scripts** https:// | + | |
- | * **Console Commands Driver** https://github.com/ | + | |
- | </ | + | |
- | + | ||
- | **HDL Reference Designs for FMCOMMS2** | + | |
- | + | ||
- | <WRAP round download 90%> | + | |
- | + | ||
- | * **ZED HDL Reference Design for Vivado: ** https:// | + | |
- | * **ZC702 HDL Reference Design for Vivado: **https:// | + | |
- | * **ZC706 HDL Reference Design for Vivado: **https:// | + | |
- | * **AC701 HDL Reference Design for Vivado: **https:// | + | |
- | * **KC705 HDL Reference Design for Vivado: **https:// | + | |
- | * **VC707 HDL Reference Design for Vivado: **https:// | + | |
- | + | ||
- | * **ML605 HDL Reference Design for ISE: ** https:// | + | |
- | </ | + | |
- | + | ||
- | **HDL Reference Designs for FMCOMMS5** | + | |
- | <WRAP round download 90%> | + | |
- | * **ZC702 HDL Reference Design for Vivado: | + | |
- | **https:// | + | |
- | * **ZC706 HDL Reference Design for Vivado: | + | |
- | **https:// | + | |
</ | </ | ||
===== Download HDL ====== | ===== Download HDL ====== | ||
- | FPGA Reference Designs on GitHub : | + | <WRAP round info 100%> |
- | + | ||
- | <WRAP round info 80%> | + | |
Please note that the projects **FMCOMMS2**, | Please note that the projects **FMCOMMS2**, | ||
- | + | The **ARRADIO** Quartus project uses [[https:// | |
- | The **ARRADIO** Quartus project uses [[https:// | + | |
- | </ | + | |
- | <WRAP round download 80%> | + | |
- | **Vivado / Quartus Downloads** | + | |
- | * Main repository with latest changes (always synced with the latest release) | + | |
- | * https:// | + | |
- | * Releases (the used tool version can be found in README.md) | + | |
- | * https:// | + | |
- | * https:// | + | |
- | * https:// | + | |
</ | </ | ||
+ | {{page>/ | ||
+ | {{page>/ | ||
+ | {{page>/ | ||
===== Download Linux Image ===== | ===== Download Linux Image ===== | ||
Line 63: | Line 26: | ||
For different platforms you'll need different images. Currently we provide a single pre-build images, that can work on all the platforms we support. | For different platforms you'll need different images. Currently we provide a single pre-build images, that can work on all the platforms we support. | ||
- | <WRAP hi round download 80%> | + | <note important>Make sure you unzip the image using either |
- | * **15 March 2016 release (2015_R2) ** | + | |
- | * [[http://swdownloads.analog.com/ | + | |
- | | + | |
- | | + | |
- | </WRAP> | + | |
- | <WRAP lo round download 80%> | + | <note important>Your SD-card needs to be at least 16 GB for releases 2019-R2 and newer. Or 8 GB for older releases.</note> |
- | * **22 December 2015 release (2015_R1) ** | + | |
- | * [[http:// | + | |
- | * Checksum 2015_R1-2015_12_22.img.xz | + | |
- | * Checksum 2015_R1-2015_12_22.img '' | + | |
- | </WRAP> | + | |
- | <WRAP lo round download 80%> | + | <note warning>If your computer has security restrictions imposed by your company' |
- | * **17 November 2015 release | + | |
- | * [[http:// | + | |
- | * Checksum 2015_R1-2015_11_17.img.xz | + | |
- | * Checksum 2015_R1-2015_11_17.img '' | + | |
- | </WRAP> | + | |
- | < | + | < |
- | * **4 September 2015 release (2015_R1) ** | + | * [[:resources: |
- | * [[http:// | + | |
- | * Checksum 2015_R1-2015_09_04.img.xz | + | |
- | * Checksum 2015_R1-2015_09_04.img | + | |
- | </ | + | |
- | + | ||
- | <WRAP lo round download 80%> | + | |
- | * **31 August 2015 release (2015_R1) ** | + | |
- | * [[http:// | + | |
- | * Checksum 2015_R1-2015_08_31.img.xz | + | |
- | * Checksum 2015_R1-2015_08_31.img | + | |
- | </ | + | |
- | + | ||
- | <WRAP lo round download 80%> | + | |
- | * **6 February 2015 release (2014_R2) ** | + | |
- | * [[http:// | + | |
- | * Checksum 2014_R2-2015_02_06.img.xz | + | |
- | * Checksum 2014_R2-2015_02_06.img | + | |
</ | </ | ||
- | Now, depending if you are using Linux or Windows, follow these instructions to write the file to your 8 Gig SD card. | + | Now, depending if you are using Linux or Windows, follow these instructions to write the file to your SD card. |
- | * [[./zynq_images/Linux Hosts]] | + | * [[resources: |
- | * [[./zynq_images/Windows Hosts]] | + | * [[resources: |
===== Download Filters ===== | ===== Download Filters ===== | ||
- | <WRAP important> | + | < |
In order to run the wizard, your [[mw> | In order to run the wizard, your [[mw> | ||
- | * MATLAB (R2012b | + | * MATLAB (R2015b |
* Signal Processing Toolbox | * Signal Processing Toolbox | ||
* DSP System Toolbox | * DSP System Toolbox | ||
Line 123: | Line 54: | ||
In order to get the wizard, please go to Analog Devices GitHub. Different releases of AD9361 Filter Design Wizard and their source files can be found here: | In order to get the wizard, please go to Analog Devices GitHub. Different releases of AD9361 Filter Design Wizard and their source files can be found here: | ||
- | <WRAP download> | + | < |
* https:// | * https:// | ||
* For each release, the wizard is available as a MATLAB App installer (mlappinstall) or in archive form (zip or tarball). | * For each release, the wizard is available as a MATLAB App installer (mlappinstall) or in archive form (zip or tarball). | ||
Line 135: | Line 66: | ||
* Within the application directory run the command " | * Within the application directory run the command " | ||
- | The Filter Design Wizard has been applied in the SimRF models of AD9361, provided by MathWorks as a hardware support package. **Download this version if to be used with the AD9361 SimRF model: | + | The Filter Design Wizard has been applied in the RF Blockset (formerly |
- | <WRAP download> | + | < |
- | * {{: | + | * {{: |
</ | </ | ||
Line 144: | Line 75: | ||
To learn more about AD9361 modeling and to download the Tx and Rx models, the hardware support package can be found here: | To learn more about AD9361 modeling and to download the Tx and Rx models, the hardware support package can be found here: | ||
- | <WRAP info> | + | < |
* http:// | * http:// | ||
</ | </ | ||
Line 150: | Line 81: | ||
===== Download IIO-Oscilloscope ===== | ===== Download IIO-Oscilloscope ===== | ||
<WRAP round download> | <WRAP round download> | ||
- | Latest releases: | + | Latest releases |
* [[https:// | * [[https:// | ||
- | + | ||
- | * **IIO Oscilloscope for Windows - v0.2-2015_R1 ** | + | |
- | * Download: [[https:// | + | |
- | + | ||
- | Historic releases: | + | |
- | + | ||
- | * **IIO Oscilloscope (OSC) for Win32 & Win64 (2014_R2 Alpha Pre-Release) ** | + | |
- | * Download: [[http:// | + | |
</ | </ | ||
Line 165: | Line 89: | ||
The libiio library can be obtained on the [[http:// | The libiio library can be obtained on the [[http:// | ||
==== Libiio installer for Windows ==== | ==== Libiio installer for Windows ==== | ||
- | <WRAP download> | + | < |
* [[https:// | * [[https:// | ||
- | * [[https:// | + | * [[https:// |
</ | </ |