This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-fmcmotcon2-ebz:software:iio_scope [02 Apr 2015 17:52] – [IIO OSC] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon2-ebz:software:iio_scope [21 Jul 2015 13:30] (current) – spelling error Lucian Sin | ||
---|---|---|---|
Line 3: | Line 3: | ||
===== IIO OSC ===== | ===== IIO OSC ===== | ||
- | ADI IIO oscilloscope is used for monitoring and controlling the AD-FMCMOTCON2-EBZ board, when using the Linux operating system. A complete user guide for the IIO oscilloscope can e found **[[resources/ | + | ADI IIO oscilloscope is used for monitoring and controlling the AD-FMCMOTCON2-EBZ board, when using the Linux operating system. A complete user guide for the IIO oscilloscope can be found **[[resources/ |
==== Signals monitoring ==== | ==== Signals monitoring ==== | ||
Line 28: | Line 28: | ||
==== Control ==== | ==== Control ==== | ||
- | This dialog allows the control of the tow motors in manual mode by directly specifying the fill factor of the PWM signals applied used to control the 3 phase inverters. The motors are driven using a 6 step comutation algorithm.\\ | + | This dialog allows the control of the two motors in manual mode by directly specifying the fill factor of the PWM signals applied used to control the 3 phase inverters. The motors are driven using a 6 step comutation algorithm.\\ |
{{: | {{: |