This is an old revision of the document!
ADI IIO oscilloscope is used for monitoring and controlling the AD-FMCMOTCON2-EBZ board, when using the Linux operating system. A complete user guide for the IIO oscilloscope can e found here.
The IIO Oscilloscope allows to monitor current, voltage, speed and control signals from the system. Below is presented a description of the different monitoring channels exposed by the IIO Oscilloscope.
Group | Channel | Description |
---|---|---|
ad-mc-adc | voltage0 | Not used |
voltage1 | Motor 1 Ia ADC raw data | |
voltage2 | Motor 1 Ib ADC raw data | |
voltage3 | Motor 1 VBus ADC raw data | |
ad-mc-adc-m2 | voltage0 | Not used |
voltage1 | Motor 2 Ia ADC raw data | |
voltage2 | Motor 2 Ib ADC raw data | |
voltage3 | Motor 2 VBus ADC raw data | |
ad-mc-speed | voltage0 | Motor 1 speed. Number of counts in 10ns units between two motor commutations. In order to display the speed in RPM, the data should be processed by checking the 1/x option and multiply by 25.000.000 |
ad-mc-speed-m2 | voltage0 | Motor 1 speed. Number of counts in 10ns units between two motor commutations. In order to display the speed in RPM, the data should be processed by checking the 1/x option and multiply by 25.000.000 |
ad-mc-ctrl | Not used | |
ad-mc-ctrl-m2 | Not used |
This dialog allows the control of the tow motors in manual mode by directly specifying the fill factor of the PWM signals applied used to control the 3 phase inverters. The motors are driven using a 6 step comutation algorithm.
Control | Description |
---|---|
Run | Starts the motor |
Delta | Selects between driving the motor using a Star-like sequence or Delta sequence |
Direction | Selects between clockwise and counterclockwise rotation directions |
PWM | In Manual mode, the PWM can be set between 50% - 100% |