Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [30 Mar 2015 14:31] Andrei Cozmaresources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [07 Nov 2016 09:37] (current) – change zedboard links Lucian Sin
Line 4: Line 4:
 ===== Supported Carriers ===== ===== Supported Carriers =====
  
-  * [[http://www.zedboard.org|ZedBoard]] +  * [[http://zedboard.org/product/zedboard|ZedBoard]] 
  
 |< 100% 100% >| |< 100% 100% >|
Line 14: Line 14:
   * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board   * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/lv_board|AD-DRVLV2-EBZ]] - Low voltage drive board
   * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional)   * [[resources/eval/user-guides/ad-fmcmotcon2-ebz/hardware/dyno|AD-DYNO2-EBZ]] - Dynamo-meter Drive System (Optional)
-  * [[http://www.zedboard.org|ZedBoard]]+  * [[http://zedboard.org/product/zedboard|ZedBoard]]
   * 12V - 48V capable DC power supply   * 12V - 48V capable DC power supply
  
Line 33: Line 33:
   * Insert the 5V supply in the left side of the DYNO   * Insert the 5V supply in the left side of the DYNO
   * Power on the ZedBoard   * Power on the ZedBoard
-  * After the ZedBoard is programmed, in order to start the motor, the Emergency Stop switch must be released and then the **Reset** switch must be pressed for a few seconds.+  * After the ZedBoard is programmed, in order to start the motor, the **Emergency Stop** switch must be released and then the **Reset** switch must be pressed for a few seconds.
  
 |< 100% 100% >| |< 100% 100% >|
resources/eval/user-guides/ad-fmcmotcon2-ebz/quickstart/lv_setup_guide.1427718705.txt.gz · Last modified: 30 Mar 2015 14:31 by Andrei Cozma