This shows you the differences between two versions of the page.
Next revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [20 Feb 2015 09:32] – created Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon2-ebz:quickstart:lv_setup_guide [27 Mar 2015 11:28] – [Getting Started] Andrei Cozma | ||
---|---|---|---|
Line 11: | Line 11: | ||
===== Required Hardware ===== | ===== Required Hardware ===== | ||
- | * AD-FMCMOTCON2-EBZ - Controller board. | + | * AD-FMCMOTCON2-EBZ - Controller board |
- | * AD-DRVLV2-EBZ - Low voltage drive board. | + | * AD-DRVLV2-EBZ - Low voltage drive board |
- | * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional). | + | * AD-DYNO2-EBZ - Dynamo-meter Drive System (Optional) |
* [[http:// | * [[http:// | ||
- | * 24V 3A capable | + | * 12V - 48V capable |
|< 100% 100% >| | |< 100% 100% >| | ||
Line 22: | Line 22: | ||
===== Getting Started ===== | ===== Getting Started ===== | ||
- | * Connect the Low voltage drive board to the Controller board. | + | * Connect the hardware as shown in the picture below |
- | * Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard | + | {{: |
- | * Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence of the encoder' | + | * Make sure the **Emergency Stop** switch |
- | {{ : | + | * Insert the DYNO sensor wire in P3 connector on the controller board with the black wire towards the FPGA. In case an encoder is used there is a one to one correspondence of the encoder' |
- | * Insert | + | * Insert the DYNO motor wire in the P2 connector |
- | {{ : | + | * Connect |
- | | + | * Make sure the following LEDs are on: |
- | {{ : | + | * DS1, DS2, DS3 and DS4 on the Controller Board |
- | * Insert the 3 pin motor connector | + | * DS1 and DS2 on the Drive Board |
- | {{ :resources: | + | * Insert the 5V supply in the left side of the DYNO |
* Power on the ZedBoard | * Power on the ZedBoard | ||
- | * After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch | + | * After the board is programmed, in order to start the motor, the Emergency Stop switch |
|< 100% 100% >| | |< 100% 100% >| | ||
^ ^ | ^ ^ | ||
- | {{navigation AD-FMCMOTCON21-EBZ# | + | {{navigation AD-FMCMOTCON2-EBZ# |