This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:lv_setup_guide [10 Feb 2014 16:30] – [Getting Started] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:quickstart:lv_setup_guide [12 Sep 2014 13:13] – [Getting Started] Andrei Cozma | ||
---|---|---|---|
Line 24: | Line 24: | ||
* Connect the Low voltage drive board to the Controller board. | * Connect the Low voltage drive board to the Controller board. | ||
* Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard | * Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard | ||
- | * Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector | + | * Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence of the encoder' |
{{ : | {{ : | ||
* Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM | * Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM | ||
Line 33: | Line 33: | ||
{{ : | {{ : | ||
* Power on the ZedBoard | * Power on the ZedBoard | ||
+ | * After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch S1 must be pressed for a few seconds. | ||
|< 100% 100% >| | |< 100% 100% >| |