Wiki

This version is outdated by a newer approved version.DiffThis version (12 Sep 2014 13:14) was approved by Andrei Cozma.The Previously approved version (21 Feb 2014 14:53) is available.Diff

This is an old revision of the document!


Hardware Setup Guide

Supported Carriers

Required Hardware

  • AD-FMCMOTCON1-EBZ - Controller board.
  • AD-DRVLV1-EBZ - Low voltage drive board.
  • AD-DYNO1-EBZ - Dynamo-meter Drive System (Optional).
  • 24V 3A capable lab power supply.

Getting Started

  • Connect the Low voltage drive board to the Controller board.
  • Connect the Controller + Drive boards assembly to FMC connector of the ZedBoard
  • Insert the 6 pin Hall connector into P7 - pin 1 is the empty slot of the Hall connector. In case an encoder is used there is a one to one corespondence of the encoder's pins to the pins of the P7 connector.

Hall connector

  • Insert the 5V supply in the left side of the DYNAMO-METER DRIVE SYSTEM

Dynamo-meter Drive System

  • Ensure that the Emergency Stop button P2 is pressed (more information about drive board buttons here)

Motor and Power connections

  • Insert the 3 pin motor connector into P1 and connect the lab power supply to P4 (more information about drive board connectors here)

Motor and Power connections

  • Power on the ZedBoard
  • After the board is programmed, in order to start the motor, the Emergency Stop button P2 must be released and then the Reset switch S1 must be pressed for a few seconds.

Navigation - AD-FMCMOTCON1-EBZ

resources/eval/user-guides/ad-fmcmotcon1-ebz/quickstart/lv_setup_guide.1410520434.txt.gz · Last modified: 12 Sep 2014 13:13 by Andrei Cozma