Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:user-guides:ad-fmcmotcon1-ebz:help_and_support [28 Dec 2013 23:18] – update Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:help_and_support [10 Feb 2021 04:45] (current) – add retired Robin Getz |
---|
====== Help and Support ====== | ====== Help and Support ====== |
| {{page>/wiki/common#retired&nofooter&noheader}} |
If you have any questions regarding the AD-FMCMOTCON1-EBZ / AD-DRVLV1-EBZ or are experiencing any problems while using the boards or while following any of the user guides feel free to ask us a question. Questions can be asked on our [[ez>community|EngineerZone support community]]. | If you have any questions regarding the ADI motor drive solutions or are experiencing any problems while using the boards or while following any of the user guides feel free to ask us a question. Questions can be asked on our [[ez>|EngineerZone support community]]. |
| |
For questions regarding the hardware or the HDL reference design please state them in the [[ez>community/fpga|FPGA Reference Designs]] sub-community. For questions regarding the Linux drivers for any of the components on the motor control boards please use the [[ez>community/linux-device-drivers/linux-software-drivers|Linux Software Drivers]] sub-community. | For questions regarding the hardware or the HDL reference design please state them in the [[ez>community/fpga|FPGA Reference Designs]] sub-community. For questions regarding the Linux drivers for any of the components on the motor control boards please use the [[ez>community/linux-device-drivers/linux-software-drivers|Linux Software Drivers]] sub-community. |
| |
For more information also check: | For more information also check: |
* [[http://www.vita.com/fmc.html|VITA's FMC info]] | * [[http://www.vita.com/fmc|VITA's FMC info]] |
* [[|Buy the AD-FMCMOTCON1-EBZ]] | |
* [[|Buy the AD-LVDRV1-EBZ]] | ===== Where to Buy ===== |
| |
| <WRAP round box 90%> |
| **[[http://www.em.avnet.com/en-us/design/drc/Pages/Zynq-Intelligent-Drives-Kit.aspx|ZYNQ Intelligent Drives Kit]]** |
| </WRAP> |
| |
{{navigation AD-FMCMOTCON1-EBZ#matlab_models|Simulink Models#.:|Overview#none}} | {{navigation AD-FMCMOTCON1-EBZ#qdesys_ip|Qdesys Motor Control IP#.:|Overview#none}} |