This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:controller_board [05 Feb 2014 16:18] – [ADC FPGA Interface] Andrei Cozma | resources:eval:user-guides:ad-fmcmotcon1-ebz:hardware:controller_board [05 Feb 2014 17:41] – [Jumper settings] Mihai Bancisor | ||
---|---|---|---|
Line 26: | Line 26: | ||
^ Measurement | ^ Measurement | ||
- | | **[[adi> | + | | **[[AD7401A]]** | 5 kV rms, isolated 2nd order Sigma-Delta modulator | |
| **[[adi> | | **[[adi> | ||
| **[[adi> | | **[[adi> | ||
Line 47: | Line 47: | ||
^ ^ | ^ ^ | ||
+ | ===== Jumper settings ===== | ||
+ | {{: | ||
+ | |< 100% 25% 40% 35% >| | ||
+ | ^ Sensor Selection | ||
+ | | **Back EMF** | P9 - position 0 | P20 - position 0 | | ||
+ | | **Single ended Hall** | P9 - position 1 | P20 - position 0 | | ||
+ | | **Differential Hall** | P9 - position 0 | P20 - position 1 | | ||
+ | | **Reserved** | P9 - position 1 | P20 - position 1 | | ||
+ | ^ Resolver Comfiguration Mode ^^^ | ||
+ | | **Normal Mode - Position input** | P3 - Not inserted | P5 - Not inserted | | ||
+ | | **Normal Mode - Velocity input** | P3 - Not inserted | P5 - Inserted | | ||
+ | | **Reserved** | P3 - Inserted | P5 - Not inserted | | ||
+ | | **Configuration Mode** | P3 - Inserted | P5 - Inserted | | ||
+ | ^ Resolver Resolution Settings | ||
+ | | **10 Bits** | P4 - Not inserted | P6 - Not inserted | | ||
+ | | **12 Bits** | P4 - Not inserted | P6 - Inserted | | ||
+ | | **14 Bits** | P4 - Inserted | P6 - Not inserted | | ||
+ | | **16 Bits** | P4 - Inserted | P6 - Inserted | | ||
+ | ^ PHYs Configuration | ||
+ | | **2.5V VDDO, different PHY addresses** | P11 & P12 - Position 0 | P9 - Inserted | | ||
+ | |||
+ | |||
+ | |< 100% 100% >| | ||
+ | ^ ^ | ||
===== Power Map ===== | ===== Power Map ===== |