This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:user-guides:ad-dac-fmc-ebz [12 Nov 2021 12:50] – [Software support] Laszlo Nagy | resources:eval:user-guides:ad-dac-fmc-ebz [08 Mar 2024 13:32] (current) – Update hdl repo links Stanca-Florina Pop | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== AD-DAC-FMC-EBZ reference HDL design ===== | ===== AD-DAC-FMC-EBZ reference HDL design ===== | ||
- | The [[https:// | + | The [[https:// |
==== HDL source code ==== | ==== HDL source code ==== | ||
Reference can be accessed from the following location: | Reference can be accessed from the following location: | ||
<WRAP center round download> | <WRAP center round download> | ||
- | * https:// | + | * https:// |
</ | </ | ||
Line 49: | Line 49: | ||
==== Configuring the design ==== | ==== Configuring the design ==== | ||
- | | + | |
<code tcl> | <code tcl> | ||
Line 56: | Line 56: | ||
</ | </ | ||
- | A list of the supported DAC devices and JESD operation modes can be found in the [[https:// | + | A list of the supported DAC devices and JESD operation modes can be found in the [[https:// |
To find out more on the JESD operation modes consult the datasheet of the selected DAC. | To find out more on the JESD operation modes consult the datasheet of the selected DAC. | ||
Line 108: | Line 108: | ||
| 00 | 2 | 1 | 1 | 4 | 1 | 16 | 16 | | | 00 | 2 | 1 | 1 | 4 | 1 | 16 | 16 | | ||
| 01 | 4 | 2 | 1 | 4 | 1 | 16 | 16 | | | 01 | 4 | 2 | 1 | 4 | 1 | 16 | 16 | | ||
- | | 02 | + | | 02* |
| 03 | 2 | 2 | 1 | 2 | 1 | 16 | 16 | | | 03 | 2 | 2 | 1 | 2 | 1 | 16 | 16 | | ||
| 04 | 4 | 4 | 1 | 2 | 1 | 16 | 16 | | | 04 | 4 | 4 | 1 | 2 | 1 | 16 | 16 | | ||
Line 119: | Line 119: | ||
| 20 | 1 | 8 | 4 | 1 | 1 | 16 | 16 | | | 20 | 1 | 8 | 4 | 1 | 1 | 16 | 16 | | ||
| 21 | 1 | 8 | 8 | 2 | 1 | 16 | 16 | | | 21 | 1 | 8 | 8 | 2 | 1 | 16 | 16 | | ||
+ | *In mode 02: | ||
+ | * Single-link supported by setting DAC_DATA_WIDTH = 128 | ||
+ | * Dual-link not supported | ||
==== AD9173/ | ==== AD9173/ |