This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:user-guides:ad-96tof1-ebz:ug_jetson [17 Dec 2021 12:59] – [Running the evaluation application] Septimiu Vana | resources:eval:user-guides:ad-96tof1-ebz:ug_jetson [17 Dec 2021 13:00] (current) – [Enabling the point cloud display in aditof-demo] Septimiu Vana | ||
---|---|---|---|
Line 75: | Line 75: | ||
- | ==== Enabling the point cloud display in aditof-demo ==== | ||
- | * The demo application has the capability to display a point cloud image if it detects an OpenCV module called viz. | ||
- | Unfortunately OpenCV does not provide binaries for this module so a manual build is needed. The steps required to | ||
- | install OpenCV and include it in the project are presented here: | ||
- | [[https:// | ||
- | |||
- | * If aditof-demo finds all the OpenCV required modules a button in the interface will allow you to display the point cloud. By toggling the button a separate window will appear. | ||
- | {{ : | ||
==== Troubleshooting ==== | ==== Troubleshooting ==== |