The SDP to FMC Interposer board is an adaptor that allows Xilinx FPGA Eval boards to connect to all daughter boards on the SDP Platform. SDP daughter boards are a wide range of component evaluation boards and Circuits from the Lab (TM) reference circuits. The SDP-I-FMC interposer provides the capabilities to prototype a Xilinx FPGA with an ADI data converter, mixed signal or RF system quickly and easily.
SDP-I-FMC Schematic:
sdp-i-fmc_rev1.pdf
Fig 1 : SDP-I-FMC Intposer Board
The SDP to FMC Interposer routes signals from the FMC connector to the SDP daughter board. There is no additional logic on the board. There is a Low Pin Count (LPC) FMC connector on board. The SDP-I-FMC can only be used with FPGA evaluation boards that have 3.3VIO logic.
The complete setup is shown below:
Example Projects for the KC705 and a range of the SDP daughter boards, which show the basic connectivity between the KC705 and the ADI eval boards, are available on the link below Xilinx Reference Designs