This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:ezlinx:isolated-spi [23 Jul 2012 13:18] – Changes to SPI1 Master jumpers text Hein Marais | resources:eval:ezlinx:isolated-spi [23 Jul 2012 14:58] – Approved Hein Marais | ||
---|---|---|---|
Line 8: | Line 8: | ||
{{ : | {{ : | ||
- | To connect Isolated SPI1 as a master, connect jumpers JP5, JP7, JP9, JP11, JP13, JP15, JP21 and JP36 while leaving jumpers JP6, JP8, JP10, JP12, JP14, JP16, JP20 and JP37 open. To connect Isolated SPI1 as a slave, connect jumpers JP6, JP8, JP10, JP12, JP14 and JP16 while leaving jumpers JP5, JP7, JP9, JP11, JP13 and JP15 open. When connecting SPI1 as a slave JP20 should also be connected, enabling | + | To connect Isolated SPI1 as a master, connect jumpers JP5, JP7, JP9, JP11, JP13, JP15, JP21 and JP36 while leaving jumpers JP6, JP8, JP10, JP12, JP14, JP16, JP20 and JP37 open. To connect Isolated SPI1 as a slave, connect jumpers JP6, JP8, JP10, JP12, JP14, JP16, JP20 and JP37 while leaving jumpers JP5, JP7, JP9, JP11, JP13, JP15, JP21 and JP36 open. When connecting SPI1 as a slave, |
These jumper settings are given in the table below: | These jumper settings are given in the table below: | ||
Line 23: | Line 23: | ||
{{ : | {{ : | ||
- | To connect Isolated SPI2 as a master, connect jumpers JP22, JP24, JP26, JP28, JP30 and JP32 while leaving jumpers JP23, JP25, JP27, JP29, JP31 and JP33 open. To connect Isolated SPI2 as a slave, connect jumpers JP23, JP25, JP27, JP29, JP31 and JP33 while leaving jumpers JP22, JP24, JP26, JP28, JP30 and JP32 open. When connecting SPI2 as a slave JP34 should also be connected, enabling the slave select and serial clock inputs on the [[http:// | + | To connect Isolated SPI2 as a master, connect jumpers JP22, JP24, JP26, JP28, JP30, JP32, JP35 and JP38 while leaving jumpers JP23, JP25, JP27, JP29, JP31, JP33, JP34 and JP39 open. To connect Isolated SPI2 as a slave, connect jumpers JP23, JP25, JP27, JP29, JP31, JP33, JP34 and JP39 while leaving jumpers JP22, JP24, JP26, JP28, JP30, JP32, JP35 and JP38 open. When connecting SPI2 as a slave JP34 should also be connected, enabling the slave select and serial clock inputs on the [[http:// |