Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:ezlinx:isolated-rs485-rs422 [14 Apr 2021 23:35]
Neil Quinn added retired page tag
resources:eval:ezlinx:isolated-rs485-rs422 [14 Apr 2021 23:36]
Neil Quinn Fixed typo
Line 7: Line 7:
 ====== ezLINX™ Isolated RS-485 / RS-422 Implementation====== ====== ezLINX™ Isolated RS-485 / RS-422 Implementation======
  
-The Isolated RS-485 and RS-422 port is implemented using the [[adi>​ADM2587E|ADM2587E]] Signal and Power isolated ​CAN transceiver. The [[adi>​ADM2587E|ADM2587E]] connects to UART2 of the ADSP-BF548 and is capable of functioning at data rates of up to 500kbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>​ADM2587E|ADM2587E]] on the //ez//LINX hardware.+The Isolated RS-485 and RS-422 port is implemented using the [[adi>​ADM2587E|ADM2587E]] Signal and Power isolated ​RS-485 ​transceiver. The [[adi>​ADM2587E|ADM2587E]] connects to UART2 of the ADSP-BF548 and is capable of functioning at data rates of up to 500kbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>​ADM2587E|ADM2587E]] on the //ez//LINX hardware.
  
 \\ \\
resources/eval/ezlinx/isolated-rs485-rs422.txt · Last modified: 14 Apr 2021 23:36 by Neil Quinn