Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |
resources:eval:ezlinx:isolated-rs485-rs422 [14 Apr 2021 23:35] – added retired page tag Neil Quinn | resources:eval:ezlinx:isolated-rs485-rs422 [14 Apr 2021 23:36] (current) – Fixed typo Neil Quinn |
---|
====== ezLINX™ Isolated RS-485 / RS-422 Implementation====== | ====== ezLINX™ Isolated RS-485 / RS-422 Implementation====== |
| |
The Isolated RS-485 and RS-422 port is implemented using the [[adi>ADM2587E|ADM2587E]] Signal and Power isolated CAN transceiver. The [[adi>ADM2587E|ADM2587E]] connects to UART2 of the ADSP-BF548 and is capable of functioning at data rates of up to 500kbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>ADM2587E|ADM2587E]] on the //ez//LINX hardware. | The Isolated RS-485 and RS-422 port is implemented using the [[adi>ADM2587E|ADM2587E]] Signal and Power isolated RS-485 transceiver. The [[adi>ADM2587E|ADM2587E]] connects to UART2 of the ADSP-BF548 and is capable of functioning at data rates of up to 500kbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>ADM2587E|ADM2587E]] on the //ez//LINX hardware. |
| |
\\ | \\ |