This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:ezlinx:isolated-rs232 [28 May 2012 12:53] – Approved Hein Marais | resources:eval:ezlinx:isolated-rs232 [03 Jan 2021 22:04] (current) – fix links Robin Getz | ||
---|---|---|---|
Line 6: | Line 6: | ||
- | The Isolated RS-232 port is implemented using the ADM3252E Signal and Power isolated RS-232 transceiver. The [[http:// | + | The Isolated RS-232 port is implemented using the ADM3252E Signal and Power isolated RS-232 transceiver. The [[adi>adm3252e|ADM3252E]] connects to UART3 of the ADSP-BF548 and is capable of functioning at data rates of up to 460kbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>adm3252e|ADM3252E]] on the //ez//LINX hardware. |
Line 12: | Line 12: | ||
- | The VCC of the [[http:// | + | The VCC of the [[adi>adm3252e|ADM3252E]] is powered with 3.3V and will generate an isolated 3.3V on VISO using ADI’s // |
A three pin screw terminal connector, J6 is used for easy access to the TOUT1(pin 2), RIN1(pin 3) and RS232_ISO_GND(Pin 1) connections. The jumper JP2 when fitted will connect the transmitter output(TOUT1) to the receiver input(RIN1), | A three pin screw terminal connector, J6 is used for easy access to the TOUT1(pin 2), RIN1(pin 3) and RS232_ISO_GND(Pin 1) connections. The jumper JP2 when fitted will connect the transmitter output(TOUT1) to the receiver input(RIN1), | ||