This is an old revision of the document!
The EVAL-ADUM3190S supports the ADuM3190s isolated error amplifier based on Analog Devices, Inc., iCoupler® technology. The ADUM3190S is ideal for linear feedback power supplies with primary side controllers enabling improvements in transient response, power density, and stability as compared to commonly used optocoupler and shunt regulator solutions. Included in the ADUM3190S is a wideband operational amplifier that can be used to set up a variety of commonly used power supply loop compensation techniques. The ADUM3190S is fast enough to allow a feedback loop to react to fast transient conditions and over current conditions. Also included is a high accuracy 1.225 V reference to compare with the supply output set point.
Complete specifications for the ADUM3190S are provided in the ADUM3190S data sheet available from Analog Devices, Inc., and should be consulted in conjunction with this Wiki user guide when using the evaluation board.
The EVAL-ADUM3190S board, shown in Figure 1, can be used to evaluate the performance and data sheet specifications of the ADUM3190S. Figure 2 shows the schematic of the EVAL-ADUM3190S circuit which can be used to test the accuracy of the ADUM3190S and perform other tests. The EVAL-ADUM3190S is a 4-layer PC board, complete with ground and power layers as shown in the Evaluation Board Schematics and Artwork section.
Figure 1. ADuM3190S Evaluation board—EVAL-ADUM3190S
Figure 1. ADuM3190S Evaluation board—EVAL-ADUM3190S
The evaluation board layout, BOM, and schematic files for the EVAL-AD9246S board can be downloaded from the links below.
DISCLAIMER: The footprint used for layout on the evaluation board is provided for general reference only. The exact footprint required for mounting this device onto a printed circuit board will depend on the device lead forming and may differ from what is provided herein. It is recommended to generate specific footprint information from the users lead forming specifications when placing this device on the application printed circuit board.
The canvas files required to run the EVAL-AD9246S board need to be downloaded, unzipped, and saved to an accessible location.
The canvas files can be downloaded from here:
ad9246s_va_canvases.zip
The FPGa file can be download from here:
ad9265_cmos.zip
This section provides quick start procedures for using the EVAL-AD9246S board. Both the default and optional settings are described.