This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:dpg:eval-ad9783 [20 Feb 2023 01:59] – John Marco Mina | resources:eval:dpg:eval-ad9783 [20 Feb 2023 04:03] – John Marco Mina | ||
---|---|---|---|
Line 50: | Line 50: | ||
- Attach [[adi> | - Attach [[adi> | ||
- Connect controller board (SDP-H1/ | - Connect controller board (SDP-H1/ | ||
- | - Connect the evaluation board to PC via USB and to a 5Vdc 1A power supply on P5 and P6. Refer to Figure 1. | + | - Connect the evaluation board to PC via USB and to a 5Vdc 1A power supply on P5 and P6. Refer to Figures 1a and 1b. |
- Connect continuous wave generator for clock input to SMA J1 and DAC output from SMA J5 (IOUT1P) or SMA J9 (IOUT2P) to a signal/ | - Connect continuous wave generator for clock input to SMA J1 and DAC output from SMA J5 (IOUT1P) or SMA J9 (IOUT2P) to a signal/ | ||
- Set clock input to 200MHz, 3dBm. | - Set clock input to 200MHz, 3dBm. | ||
Line 59: | Line 59: | ||
- The default values for the register is displayed and set. The values can be changed on the Chip View GUI, or on the **Memory Map** for registers not available in the GUI. For more info on the memory map, refer to [[adi> | - The default values for the register is displayed and set. The values can be changed on the Chip View GUI, or on the **Memory Map** for registers not available in the GUI. For more info on the memory map, refer to [[adi> | ||
//Figure 4. Apply Changes and Read All button | //Figure 4. Apply Changes and Read All button | ||
- | - Start DPG Downloader Lite. The controller board (SDP-H1/ | + | - Start DPG Downloader Lite. The controller board (SDP-H1/ |
- | - In DPG Downloader Lite, from the **Add Generator Waveforms** pulldown menu select **Single Tone** and apply the settings as shown in Figure 5. Set the **Data Rate** to 200MHz and Desired Frequency to 16MHz. Set **DAC Resolution** to 16 for AD9783, 14 for AD9781, and 12 for AD9780. Uncheck the **Unsigned Data** box and Check the **Generate Complex Data (I & Q)**. | + | - In DPG Downloader Lite, from the **Add Generator Waveforms** pulldown menu select **Single Tone** and apply the settings as shown in Figures 5a and 5b. Set the **Data Rate** to 200MHz and Desired Frequency to 16MHz. Set **DAC Resolution** to 16 for AD9783, 14 for AD9781, and 12 for AD9780. Uncheck the **Unsigned Data** box and Check the **Generate Complex Data (I & Q)**. |
- Select the I/Q tone from the **I/Q Data Vector** pulldown menu. | - Select the I/Q tone from the **I/Q Data Vector** pulldown menu. | ||
- Press the download arrow and then the play button. The spectrum similar to Figure 6 should appear in the signal/ | - Press the download arrow and then the play button. The spectrum similar to Figure 6 should appear in the signal/ |