Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:dpg:ad9739-ebz [20 Sep 2021 09:27] – Update to SDPH1 and ADSV7 Melissa Lorenz Lacanlaleresources:eval:dpg:ad9739-ebz [15 Feb 2022 02:28] (current) – [Software Needed:] Melissa Lorenz Lacanlale
Line 33: Line 33:
 =====Software Needed:===== =====Software Needed:=====
   * [[:resources:tools-software:ace|Analysis | Control | Evaluation (ACE) Software]]   * [[:resources:tools-software:ace|Analysis | Control | Evaluation (ACE) Software]]
-  * [[:resources:tools-software:ace:dpg-lite|DPG Lite]] or [[:resources:eval:dpg:dpgdownloader|DPG Downloader]]+  * [[:resources:tools-software:ace:dpg-lite|DPG Lite]] (Recommended; Installed with ACE)  or [[:resources:eval:dpg:dpgdownloader|DPG Downloader]] 
 + <note important>**Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources:tools-software:ace:knownissues#high-speed_dac_eval_boards_are_not_discovered|here]].</note> 
  
 =====Hardware Needed:===== =====Hardware Needed:=====
   * [[adi>eval-ad9739|AD9739-R2-EBZ]] Evaluation Board   * [[adi>eval-ad9739|AD9739-R2-EBZ]] Evaluation Board
   * [[:resources:eval:dpg:hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:resources:eval:ads7-v2|ADS7-V2EBZ]]    * [[:resources:eval:dpg:hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:resources:eval:ads7-v2|ADS7-V2EBZ]] 
-  * Evaluation Kit 
   * [[adi>AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board   * [[adi>AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board
   * 5Vdc 2A Power Supply   * 5Vdc 2A Power Supply
Line 56: Line 57:
  
 =====Quick Start Guide===== =====Quick Start Guide=====
-  - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB and a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b.+  - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USBa 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b.
      * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.      * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart.
      * If using **ADS7-V2**, set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.      * If using **ADS7-V2**, set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply.
Line 63: Line 64:
      * If using **ADS7-V2**, The first three indicators should light up as shown in figure 2b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP>      * If using **ADS7-V2**, The first three indicators should light up as shown in figure 2b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP>
   - Double click the AD9739 Box to open chip view.    - Double click the AD9739 Box to open chip view. 
-     * If using **SDP-H1**, The DLL_LOCKED indicator should be enabled as shown in figure 3a.+     * If using **SDP-H1**, The DLL_LOCKED indicator should light up as shown in figure 3a.
      * If using **ADS7-V2**, All three indicators should light up as shown in figure 3b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_chipview.png?nolink&600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_adsv7_ace_chipview.png?nolink&600 |{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP>      * If using **ADS7-V2**, All three indicators should light up as shown in figure 3b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_chipview.png?nolink&600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_adsv7_ace_chipview.png?nolink&600 |{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP>
   - Start DPG Lite or DPG Downloader.   - Start DPG Lite or DPG Downloader.
-    * At the SDP-H1 part of the softwarethe device part number and **DCO frequency** of around **75 MHz** should be displayed. +    * At the SDP-H1 settingsensure that Evaluation board is equal to AD9739 and **DCO frequency** of around **75 MHz** should be displayed. 
-    * At the ADS7-V2 part of the softwarethe device part number and **DCO frequency** of around **500 MHz** should be displayed.+    * At the ADS7-V2 settingsensure that Evaluation board is equal to AD9739 and **DCO frequency** of around **500 MHz** should be displayed.
   - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b.    - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. 
     * When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz.     * When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz.
Line 78: Line 79:
 =====Troubleshooting===== =====Troubleshooting=====
 This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur:
-  * Check the supply voltage of the evaluation board. Voltage rail should be 3.3V.+  * Check if the Voltage supply test points of the evaluation board has the correct value
   * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up.   * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up.
   * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up.   * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up.
resources/eval/dpg/ad9739-ebz.1632122877.txt.gz · Last modified: 20 Sep 2021 09:27 by Melissa Lorenz Lacanlale