This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9739-ebz [14 Sep 2021 10:08] – Update to SDPH1 and ADSV7 Melissa Lorenz Lacanlale | resources:eval:dpg:ad9739-ebz [15 Feb 2022 02:28] (current) – [Software Needed:] Melissa Lorenz Lacanlale | ||
---|---|---|---|
Line 33: | Line 33: | ||
=====Software Needed: | =====Software Needed: | ||
* [[: | * [[: | ||
- | * [[: | + | * [[: |
+ | < | ||
=====Hardware Needed: | =====Hardware Needed: | ||
- | * [[adi> | + | * [[adi> |
* [[: | * [[: | ||
- | * Evaluation Kit | ||
* [[adi> | * [[adi> | ||
* 5Vdc 2A Power Supply | * 5Vdc 2A Power Supply | ||
Line 56: | Line 57: | ||
=====Quick Start Guide===== | =====Quick Start Guide===== | ||
- | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/ | + | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/ |
* If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | ||
* If using **ADS7-V2**, | * If using **ADS7-V2**, | ||
- | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9739 evaluation board. From the AD9739-EBZ tab, Click **“Run Example Startup Routine (Sync Disabled)”**. | + | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9739 evaluation board. From the AD9739-EBZ tab, Click **“Run Example Startup Routine (Sync Disabled)”**. |
- | - Double click the AD9739 Box to open chip view. The **DLL_LOCKED** indicator should | + | * If using **SDP-H1**, The MU Controller Locked |
+ | * If using **ADS7-V2**, The first three indicators | ||
+ | - Double click the AD9739 Box to open chip view. | ||
+ | * If using **SDP-H1**, The DLL_LOCKED | ||
+ | * If using **ADS7-V2**, | ||
- Start DPG Lite or DPG Downloader. | - Start DPG Lite or DPG Downloader. | ||
- | * At the SDP-H1 | + | * At the SDP-H1 |
- | * At the ADS7-V2 | + | * At the ADS7-V2 |
- In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. | - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. | ||
* When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz. | * When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz. | ||
* When using ADS-V2, set **Data Rate** to 2 GHz and **Desired Frequency** to 180 MHz. | * When using ADS-V2, set **Data Rate** to 2 GHz and **Desired Frequency** to 180 MHz. | ||
- | - Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 14 bits. Check off the **Unsigned Data** box.\\ <WRAP centeralign> | + | - Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 14 bits. Check off the **Unsigned Data** box. |
- | - Select the Single Tone from the **Data Vector** pulldown menu | + | - Select the Single Tone from the **Data Vector** pulldown menu \\ <WRAP centeralign> |
- Press the download arrow and then the play button. The FFT plots similar to Figures 5a and 5b should appear in the signal/ | - Press the download arrow and then the play button. The FFT plots similar to Figures 5a and 5b should appear in the signal/ | ||
Line 74: | Line 79: | ||
=====Troubleshooting===== | =====Troubleshooting===== | ||
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | ||
- | * Check the supply | + | * Check if the Voltage |
* Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | ||
* Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. | * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. |