Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:dpg:ad9739-ebz [20 Sep 2021 09:27] – Update to SDPH1 and ADSV7 Melissa Lorenz Lacanlale | resources:eval:dpg:ad9739-ebz [15 Feb 2022 02:28] (current) – [Software Needed:] Melissa Lorenz Lacanlale |
---|
=====Software Needed:===== | =====Software Needed:===== |
* [[:resources:tools-software:ace|Analysis | Control | Evaluation (ACE) Software]] | * [[:resources:tools-software:ace|Analysis | Control | Evaluation (ACE) Software]] |
* [[:resources:tools-software:ace:dpg-lite|DPG Lite]] or [[:resources:eval:dpg:dpgdownloader|DPG Downloader]] | * [[:resources:tools-software:ace:dpg-lite|DPG Lite]] (Recommended; Installed with ACE) or [[:resources:eval:dpg:dpgdownloader|DPG Downloader]] |
| <note important>**Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources:tools-software:ace:knownissues#high-speed_dac_eval_boards_are_not_discovered|here]].</note> |
| |
=====Hardware Needed:===== | =====Hardware Needed:===== |
* [[adi>eval-ad9739|AD9739-R2-EBZ]] Evaluation Board | * [[adi>eval-ad9739|AD9739-R2-EBZ]] Evaluation Board |
* [[:resources:eval:dpg:hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:resources:eval:ads7-v2|ADS7-V2EBZ]] | * [[:resources:eval:dpg:hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:resources:eval:ads7-v2|ADS7-V2EBZ]] |
* Evaluation Kit | |
* [[adi>AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board | * [[adi>AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board |
* 5Vdc 2A Power Supply | * 5Vdc 2A Power Supply |
| |
=====Quick Start Guide===== | =====Quick Start Guide===== |
- Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB and a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b. | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J3, and the DAC output from J1 to a signal/spectrum analyzer. Connect the evaluation board to PC via USB, a 5Vdc 2A power supply to J17. Refer to Figures 1a and 1b. |
* If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. | * If using **SDP-H1**, set clock input to **300 MHz and 0 dBm**. Connect SDP-H1 to PC via USB and to a 12Vdc wall wart. |
* If using **ADS7-V2**, set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply. | * If using **ADS7-V2**, set the clock input to **2 GHz and 0 dBm**. Connect ADS-V2 to PC via USB and to a 12V 60W AC/DC power supply. Switch the board ON using S1 beside the connector for 12V supply. |
* If using **ADS7-V2**, The first three indicators should light up as shown in figure 2b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> | * If using **ADS7-V2**, The first three indicators should light up as shown in figure 2b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 2a. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> |
- Double click the AD9739 Box to open chip view. | - Double click the AD9739 Box to open chip view. |
* If using **SDP-H1**, The DLL_LOCKED indicator should be enabled as shown in figure 3a. | * If using **SDP-H1**, The DLL_LOCKED indicator should light up as shown in figure 3a. |
* If using **ADS7-V2**, All three indicators should light up as shown in figure 3b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_chipview.png?nolink&600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_adsv7_ace_chipview.png?nolink&600 |{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> | * If using **ADS7-V2**, All three indicators should light up as shown in figure 3b. <WRAP centeralign>{{ :resources:eval:dpg:ad9739_ace_chipview.png?nolink&600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</WRAP> <WRAP centeralign>{{ :resources:eval:dpg:ad9739_adsv7_ace_chipview.png?nolink&600 |{{ :resources:eval:dpg:ad9739_ads7_ace_boardview.png?nolink&600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</WRAP> |
- Start DPG Lite or DPG Downloader. | - Start DPG Lite or DPG Downloader. |
* At the SDP-H1 part of the software, the device part number and **DCO frequency** of around **75 MHz** should be displayed. | * At the SDP-H1 settings, ensure that Evaluation board is equal to AD9739 and **DCO frequency** of around **75 MHz** should be displayed. |
* At the ADS7-V2 part of the software, the device part number and **DCO frequency** of around **500 MHz** should be displayed. | * At the ADS7-V2 settings, ensure that Evaluation board is equal to AD9739 and **DCO frequency** of around **500 MHz** should be displayed. |
- In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. | - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. |
* When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz. | * When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz. |
=====Troubleshooting===== | =====Troubleshooting===== |
This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: | This section lists items to check and practices to use when debugging any unexpected performance of a board. If unexpected results occur: |
* Check the supply voltage of the evaluation board. Voltage rail should be 3.3V. | * Check if the Voltage supply test points of the evaluation board has the correct value. |
* Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. | * Check if all (3) blue LEDs on the AD-DAC-FMC-ADP board is lit up. Reconnect the board to the FMC connector of SDP-H1 if not lit up. |
* Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. | * Check if the SDP-H1 is being supplied properly by 12Vdc adaptor. Some LEDs on the SDP-H1 should lit up. |