Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:eval:dpg:ad9739-ebz [21 Sep 2021 10:16]
Melissa Lorenz Lacanlale [Quick Start Guide]
resources:eval:dpg:ad9739-ebz [28 Sep 2021 07:26] (current)
Melissa Lorenz Lacanlale Update to SDPH1 and ADSV7
Line 38: Line 38:
   * [[adi>​eval-ad9739|AD9739-R2-EBZ]] Evaluation Board   * [[adi>​eval-ad9739|AD9739-R2-EBZ]] Evaluation Board
   * [[:​resources:​eval:​dpg:​hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:​resources:​eval:​ads7-v2|ADS7-V2EBZ]] ​   * [[:​resources:​eval:​dpg:​hsdac-sdp-h1|SDP-H1]] (EVAL-SDP-CH1Z) or [[:​resources:​eval:​ads7-v2|ADS7-V2EBZ]] ​
-  * Evaluation Kit 
   * [[adi>​AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board   * [[adi>​AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board
   * 5Vdc 2A Power Supply   * 5Vdc 2A Power Supply
Line 66: Line 65:
      * If using **ADS7-V2**,​ All three indicators should light up as shown in figure 3b. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ace_chipview.png?​nolink&​600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</​WRAP>​ <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_adsv7_ace_chipview.png?​nolink&​600 |{{ :​resources:​eval:​dpg:​ad9739_ads7_ace_boardview.png?​nolink&​600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</​WRAP>​      * If using **ADS7-V2**,​ All three indicators should light up as shown in figure 3b. <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_ace_chipview.png?​nolink&​600 |}}//Figure 3a. ACE Initial Board Configuration Wizard for SDP-H1//</​WRAP>​ <WRAP centeralign>​{{ :​resources:​eval:​dpg:​ad9739_adsv7_ace_chipview.png?​nolink&​600 |{{ :​resources:​eval:​dpg:​ad9739_ads7_ace_boardview.png?​nolink&​600 |}}//Figure 3b. ACE Initial Board Configuration Wizard for ADS7-V2//</​WRAP>​
   - Start DPG Lite or DPG Downloader.   - Start DPG Lite or DPG Downloader.
-    * At the SDP-H1 ​part of the softwarethe device part number ​and **DCO frequency** of around **75 MHz** should be displayed. +    * At the SDP-H1 ​settingsensure that Evaluation board is equal to AD9739 ​and **DCO frequency** of around **75 MHz** should be displayed. 
-    * At the ADS7-V2 ​part of the softwarethe device part number ​and **DCO frequency** of around **500 MHz** should be displayed.+    * At the ADS7-V2 ​settingsensure that Evaluation board is equal to AD9739 ​and **DCO frequency** of around **500 MHz** should be displayed.
   - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b.    - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 4a and 4b. 
     * When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz.     * When using SDP-H1, set **Data Rate** to 300 MHz and **Desired Frequency** to 20 MHz.
resources/eval/dpg/ad9739-ebz.txt · Last modified: 28 Sep 2021 07:26 by Melissa Lorenz Lacanlale