This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9154-ace-fmc-ebz [30 Nov 2015 19:40] – d Larry Welch | resources:eval:dpg:ad9154-ace-fmc-ebz [07 Feb 2023 09:22] (current) – Quick Start Guide Shine Cabatan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== | + | ====== |
- | ===== Getting Started with the AD9154-FMC-EBZ Evaluation Board and Software ===== | + | |
- | ==== What's in the Box ==== | + | |
- | * [[adi> | + | |
- | * Evaluation Board CD | + | |
- | * Mini-USB Cable | + | |
- | ==== Recommended Equipment List ==== | + | |
- | * Sinusoidal Clock Source | + | |
- | * Spectrum Analyzer | + | |
- | * Oscilloscope | + | |
- | * Data Pattern Generator with FMC Interface ADS7 | + | |
- | ===== Introduction ====== | + | |
- | The AD9154-FMC-EBZ connects to an ADS7 data pattern generator system. The AD9154 is a quad JESD204B signal processing RF Digital to Analog Converter. The ADS7 automatically formats the data and sends it to the AD9154-FMC-EBZ via its JESD204B lanes. The AD9154-FMC-EBZ is an FMC mezzanine card. +12V, +3.3V, and VADJ power supply rails are provided by the ADS7 system via the FMC connector P1. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, JESD204B SYSREF signals, and a GBTCLK clock used by the ADS7. There is also an FMC standard I2C bus that is used by the ADS7 to identify the AD9154-FMC-EBZ. This I2C interface is implemented in firmware in the AD9154-FMC-EBZ PIC processor (XU1). PIC firmware is installed in PIC non-volatile memory by ADI. All ADS7 to/from AD9154-FMC-EBZ interface signals are connected via the FMC connector P1. | + | |
- | ===== AD9154 Evaluation Software ===== | + | |
- | The AD9154 Evaluation Board software runs on the ADI ACE graphical user interface (GUI). ACE is included on the Evaluation board CD. Registers on the AD9154 and AD9516 products are programmed by the ACE software via a USB cable connecting the user’s PC to the AD9154-FMC-EBZ XP2 connector. Software in the AD9154-FMC-EBZ PIC processor (XU1) provides the interface between the USB bus and the SPI busses of the AD9154 and AD9516. | + | |
- | ===== Hardware Setup ===== | + | |
- | | + | |
- | <WRAP center> | + | |
- | {{: | + | |
- | | Figure 1. AD9154-FMC-EBZ Lab Block Diagram | + | |
- | {{: | + | |
- | | Figure 2. Top and Bottom view of AD9154-FMC-EBZ | + | |
- | </ | + | |
- | A low phase noise high frequency clock source should be connected to the SMA connector J1. A spectrum analyzer should be connected to the EVB SMA connector J4. Connect SMA connectors J5, J14 and J17 of the EVB to an oscilloscope. The evaluation board connects to the ADS7 through the connector P1. The PC should be connected to the EVB using the mini-USB connector XP2. Figure 1 shows a block diagram of the set-up. | + | |
- | ===== Getting Started ===== | + | |
- | The PC software is included in the CD shipped with the EVB. The installation will include the software as well as all the AD9154 EVB files including schematic, board layout, datasheet, this quick start guide and other files. | + | |
- | ==== Initial Set-Up ==== | + | |
- | 1. Install the customer evaluation board software and support files, including DPGDownloader and ACE GUI on your PC. Follow the instructions in the installation wizard and use the default (recommended) installation settings. | + | |
- | 2. Plug the AD9154-FMC-EBZ into port FMC_1 of the ADS7 System. Use a USB cable to connect the EVB to your PC and connect the lab equipment to the EVB as shown in Figure 1. \\ \\ | + | |
- | 3. Connect the ADS7 unit to your PC via USB and turn on the ADS7. \\ \\ | + | |
- | 4. Connect SMA connector J5 to a spectrum analyzer, connect SMA connectors J17, J4 and J14 to an oscilloscope. | + | |
- | ==== Single Tone Demonstration ==== | + | |
- | === Single Tone Demo Lab Bench Configuration Procedure: | + | |
- | These settings configure the AD9154 to output a 180Mhz 0dbFS sine wave using the ADS7 on all four AD9154 DACs. | + | ===== Preface ===== |
- | - Configure | + | This user guide describes both the hardware |
- | <WRAP center> | + | The [[adi>EVAL-AD9154|AD9154-FMC-EBZ]] is an FMC mezzanine card and connects to an [[adi> |
- | {{: | + | ===== Typical Setup ===== |
- | | Figure 3. Initial DPG Downloader Panel | | + | |
- | </ | + | |
- | === Single Tone Demo Hardware and Software Start Up Procedure:=== | + | |
- | 1. Run DPG Downloader from Start-> | + | |
- | < | + | < |
- | 2. Open ACE from Start-> | + | |
- | 3. Press the AD9154 icon and populate the AD9154 initialization wizard as shown in figure 4b, JESD mode 0, Interpolation 2. Leave all other settings in their default state. Press rhe APPLY button. JESD204B PLL lock will turn green as shown in figure 4c. Press the AD9154 icon in the initialization wizard tab. The AD9154 block diagram view will appear populated as shown in figure 4d.\\ \\ | + | |
- | <WRAP center> | + | |
- | {{: | + | |
- | | | + | |
- | {{: | + | |
- | | Figure 4b. ACE AD9154 Initialization Wizard tab with selections made | | + | |
- | {{: | + | |
- | | Figure 4c. ACE AD9154 Initialization Wizard tab after pressing APPLY | | + | |
- | {{: | + | |
- | | Figure 4d. ACE AD9154 Block Diagram View after Initialization | + | |
- | </ | + | |
- | 4. In DPG Downloader Window Select Single Tone under the Add Generated Waveforms Tab. Set Data Rate: 750Mhz, Desired Frequency: 180Mhz, Amplitude: 0dbFS, Uncheck Unsigned Data, Check Generate Complex Data (I&Q) | + | |
- | 5. Select JESD Mode: Mode 0, Select Subclass 0 | + | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</ |
- | 6. Populate the data playback selections for each DAC output as shown in Figure 5. | + | ===== Helpful Files/Links ===== |
- | 7. Click Download button and click Play button. The signals shown in figures 6 and 7 will appear on the DAC outputs (J17, J4, J5, and J14), Serial Line Rate will be 7.5Gbps. The green SYNC check mark indicates that the JESD204B link is up and running. | + | * User Guides for non-FMC card users: |
+ | * [[: | ||
+ | * [[: | ||
+ | * [[: | ||
+ | * Datasheet: [[adi> | ||
+ | * IBIS Model: [[ibis> | ||
+ | * AMI Model: [[https:// | ||
+ | * Schematic: {{: | ||
+ | * Bill of Materials: {{: | ||
+ | * PCB Gerber Files: {{: | ||
+ | * PCB BRD File: {{: | ||
+ | * PCB Layout PDF: {{: | ||
+ | ===== Software Needed ===== | ||
- | <WRAP center> | + | * [[:resources:tools-software:ace|Analysis |
- | {{:resources:eval:dpg: | + | * [[: |
- | | | + | * [[adi>plugins/ |
- | </WRAP> | + | |
- | 8. Here’s what you will see on DAC0, DAC1, and DAC3 on the scope \\ \\ | + | <note important> |
+ | * Do not install ACE on a computer with DAC Software Suite. | ||
+ | * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources: | ||
+ | </ | ||
- | + | ===== Hardware Needed ===== | |
- | <WRAP center> | + | * [[adi>EVAL-AD9154|AD9154-FMC-EBZ]] Evaluation Board which comes with: |
+ | * USB-A to USB-Mini Cable | ||
+ | * [[: | ||
+ | * 12V 60W AC/DC Power Supply | ||
+ | * Power Cord | ||
+ | * USB-A to USB-B Cable | ||
+ | * PC with ACE and DPG Lite Software Applications | ||
+ | * Low Phase Noise High-Frequency Continuous Wave Generator | ||
+ | * Signal/ | ||
+ | * 2 to 5 SMA Cables | ||
+ | ===== Quick Start Guide ===== | ||
- | 9. Here is what you will see at the output of DAC2 on the Spectrum Analyzer. | + | - Attach AD9154-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect |
+ | - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output.< | ||
+ | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device | ||
+ | - Open ACE. The board will automatically be recognized by the software as shown in Figure 3. Otherwise, install the plugin for AD9154 evaluation board by following the steps in this page: [[: | ||
+ | - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 4. JESD204B PLL should lock and the indicator should turn green. | ||
+ | * **Links:** Single Link | ||
+ | * **JESD Mode:** 0 | ||
+ | * **Subclass1: | ||
+ | * **Interpolation: | ||
+ | * **DAC PLL:** False | ||
+ | * **FDAC:** 1.5 GHz <WRAP centeralign> | ||
+ | - In DPG Lite or DPG Downloader, configure single tone waveform generation. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Apply the following settings: | ||
+ | * **Data Rate:** 750 MHz | ||
+ | * **Desired Frequency: | ||
+ | * **DAC Resolution: | ||
+ | * **Amplitude: | ||
+ | * **Unsigned Data:** unchecked | ||
+ | * **Generate Complex Data (I & Q):** checked | ||
+ | - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0. <WRAP centeralign> | ||
+ | - Press the download arrow ({{: | ||
- | {{: | ||
- | |||
- | | Figure 6. DAC Output Spectrum Analyzer Display | ||
- | </ | ||
- | |||
- | {{: | ||
- | | |