Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:dpg:ad9136-fmc-ebz [02 Aug 2022 10:21] – [Quick Start Guide] Shine Cabatan | resources:eval:dpg:ad9136-fmc-ebz [11 Oct 2022 14:05] (current) – [Software Needed] Shine Cabatan |
---|
<WRAP centeralign>{{ :resources:eval:dpg:ad9135-fmc-ebz_setup_with_label.jpg?600 |}}//Figure 1a. AD9135-FMC-EBZ Setup with ADS7-V2EBZ//</WRAP> | <WRAP centeralign>{{ :resources:eval:dpg:ad9135-fmc-ebz_setup_with_label.jpg?600 |}}//Figure 1a. AD9135-FMC-EBZ Setup with ADS7-V2EBZ//</WRAP> |
| |
<WRAP centeralign>{{ :resources:eval:dpg:ad9135-fmc-ebz_setup_with_label.jpg?600 |}}//Figure 1b. AD9135-FMC-EBZ Setup with ADS8-V1EBZ//</WRAP> | <WRAP centeralign>{{ :resources:eval:dpg:ad9135-fmc-ebz_setup2_with_labels.jpg?600 |}}//Figure 1b. AD9135-FMC-EBZ Setup with ADS8-V1EBZ//</WRAP> |
| |
<WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_setup_with_label.jpg?600 |}}//Figure 2a. AD9136-FMC-EBZ Setup with ADS7-V2EBZ//</WRAP> | <WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_setup_with_labels.jpg?600 |}}//Figure 2a. AD9136-FMC-EBZ Setup with ADS7-V2EBZ//</WRAP> |
| |
<WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_setup_with_label.jpg?600 |}}//Figure 2b. AD9136-FMC-EBZ Setup with ADS8-V1EBZ//</WRAP> | <WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_setup2_with_labels.jpg?600 |}}//Figure 2b. AD9136-FMC-EBZ Setup with ADS8-V1EBZ//</WRAP> |
| |
<note tip>Tip: Click on any picture in this guide to open an enlarged version.</note> | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</note> |
| |
* [[:resources:eval:dpg:ad9136-ebz|AD9135-EBZ/AD9136-EBZ User Guide]] for non-FMC card users | * [[:resources:eval:dpg:ad9136-ebz|AD9135-EBZ/AD9136-EBZ User Guide]] for non-FMC card users |
| * [[:resources:eval:dpg:ads7|ADS7-V1/-V2 for High-Speed DAC Evaluation]] |
* Datasheet: [[adi>media/en/technical-documentation/data-sheets/AD9135_9136.pdf|AD9135/AD9136]] | * Datasheet: [[adi>media/en/technical-documentation/data-sheets/AD9135_9136.pdf|AD9135/AD9136]] |
* IBIS Model: [[ibis>ad9135bcpz|AD9135]],[[ibis>ad9136bcpz|AD9136]] | * IBIS Model: [[ibis>ad9135bcpz|AD9135]],[[ibis>ad9136bcpz|AD9136]] |
* ACE Plugin for Specific Device: [[adi>plugins/ace/board.ad9135.1.2020.12100.acezip|AD9135]], [[adi>plugins/ace/board.ad9136.1.2020.12100.acezip|AD9136]] | * ACE Plugin for Specific Device: [[adi>plugins/ace/board.ad9135.1.2020.12100.acezip|AD9135]], [[adi>plugins/ace/board.ad9136.1.2020.12100.acezip|AD9136]] |
| |
<note important>**Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources:tools-software:ace:knownissues#high-speed_dac_eval_boards_are_not_discovered|here]].</note> | <note important> |
| * Do not install ACE on a computer with DAC Software Suite. |
| * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources:tools-software:ace:knownissues#high-speed_dac_eval_boards_are_not_discovered|here]]. |
| </note> |
| |
===== Hardware Needed ===== | ===== Hardware Needed ===== |
===== Quick Start Guide ===== | ===== Quick Start Guide ===== |
| |
- Attach AD9135-FMC-EBZ/AD9136-FMC-EBZ onto the FMC connector of ADS7-V2 or ADS8-V1 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, the DAC output at J17 to a signal/spectrum analyzer, and, if desired, the other DAC output at J5 to an oscilloscope. Connect ADS7-V2/ADS8-V1 to PC via USB and to a 12V 60W AC/DC power supply, then switch the board ON using S1 beside the connector for 12V supply. Refer to [[:resources:eval:dpg:ad9136-fmc-ebz|Typical Setup]] section for pictures of actual evaluation setup. | - Attach AD9135-FMC-EBZ/AD9136-FMC-EBZ onto the FMC connector of ADS7-V2 or ADS8-V1 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, the DAC output at J17 to a signal/spectrum analyzer, and, if desired, the other DAC output at J5 to an oscilloscope. Connect ADS7-V2/ADS8-V1 to PC via USB and to a 12V 60W AC/DC power supply, then switch the board ON using S1 beside the connector for 12V supply. Refer to [[:resources:eval:dpg:ad9136-fmc-ebz#typical_setup|Typical Setup]] section for pictures of actual evaluation setup. |
- Set the frequency of the continuous waveform generator output to **2.0 GHz** and the output level to **+3 dBm**. Enable the output. | - Set the frequency of the continuous waveform generator output to **2.0 GHz** and the output level to **+3 dBm**. Enable the output.<WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_dpg_board_detect.png?600 |}}//Figure 3. ADS7-V2 and AD9136 detected in DPG Software//</WRAP> |
- Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, respectively. <insert figures> | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, respectively. <WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_ace_board_detect.png?600 |}}//Figure 4. AD9136-FMC-EBZ detected in ACE//</WRAP> |
- Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9135/AD9136 evaluation board by following the steps in this page: [[:resources:tools-software:ace:userguide:quickstart|Quickstart - ACE Quickstart and Plug-in Installation]]. | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9135/AD9136 evaluation board by following the steps in this page: [[:resources:tools-software:ace:userguide:quickstart|Quickstart - ACE Quickstart and Plug-in Installation]]. <WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_ace_configuration_wizard.png?600 |}}//Figure 5. ACE Initial Configuration Wizard//</WRAP><WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_ace_chipview.png?600 |}}//Figure 6. ACE AD9136 Chipview Tab//</WRAP> |
- In ACE, apply the configuration wizard settings enumerated below and shown in Figure <>. JESD204B PLL should lock and the indicator should turn green. | - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 5. JESD204B PLL should lock and the indicator should turn green. |
* **Links:** Dual Link | * **Links:** Dual Link |
* **JESD Mode:** 8 | * **JESD Mode:** 8 |
* **Interpolation:** 1 | * **Interpolation:** 1 |
* **DAC PLL:** False | * **DAC PLL:** False |
* **FDAC:** 2 GHz | * **FDAC:** 2 GHz<WRAP centeralign>{{ :resources:eval:dpg:ad9136-fmc-ebz_dpg_output_generation.png?600 |}}//Figure 7. Single Tone and ADS7-V2 Configuration Panels in DPG//</WRAP> |
- In DPG Lite or DPG Downloader, configure generation of two single tone waveforms. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Do this two times then configure the panels as follows: | - In DPG Lite or DPG Downloader, configure generation of two single tone waveforms. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Do this two times then configure the panels as follows: |
* **Data Rate** = 2 GHz, **Amplitude** = -1dBFS, **Unsigned Data** is unchecked for both panels. | * **Data Rate** = 2 GHz, **Amplitude** = -1dBFS, **Unsigned Data** is unchecked for both panels. |
* **Desired Frequency = 112 MHz** in one panel while **Desired Frequency = 221 MHz** in the other. | * **Desired Frequency = 112 MHz** in one panel while **Desired Frequency = 221 MHz** in the other. |
* If using AD9135, set **DAC Resolution** to **11 bits**. Otherwise, leave as is (16 bits). | * If using AD9135, set **DAC Resolution** to **11 bits**. Otherwise, leave as is (16 bits). |
- In the ADS7-V2 or ADS8-V1 panel in the DPG window, configure **Data Playback** by selecting tone2 for DAC0 and tone1 for DAC1. Set **JESD Mode** to Mode 8, **Links** to Dual, and **Subclass** to 1. | - In the ADS7-V2 or ADS8-V1 panel in the DPG window, configure **Data Playback** by selecting tone2 for DAC0 and tone1 for DAC1. Set **JESD Mode** to Mode 8, **Links** to Dual, and **Subclass** to 1. <WRAP centeralign> {{ :resources:eval:dpg:ad9136:ad9136-35_dac0_sa_output.png?600 | }}//Figure 8. DAC0 Output Spectrum Analyzer Display// </WRAP> <WRAP centeralign> {{ :resources:eval:dpg:ad9136:ad9136-35_dac1_scope_output.png?600 | }}//Figure 9. DAC1 Output Scope Display// </WRAP> |
- Press the download arrow ({{:resources:eval:dpg:9154_down_arrow.png}}) then the play button ({{:resources:eval:dpg:9154_right_green_arrow.png}}). **Serial Line Rate** should appear as 10 Gbps and **Sync Status** should have two check marks. Refer to FFT plot of the DAC0 output in Figure <> and the oscilloscope capture of DAC1 output in Figure <>. | - Press the download arrow ({{:resources:eval:dpg:9154_down_arrow.png}}) then the play button ({{:resources:eval:dpg:9154_right_green_arrow.png}}). **Serial Line Rate** should appear as 10 Gbps and **Sync Status** should have two check marks. Refer to FFT plot of the DAC0 output in Figure 8 and the oscilloscope capture of DAC1 output in Figure 9. |
| |
<WRAP centeralign> {{ :resources:eval:dpg:ad9136:ad9136-35_dac0_sa_output.png?600 | }}//Figure 9. DAC0 Output Spectrum Analyzer Display// </WRAP> | |
| |
<WRAP centeralign> {{ :resources:eval:dpg:ad9136:ad9136-35_dac1_scope_output.png?600 | }}//Figure 8. DAC1 Output Scope Display// </WRAP> | |