This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:developer-kits:x-band-dev-kit:hardware-connections [22 Mar 2022 19:01] – XUD1A to Stingray Connection update Sam Ringwood | resources:eval:developer-kits:x-band-dev-kit:hardware-connections [17 May 2022 17:27] (current) – Sam Ringwood | ||
---|---|---|---|
Line 17: | Line 17: | ||
\\ | \\ | ||
==== RF Connectors ==== | ==== RF Connectors ==== | ||
- | - The Stingray board uses SMPM connectors on both sides of the board, so depending on how the board is used, adapters to mate with test equipment cabling may be required. Note that the Stingray board includes | + | - The Stingray board uses SMPM connectors on both sides of the board, so depending on how the board is used, adapters to mate with test equipment cabling may be required. Note that the Stingray board includes |
- | - The XUD1a board uses SMA connectors on the RF side of the board and SMPM connectors on the IF side of the board. | + | - The XUD1a board uses SMA connectors on the RF side of the board and SMPM connectors on the IF side of the board. Note that the XUD1A board includes 1x 12" SMPM-SMA cable. |
- The MxFE board uses SMA connectors for both the ADCs and DACs. | - The MxFE board uses SMA connectors for both the ADCs and DACs. | ||
Line 27: | Line 27: | ||
- J55 from the ZCU102 should connect to P3 on the Stingray board using a ribbon cable and any required adapters. Note that pin 1 should connect to pin 1. This will require two PMOD cables to vertically flip the pinout from the ZCU102 to match that of the Stingray board. \\ \\ | - J55 from the ZCU102 should connect to P3 on the Stingray board using a ribbon cable and any required adapters. Note that pin 1 should connect to pin 1. This will require two PMOD cables to vertically flip the pinout from the ZCU102 to match that of the Stingray board. \\ \\ | ||
- J87 from the ZCU102 should connect to P4 on the Stingray board using a ribbon cable and any required adapters. Note that pin 1 should connect to pin 1. This will require two PMOD cables to vertically flip the pinout from the ZCU102 to match that of the Stingray board. | - J87 from the ZCU102 should connect to P4 on the Stingray board using a ribbon cable and any required adapters. Note that pin 1 should connect to pin 1. This will require two PMOD cables to vertically flip the pinout from the ZCU102 to match that of the Stingray board. | ||
+ | |||
+ | |||
+ | {{ : | ||
\\ | \\ | ||
===== XUD1a: ADXUD1AEBZ ===== | ===== XUD1a: ADXUD1AEBZ ===== | ||
- | Connect the XUD1a evaluation board to the ZCU102' | + | Connect the XUD1a evaluation board to the ZCU102' |
- | {{ /resources/eval/developer-kits/x-band-dev-kit/ | + | |
+ | {{ :resources:eval:developer-kits:x-band-dev-kit: | ||
\\ | \\ | ||
Line 68: | Line 72: | ||
^ 4 | J1A (SMA) | 4 (SMA) | | ^ 4 | J1A (SMA) | 4 (SMA) | | ||
+ | ===== Support ===== | ||
+ | For additional questions or support, please visit the Engineering Zone forum at [[ez> | ||
+ | |||
+ | [[resources/ |