Both sides previous revisionPrevious revisionNext revision | Previous revision |
resources:eval:ad9467-fmc-250ebz [16 Jul 2015 11:08] – [Typical Measurement Setup] Lucian Sin | resources:eval:ad9467-fmc-250ebz [25 Apr 2023 13:29] (current) – Fix typo regarding the value of oscillator frequency Iulia Moldovan |
---|
====== EVALUATING THE AD9467-FMC-250EBZ ANALOG-TO-DIGITAL CONVERTER ====== | ====== EVALUATING THE AD9467-FMC-250EBZ ANALOG-TO-DIGITAL CONVERTER ====== |
===== Preface ===== | ===== Preface ===== |
This user guide describes the [[adi>AD9467|AD9467]] evaluation board [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] which provides all the support circuitry required to operate the ADC in its various modes and configurations. The application software to interface with the devices is also described. | This user guide describes the [[adi>AD9467|AD9467]] evaluation board [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] which provides all the support circuitry required to operate the ADC in its various modes and configurations. The application software to interface with the devices is also described. |
\\ | \\ |
\\ | \\ |
===== AD9467-FMC-250EBZ ===== | ===== AD9467-FMC-250EBZ ===== |
{{ :resources:eval:ad9467_board.png?700 |}}<WRAP centeralign> | {{ :resources:eval:ad9467_board.png?700 |}}<WRAP centeralign> |
//Figure 1. [[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] Evaluation Board//</WRAP> | //Figure 1. [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] Evaluation Board//</WRAP> |
| |
===== Typical Measurement Setup ===== | ===== Typical Measurement Setup ===== |
{{ :resources:eval:ad9467_datacapture.png?900 |}}<WRAP centeralign> | {{ :resources:eval:ad9467_datacapture.png?900 |}}<WRAP centeralign> |
//Figure 2. Evaluation Board Connection—[[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] (on Left) and [[adi>SDP-H1|SDP-H1]] (on Right)// | //Figure 2. Evaluation Board Connection—[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] (on Left) and [[adi>SDP-H1|SDP-H1]] (on Right)// |
</WRAP> | </WRAP> |
| |
===== Helpful Documents ===== | ===== Helpful Documents ===== |
* [[adi>AD9467|AD9467]] Data Sheet | * [[adi>AD9467|AD9467]] Data Sheet |
* EVAL-SDP-CH1Z data capture kit [[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] | * EVAL-SDP-CH1Z data capture kit [[adi>en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] |
* [[adi>an-905|AN-905 Application Note]], //VisualAnalog Converter Evaluation Tool Version 1.0 User Manual// | * [[adi>an-905|AN-905 Application Note]], //VisualAnalog Converter Evaluation Tool Version 1.0 User Manual// |
* [[adi>an-878|AN-878 Application Note]], //High Speed ADC SPI Control Software// | * [[adi>an-878|AN-878 Application Note]], //High Speed ADC SPI Control Software// |
* [[adi>an-835|AN-835 Application Note]], //Understanding ADC Testing and Evaluation// | * [[adi>an-835|AN-835 Application Note]], //Understanding ADC Testing and Evaluation// |
===== Software Needed ===== | ===== Software Needed ===== |
* VisualAnalog [[ftp://ftp.analog.com/pub/HSSP_SW/VisualAnalog/VisualAnalog_Setup.exe]] | * [[adi>VisualAnalog|VisualAnalog]] |
* SPIController [[ftp://ftp.analog.com/pub/adispi/A2DComponents/Install/SPIController_Setup.exe]] | * [[adi>/en/design-center/interactive-design-tools/spicontroller.html|SPIController]] |
| |
===== Design and Integration Files ===== | ===== Design and Integration Files ===== |
* FPGA BIN file ftp://ftp.analog.com/pub/HSC_ADC_Apps/SDP-H1/ad9467_sdp_h1.bin | * {{:resources:eval:ad9467fmc:ad9467_sdp_h1.zip|FPGA bin file (Unzip before use)}} |
* [[http://wiki.analog.com/resources/fpga/xilinx/fmc/ad9467#downloads |Schematics, Bill Of Materials, and Gerber Layout/Fabrication Files]] | * [[/resources/fpga/xilinx/fmc/ad9467#downloads |Schematics, Bill Of Materials, and Gerber Layout/Fabrication Files]] |
===== Equipment Needed ===== | ===== Equipment Needed ===== |
* Analog signal source and antialiasing filter | * Analog signal source and antialiasing filter |
* USB 2.0 port | * USB 2.0 port |
* [[adi>AD9467|AD9467-FMC-250EBZ]] board | * [[adi>AD9467|AD9467-FMC-250EBZ]] board |
*[[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] FPGA-based data capture kit | *[[adi>en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] FPGA-based data capture kit |
| |
===== Getting Started ===== | ===== Getting Started ===== |
This section provides quick start procedures for using the [[adi>AD9467|AD9467-FMC-250EBZ]] board. \\ | This section provides quick start procedures for using the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] board. \\ |
| |
==== Configuring the Board ==== | ==== Configuring the Board ==== |
Before using the software for testing, configure the evaluation board as follows: | Before using the software for testing, configure the evaluation board as follows: |
- Connect the [[adi>AD9467|AD9467-FMC-250EBZ]] evaluation board to the [[adi>SDP-H1|SDP-H1]] data capture board, as shown in Figure 2. | - Connect the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-AD9467.html#eb-overview|AD9467-FMC-250EBZ]] evaluation board to the [[adi>SDP-H1|SDP-H1]] data capture board, as shown in Figure 2. |
- Connect one 12V, 2.5A switching power supply (such as the one supplied) to the [[adi>SDP-H1|SDP-H1]] board. Connect the Mini-B USB port of the [[adi>SDP-H1|SDP-H1]] board to the PC with the supplied USB cable. | - Connect one 12V, 2.5A switching power supply (such as the one supplied) to the [[adi>SDP-H1|SDP-H1]] board. Connect the Mini-B USB port of the [[adi>SDP-H1|SDP-H1]] board to the PC with the supplied USB cable. |
- The [[http://www.analog.com/en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] will appear in the Device Manager as shown in Figure 3. {{ :resources:eval:device_manger.png?200 |}}<WRAP centeralign> | - The [[adi>en/system-demonstration-platform/controller-boards/evaluation/EVAL-SDP-H1/eb.html|SDP-H1]] will appear in the Device Manager as shown in Figure 3. {{ :resources:eval:device_manger.png?200 |}}<WRAP centeralign> |
//Figure 3. Device Manager Showing SDP-H1 //</WRAP> | //Figure 3. Device Manager Showing SDP-H1 //</WRAP> |
- If the Device Manager does not show the [[adi>SDP-H1|SDP-H1]] listed as shown in Figure 2, unplug all USB devices from the PC, uninstall and re-install SPIController and VisualAnalog and restart the hardware setup from step 1. | - If the Device Manager does not show the [[adi>SDP-H1|SDP-H1]] listed as shown in Figure 2, unplug all USB devices from the PC, uninstall and re-install SPIController and VisualAnalog and restart the hardware setup from step 1. |
* Ensure that the ADC has a valid clock input | * Ensure that the ADC has a valid clock input |
| |
| ===== AD9517-4 Configuration (Optional) ===== |
| The AD9467-FMC-250EBZ is configured from the factory to use an external clock connected to J201. Alternatively, the AD9467-FMC-250EBZ can be configured to use the on-board 250MHz oscillator and AD9517-4 Clock Generator to generate the 250 Msps clock input. (Note: some boards have shipped with a 250 MHz oscillator and will require a different configuration) |
| |
| ** Hardware Modifications ** |
| *Remove the following components: R209, R210, C209, C210 |
| *Add the following components: C205, C206, C300, C301, C304, C305 |
| *Make sure that Jumper P200 is on the "On" Position |
| |
| **Additional Software Needed** |
| *{{:resources:eval:ad9467fmc:configure_ad9517_ad9467-fmc-250ebz_.zip|configure_ad9517_AD9467-FMC-250EBZ MGP file}} |
| ** Setup Instructions ** |
| - Make sure that a clock source is not connected to J201 |
| - Configure SPIcontroller and VisualAnalog as described above |
| - Launch a 2nd instance of SPIController. |
| - Load the AD9517spiR03.cfg configuration file. |
| - Click Config>Controller Dialog |
| - Select "2" Under FIFO Chip Sel # {{ :resources:eval:ad9467fmc:SPI_Controller_Cfg_Dialog2.PNG?262 |}}<WRAP centeralign> |
| //Figure 12. Select Fifo Chip Sel # 2 in SPIController//</WRAP> |
| - Click Apply and OK |
| - Click File>Macro Group Open |
| - Select the configure_ad9517_AD9467-FMC-250EBZ .mgp file |
| - Check the Enable Check Box {{ :resources:eval:ad9467fmc:MacroEditor-Enable.PNG?375 |}}<WRAP centeralign> |
| //Figure 13. Select Enable Macro in SPIController//</WRAP> |
| - Click Run Macros {{ :resources:eval:ad9467fmc:run.PNG?23 |}}<WRAP centeralign> |
| //Figure 14. Click Run Macros in SPIController//</WRAP> |
| - Make sure that LED CR300 is illuminated on the AD9467-FMC-250EBZ. |
| |
| ** Obtaining an FFT ** |
| - Click the Run button in VisualAnalog , you should see the captured data similar to the plot shown in Figure 9 {{ :resources:eval:ad9467fmc:fft-ad9517.png?736 |}} <WRAP centeralign> |
| //Figure 15. AD9467-FMC-250 FFT at 140.3MHz Analog Input (performance may be degraded compared to high-quality direct clock)//</WRAP> |
| |
| |
| |