This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9259-50ebz [03 Dec 2021 04:03] – [Typical Measurement Setup] Meriam Yuson-Aguila | resources:eval:ad9259-50ebz [03 Dec 2021 04:28] (current) – [Equipment Needed] Meriam Yuson-Aguila | ||
---|---|---|---|
Line 1: | Line 1: | ||
====== EVALUATING THE AD9228 / AD9259 / AD9287 ANALOG-TO-DIGITAL CONVERTERS ====== | ====== EVALUATING THE AD9228 / AD9259 / AD9287 ANALOG-TO-DIGITAL CONVERTERS ====== | ||
===== Preface ===== | ===== Preface ===== | ||
- | This user guide describes the [[adi> | + | This user guide describes the [[adi> |
\\ | \\ | ||
\\ | \\ | ||
Line 9: | Line 9: | ||
{{ : | {{ : | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | //Figure 1. Evaluation Board Connection—[[adi> | + | //Figure 1. Evaluation Board Connection—[[adi> |
</ | </ | ||
Line 34: | Line 34: | ||
* PC running Windows® | * PC running Windows® | ||
* USB 2.0 port, recommended (USB 1.1-compatible) | * USB 2.0 port, recommended (USB 1.1-compatible) | ||
- | * [[adi> | + | * [[adi> |
* [[adi> | * [[adi> | ||
===== Getting Started ===== | ===== Getting Started ===== | ||
- | This section provides quick start procedures for using the [[adi> | + | This section provides quick start procedures for using the [[adi> |
==== Configuring the Board ==== | ==== Configuring the Board ==== | ||
Before using the software for testing, configure the evaluation board as follows: | Before using the software for testing, configure the evaluation board as follows: | ||
- Connect the boards to each other as shown in Figure 1. | - Connect the boards to each other as shown in Figure 1. | ||
- | - Connect one 6 V, 2 A switching power supply (such as the CUI KSAFD0500300W1US that is supplied) to P503 on the [[adi> | + | - Connect one 6 V, 2 A switching power supply (such as the CUI KSAFD0500300W1US that is supplied) to P503 on the [[adi> |
- Connect one 6 V, 2 A switching power supply (such as the supplied CUI KSAFD0500300W1US) to J4 on the [[adi> | - Connect one 6 V, 2 A switching power supply (such as the supplied CUI KSAFD0500300W1US) to J4 on the [[adi> | ||
- Connect the [[adi> | - Connect the [[adi> |