This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9259-50ebz [03 Dec 2021 04:26] – [Getting Started] Meriam Yuson-Aguila | resources:eval:ad9259-50ebz [03 Dec 2021 04:28] (current) – [Equipment Needed] Meriam Yuson-Aguila | ||
---|---|---|---|
Line 9: | Line 9: | ||
{{ : | {{ : | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | //Figure 1. Evaluation Board Connection—[[adi> | + | //Figure 1. Evaluation Board Connection—[[adi> |
</ | </ | ||
Line 34: | Line 34: | ||
* PC running Windows® | * PC running Windows® | ||
* USB 2.0 port, recommended (USB 1.1-compatible) | * USB 2.0 port, recommended (USB 1.1-compatible) | ||
- | * [[adi> | + | * [[adi> |
* [[adi> | * [[adi> | ||
Line 43: | Line 43: | ||
Before using the software for testing, configure the evaluation board as follows: | Before using the software for testing, configure the evaluation board as follows: | ||
- Connect the boards to each other as shown in Figure 1. | - Connect the boards to each other as shown in Figure 1. | ||
- | - Connect one 6 V, 2 A switching power supply (such as the CUI KSAFD0500300W1US that is supplied) to P503 on the [[adi> | + | - Connect one 6 V, 2 A switching power supply (such as the CUI KSAFD0500300W1US that is supplied) to P503 on the [[adi> |
- Connect one 6 V, 2 A switching power supply (such as the supplied CUI KSAFD0500300W1US) to J4 on the [[adi> | - Connect one 6 V, 2 A switching power supply (such as the supplied CUI KSAFD0500300W1US) to J4 on the [[adi> | ||
- Connect the [[adi> | - Connect the [[adi> |