This is an old revision of the document!
This wiki site includes information about the AD6676 and the associated evaluation board, the AD6676EBZ.
The AD6676 datasheet provides a significant amount of information to aid in understanding the AD6676 capabilities and can assist in the evaluation process. The datasheet along with the user guide and other board files provided here should be consulted when using the evaluation board.
The AD6676 is compatible with the HSC-ADC-EVALEZ, the ADI FPGA-Based Data Capture Kit.
The software required to use the AD6676EBZ with the HSC-ADC-EVALEZ capture board can be downloaded at the following Analog Devices ftp site:
For additional information or questions, send an email to highspeed.converters@analog.com. The user guide describes the AD6676 evaluation board, AD6676EBZ, which provides all of the support circuitry required to operate the part in various modes and configurations. The application software used to interface with the devices is also described.
User Guide for the AD6676 ad6676_evb_rev1_quickstartguide_2015_03_27.pdf (UPDATED March 2015)
AD6676 Evaluation Board Schematic Board 13029 Rev D SCHEMATIC [PDF File]
AD6676 Evaluation Board Gerber Files Board 13029 Rev D GERBERS [Zip File]
AD6676 Evaluation Board BOM File Board 13029 Rev D Bill of Material [XLS file]
AD6676 DemoTool Software Installation Files : AD6676 Evaluation Software
The link below is to an external website which has a project with HDL code that can be used with some FPGA development board to interface to the AD6676
External Link to github.com AD6676 library
External Link to github.com AD6676 project
External Link to general github.com website
AD6676 Ibis Model AD6676 Ibis [ZIP file]
AD6676 Ibis AMI Model Email highspeed.converters@analog.com to request
AD6676 Simulink Model Package AD6676 Simulink Model
AD6676 Simulink User's Guide
AD6676 Simulink User's Guide [pdf file]