Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revision Previous revision
resources:demo:reference-designs:demo-ad5758-ao8z:introduction [15 Aug 2019 12:33]
Donal O''Sullivan [Introduction]
resources:demo:reference-designs:demo-ad5758-ao8z:introduction [29 Dec 2020 23:03]
Robin Getz fix links
Line 6: Line 6:
 //Figure 1 - Block diagram of a single channel// //Figure 1 - Block diagram of a single channel//
  
-This Board is a demonstration a system level solution where the [[adi>http://​www.analog.com/​ad5758|AD5758]] and the [[adi>http://​www.analog.com/​adp1031|ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions.+This Board is a demonstration a system level solution where the [[adi>​AD5758]] and the [[adi>​ADP1031]] can be used together to implement a compact, eight channel, channel-to-channel isolated, precision analog output (AO) module, while achieving less than 2 W worst case power dissipation over a wide range of operating conditions.
  
-The [[adi>http://​www.analog.com/​adp1031|ADP1031]] solves the isolation and size challenges and the [[adi>http://​www.analog.com/​ad5758|AD5758]] provides a low power dissipation,​ precision, configurable current or voltage output channel. ​+The [[adi>​ADP1031]] solves the isolation and size challenges and the [[adi>​AD5758]] provides a low power dissipation,​ precision, configurable current or voltage output channel. ​
  
-This board uses the [[adi>http://​www.analog.com/​aducm3029|ADUCM3029]] as the system controller to control each channel independently.+This board uses the [[adi>​ADUCM3029]] as the system controller to control each channel independently.
  
 {{:​resources:​demo:​reference-designs:​demo-ad5758-ao8z:​gui:​block_diagram.png|}}\\ {{:​resources:​demo:​reference-designs:​demo-ad5758-ao8z:​gui:​block_diagram.png|}}\\
resources/demo/reference-designs/demo-ad5758-ao8z/introduction.txt · Last modified: 29 Dec 2020 23:03 by Robin Getz