This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
wiki:editing [11 May 2011 23:14] – Approved andyr | wiki:editing [25 Apr 2014 19:29] (current) – re-word with new process Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Page editing | + | ====== Page Editing |
- | To edit a page in the wiki, simply log in, and click the button labeled "Edit this page" shown on the top of the page. This will switch to editing | + | Developing Documentation is a combination |
- | Wiki pages are written in a simple, plain-text [[syntax]], that allows structuring the page and pleasant formatting while retaining high readability of the page source. When you edit a page and save your changes, the previous content will not be lost. Instead it will be saved as an old revision of the page in the [[doku> | + | Wiki pages are written in a simple, plain-text [[syntax]] with a few [[more_syntax|extensions]], that allows structuring the page and pleasant formatting while retaining high readability of the page source. When you edit a page and save your changes, the previous content will **not** be lost. Instead it will be saved as an old revision of the page in the [[doku> |
- | Before you edit your first " | + | Before you edit your first " |
- | ===== Developing Documentation | + | ===== Editing Existing Pages ===== |
- | Developing Documentation will be a combination of editing existing | + | To edit a page in the wiki, simply log in (you must be logged in, with a valid myAnalog account to edit wiki pages), and either : |
+ | * edit the **entire page** at once, by clicking the button labeled "Edit this page" shown on the top of the page. | ||
+ | * edit **a section**, by clicking the button labeled " | ||
+ | Clicking on either button will switch to [[syntax|editing]] mode for this page, and you can change the wiki source of this page in an embedded editor. Before saving changes (by clicking on the //Save// button), examine your changes, by looking at a //Preview// or see a difference, by clicking on the //Changes// button. | ||
- | ==== Editing existing | + | ===== Creating new pages ===== |
- | Editing an existing page, is as simple as going to that page, and clicking on the //Edit this page// button at the top of the page, or the //Edit// links at each section break. Editing sections is sometimes easier, since it is just less text to deal with. | + | |
- | Before saving changes (by clicking on the //Save// button), examine your changes, by looking at a //Preview// or see a difference, by clicking on the //Changes// button. | + | There are two ways to create new pages. Both require that you are logged into the wiki and have special access |
- | + | ||
- | ==== Creating new pages (Requires Special Access)==== | + | |
- | There are two ways to create new pages. Both require that you are logged into the wiki and have special access. | + | |
- go to the page that you want to create (by typing in the exact path), and clicking on the " | - go to the page that you want to create (by typing in the exact path), and clicking on the " | ||
- create a link by editing an existing page, to something that doesn' | - create a link by editing an existing page, to something that doesn' | ||
- | ===== Process/Publishing | + | ====== The Creation/Editing Process ====== |
Just like paper documentation, | Just like paper documentation, | ||
Public pages will always have a banner at the top of each page, with information about the Approval/ | Public pages will always have a banner at the top of each page, with information about the Approval/ | ||
- | ==== Under Development ==== | + | The development process is something like: |
- | Anyone creating a page can add a %%~~UNDERCONSTRUCTION~~%% tag anywhere into their page - and no one can look at it, or edit it except the original author. This allows documentation to be created over days/weeks before it becomes | + | < |
+ | digraph { | ||
+ | subgraph cluster_0 { | ||
+ | style=filled; | ||
+ | color=lightgrey; | ||
+ | node [style=filled, | ||
+ | " | ||
+ | label = "Under Development"; | ||
+ | } | ||
- | ==== Approvals ==== | + | subgraph cluster_1 { |
+ | node [style=filled]; | ||
+ | " | ||
+ | label | ||
+ | color=blue | ||
+ | } | ||
- | Any Analog Devices Employee can //Approve// a page. You do so by editing the page, and ticking the '' | + | "Under Development" |
+ | " | ||
+ | } | ||
+ | </graphviz> | ||
- | ==== Drafts | + | ===== Under Development ===== |
- | Anyone logged into the wiki, can edit a page, and their version will be saved as a draft. | + | When a page is initially created on the Wiki, it will only be visible to Analog Devices employees until it is approved. |
+ | |||
+ | Once a page has been approved (by an ADI employee), it will be public and visible to both internal and external audiences. | ||
+ | |||
+ | Once content is public, any edits made to it will also be public. | ||
+ | |||
+ | ===== Drafts ===== | ||
+ | |||
+ | Anyone logged into the wiki, can edit a page, and their version will be saved as a draft. You do not need to be an Analog Devices employee to edit a page. If you see a problem - please fix it. | ||
Anyone not logged into the site will see the latest approved revision by default (unless there isn't one). All users can still view any revision of a page if they specifically request it -- whether or not it is approved. | Anyone not logged into the site will see the latest approved revision by default (unless there isn't one). All users can still view any revision of a page if they specifically request it -- whether or not it is approved. | ||
- | ===== Troubleshooting ===== | + | ===== Approvals ===== |
+ | |||
+ | Any Analog Devices Employee can //Approve// a page. You do so by clicking the " | ||
+ | |||
+ | ====== Troubleshooting | ||
In some cases, the editing of a page is impossible. This can be mainly for these reasons : | In some cases, the editing of a page is impossible. This can be mainly for these reasons : |