Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:tools:pluto:users [24 Aug 2018 13:02] – [Contents] Michael Hennerich | university:tools:pluto:users [08 Jun 2019 17:29] – add phase noise page Robin Getz |
---|
- [[./users/far_fast|How Far, How fast?]] | - [[./users/far_fast|How Far, How fast?]] |
- [[./users/transmit|RF Output]] | - [[./users/transmit|RF Output]] |
| - [[./users/phase_noise|Phase Noise & Accuracy]] |
- [[./users/receive|RF Input]] | - [[./users/receive|RF Input]] |
- [[./users/receiver_sensitivity|Receiver Sensitivity]] | - [[./users/receiver_sensitivity|Receiver Sensitivity]] |
- [[./users/calibration|Calibrating]] the ADALM-PLUTO. | - [[./users/calibration|Calibrating]] the ADALM-PLUTO. |
- [[./users/customizing|Customizing]] the ADALM-PLUTO. | - [[./users/customizing|Customizing]] the ADALM-PLUTO. |
- using more than one the ADALM-PLUTO on the same PC. | |
- Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from: | - Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from: |
- Using Pluto with the [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] | - [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] |
- example 1 | - [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio |
- Using Pluto with the [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio and the Qt graphical toolkit. | - [[https://www.mathworks.com/hardware-support/adalm-pluto-radio.html|Official support for MATLAB and Simulink]] |
- Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB]] | - [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB IIO Bindings]] |
- example 1 | - [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] |
- Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|Simulink]] | - [[https://github.com/f4exb/sdrangel|SDRangel]], an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware. |
- example 2 | - [[https://airspy.com/download/|SDR#]]. The PlutoSDR frontend for SDRsharp can be found here: [[https://github.com/Manawyrm/sdrsharp-plutosdr|sdrsharp-plutosdr]] |
- Using Pluto with [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] | - [[https://github.com/pothosware/SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https://github.com/jocover/SoapyPlutoSDR|SoapyPlutoSDR]] |
- [[./examples/gnuradio|Example 1]] | - [[https://github.com/radiosd/PlutoSdr|Access and control of PlutoSDR hardware using python bindings to libiio]] |
- Using Pluto with [[https://github.com/f4exb/sdrangel|SDRangel]]. SDRangel is an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware. | |
- Using Pluto with SDR#. The PlutoSDR frontend for SDRsharp can be found here: [[https://github.com/Manawyrm/sdrsharp-plutosdr|sdrsharp-plutosdr]] | |
- Using Pluto with [[https://github.com/pothosware/SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https://github.com/jocover/SoapyPlutoSDR|SoapyPlutoSDR]] | |
- Using Pluto with [[https://github.com/radiosd/PlutoSdr|Access and control of PlutoSDR hardware using python bindings to libiio]] | |
| |
| |
| |