Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
university:tools:pluto:users [08 Feb 2017 00:30] – [Contents] Robin Getz | university:tools:pluto:users [14 Jan 2021 05:38] – use mw> interwiki links Robin Getz |
---|
{{ :university:tools:pluto:pluto_in_hand.png?200|}} | {{ :university:tools:pluto:pluto_in_hand.png?200|}} |
| |
Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNURadio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product). | Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, etc.) platform over USB. As you can see, we have lots of examples with MATLAB and Simulink, as we find that a very powerful environment, and a path to a releasable radio (you can take your algorithms, and easily embed them into a custom product). |
| |
===== Contents ===== | ===== Contents ===== |
- [[./users/name|What's with the name?]] //PlutoSDR?// | - [[./users/name|What's with the name?]] //PlutoSDR?// |
- [[./users/understanding|Understanding the Internals]] | - [[./users/understanding|Understanding the Internals]] |
| - [[./users/temp|How hot?]] |
| - [[./users/far_fast|How Far, How fast?]] |
| - [[./users/transmit|RF Output]] |
| - [[./users/phase_noise|Phase Noise & Accuracy]] |
| - [[./users/receive|RF Input]] |
| - [[./users/receiver_sensitivity|Receiver Sensitivity]] |
| - [[./users/non_quad|Dealing with Non-Quadrature signals]] |
| - [[./users/antennas|Antennas]] |
- [[./users/quick_start|Quick Start]] | - [[./users/quick_start|Quick Start]] |
- Intro to the Software. Installing Device Drivers on: | - Intro to the Software. Installing Device Drivers on: |
- [[./users/calibration|Calibrating]] the ADALM-PLUTO. | - [[./users/calibration|Calibrating]] the ADALM-PLUTO. |
- [[./users/customizing|Customizing]] the ADALM-PLUTO. | - [[./users/customizing|Customizing]] the ADALM-PLUTO. |
- using more than one the ADALM-PLUTO on the same PC. | |
- Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from: | - Once the driver are configured and set up, you can interact with the [[adi>ADALM-PLUTO]] Active Learning Module from: |
- Using Pluto with the [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] | - [[/resources/tools-software/linux-software/iio_oscilloscope|IIO oscilloscope]] |
- example 1 | - [[http://gqrx.dk/|gqrx]], an open source software defined radio receiver (SDR) powered by the GNU Radio |
- Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB]] | - [[mw>hardware-support/adalm-pluto-radio.html|Official support for MATLAB and Simulink]] |
- example 1 | - [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|MATLAB IIO Bindings]] |
- Using Pluto with [[/resources/tools-software/linux-software/libiio/clients/matlab_simulink|Simulink]] | - [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] |
- example 2 | - [[https://github.com/f4exb/sdrangel|SDRangel]], an Open Source Qt5 / OpenGL 3.0+ SDR and signal analyzer frontend to various hardware. |
- Using Pluto with [[/resources/tools-software/linux-software/gnuradio|GNURadio]] | - [[https://airspy.com/download/|SDR#]]. The PlutoSDR frontend for SDRsharp can be found here: [[https://github.com/Manawyrm/sdrsharp-plutosdr|sdrsharp-plutosdr]] |
- example 1 | - [[https://github.com/pothosware/SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https://github.com/jocover/SoapyPlutoSDR|SoapyPlutoSDR]] |
| - [[https://github.com/radiosd/PlutoSdr|Access and control of PlutoSDR hardware using python bindings to libiio]] |
| - [[:resources/tools-software/linux-software/pyadi-iio|Python Interfaces]] |
| - [[:university/tools/pluto/controlling_the_transceiver_and_transferring_data|C Examples]] |
| |
| |
| |