This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
university:tools:pluto:users [10 Apr 2017 18:29] – add a how far/fast section Robin Getz | university:tools:pluto:users [15 Mar 2019 19:03] – Cleanup of unnecessary repetative statements Travis Collins | ||
---|---|---|---|
Line 3: | Line 3: | ||
{{ : | {{ : | ||
- | Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, | + | Everyone using Pluto should read these pages. They will demonstrate how to interact with RF signals with MATLAB, Simulink, GNU Radio or custom C, C++, C#, or Python code on a host (x86) or embedded (Raspberry Pi, Beaglebone, 96boards.org, |
===== Contents ===== | ===== Contents ===== | ||
Line 23: | Line 23: | ||
- [[./ | - [[./ | ||
- [[./ | - [[./ | ||
- | - using more than one the ADALM-PLUTO on the same PC. | ||
- Once the driver are configured and set up, you can interact with the [[adi> | - Once the driver are configured and set up, you can interact with the [[adi> | ||
- | - Using Pluto with the [[/ | + | - [[/ |
- | - example 1 | + | - [[http:// |
- | - Using Pluto with the [[http:// | + | - [[/ |
- | - Using Pluto with [[/ | + | - [[/ |
- | - example 1 | + | - [[https://github.com/ |
- | - Using Pluto with [[/ | + | - SDR#. The PlutoSDR frontend for SDRsharp can be found here: [[https:// |
- | - example 2 | + | - [[https://github.com/pothosware/SoapySDR|SoapySDR]]. The Soapy SDR plugin for PlutoSDR can be found here: [[https:// |
- | - Using Pluto with [[/resources/tools-software/linux-software/gnuradio|GNU Radio]] | + | - [[https:// |
- | - example 1 | + | |