This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
university:tools:pluto:users:transmit [08 Jun 2019 15:10] – [Transmit Power] Robin Getz | university:tools:pluto:users:transmit [08 Jun 2019 15:25] (current) – [Transmit Power] Robin Getz | ||
---|---|---|---|
Line 35: | Line 35: | ||
- | {{: | + | {{: |
- | {{ : | + | |
+ | {{ : | ||
The random peaks in the -10 dB attenuation settings are (I think) random noise caused by the Tx calibrations when the LO changes by more than 100 MHz. | The random peaks in the -10 dB attenuation settings are (I think) random noise caused by the Tx calibrations when the LO changes by more than 100 MHz. |